Renewables at scale: How legacy grids can keep pace with the Renewable Energy Transition

The biggest obstacle to the renewable energy transition may not be a lack of renewable energy. It may be the grid we already have.  

Solar, wind, hydroelectric power and other renewable sources are scaling rapidly, while electricity demand is becoming more dynamic as transportation, buildings, industry and digital infrastructure electrify. The energy transition is changing not only where our electricity comes from, but how the entire power system needs to operate. Much of today’s electrical infrastructure was designed for a different energy system: large, centralized power plants generating relatively predictable electricity that flows primarily in one direction through transmission and distribution networks toward consumers.  

That model is changing. Solar and wind generation can fluctuate with weather and time of day, while rooftop solar, batteries, community generation and other distributed energy resources are introducing thousands of new assets at the edge of the grid. Consumers are increasingly becoming “prosumers,” moving between consuming and producing electricity, while batteries can change when electricity enters and leaves the network. For utilities, the renewable energy transition is therefore also a grid management challenge. Integrating renewables at scale requires a network that can see what is happening in real time, anticipate changes in generation and demand, and coordinate an increasingly complex mix of resources.  

The answer is not to abandon the legacy grid or rebuild it from the ground up. It is to make the grid we already have more intelligent, flexible and responsive. This requires a new era of Energy Intelligence connecting electrical infrastructure, software and data to help utilities anticipate constraints, orchestrate flexibility and integrate renewable energy at scale.  

Why the legacy grid wasn’t built for renewables?  

For decades, electricity networks were engineered around centralized generation and relatively predictable demand. Renewable energy is changing that architecture by making power flows more dynamic and, increasingly, bidirectional. Electricity can move from customers and distributed generators back into the grid, generation can change rapidly as weather conditions shift, and thousands of rooftop solar systems, batteries and other distributed resources can collectively affect network conditions.  

This puts new demands on transformers, substations, feeders and other infrastructure that may not have been designed for today’s complex power flows. The issue is not renewable energy itself; it is whether the grid has the visibility, flexibility and control needed to manage renewable generation reliably as its share of the energy mix increases.  

That distinction matters. Rather than treating renewable integration as a reason to replace everything, utilities can focus physical investment where it is needed while using digital technologies to make existing infrastructure work harder and smarter.  

Building the intelligence layer for a renewable-ready grid  

A renewable-ready grid needs more than new generation and new wires. It needs an intelligence layer that connects physical infrastructure with the growing number of resources operating across the network.  

That means bringing together medium- and low-voltage distribution infrastructure, renewable generation, distributed energy resources, battery storage, smart substations and switchgear with real-time monitoring, advanced distribution management, automated operations, forecasting and analytics. Advanced Distribution Management Systems (ADMS) and Distributed Energy Resource Management Systems (DERMS) can help utilities turn growing volumes of data and connected assets into actionable information. A unified digital grid platform connects data and network models across planning, operations and flexibility management, linking enterprise software with intelligence at the grid edge.  

The objective is straightforward: give operators a clearer understanding of what is happening across the network and the tools to respond. Real-time data from substations, feeders, smart devices, renewable assets, storage and customers can help identify emerging constraints and changing network conditions, while forecasting can help operators anticipate shifts in generation and demand. AI-enabled forecasting can help utilities anticipate changes in renewable generation and electricity demand, supporting earlier identification of network constraints and better-informed operational decisions.  

Digitalization, however, is not a replacement for physical infrastructure. It is the intelligence layer that allows existing and new infrastructure to operate more effectively together. That distinction will become increasingly important as utilities determine where additional capacity is essential and where better visibility, coordination and control can unlock more value from assets already in the network.  

What leading energy systems are already proving?  

This approach is already being put into practice in different markets.  

In Serbia, ElektroDistribucija Srbije (EDS) is upgrading its medium-voltage distribution system with Schneider Electric to help integrate increasing amounts of variable renewable energy while maintaining stability and reliability for its 3.8 million customers. The project demonstrates how modernizing distribution infrastructure can create greater flexibility for renewable energy while improving network performance.  

In Malaysia, PETRONAS and the Centre for Offshore Renewable Energy (CEFORE) are combining offshore wind, solar and wave energy within a microgrid supported by energy storage and smart energy management systems. The project demonstrates how multiple renewable sources and storage can be coordinated within a more resilient energy ecosystem.  

Australia offers another example of modernization and decarbonization happening together. Schneider Electric is working with Ausgrid on an SF₆-free kiosk pad substation incorporating automation capabilities and connectivity with the utility’s Advanced Distribution Management System. The project illustrates how new electrical infrastructure can reduce environmental impact while digital connectivity provides greater operational visibility and remote control.  

The applications differ, but the principle is consistent: the future grid will combine electrical infrastructure with digital intelligence to continuously adapt to changing conditions.  

Three challenges utilities must solve to scale renewables  

As renewable penetration increases, utilities will need to address three interconnected challenges: visibility, flexibility and modernization.  

1. See the Grid in real time  

Before utilities can make the grid more flexible, they need to make it visible. Utilities cannot effectively manage thousands of distributed generation and storage assets without a clear, real-time understanding of what is happening across the network.  

Connecting data from substations, feeders, smart devices, renewable assets, storage systems and customers into a common operational environment can help operators identify emerging constraints, understand disruptions and respond more quickly to changes in generation and demand.  

Better visibility also improves investment decisions. Without a detailed understanding of how the network is operating, utilities may default to building additional infrastructure to address potential constraints. Better data can help distinguish where physical reinforcement is necessary from where digital optimization or operational changes could unlock additional capacity.  

2. Make the grid more flexible  

Visibility alone is not enough. Renewable generation changes the timing, location and predictability of electricity production, so the grid needs more ways to balance supply and demand.  

Flexibility can come from battery energy storage, distributed generation, demand-side management, automated switching, dynamic network management, microgrids and better forecasting. DERMS can also help utilities coordinate distributed resources so solar, storage and other assets operate as active participants in the broader energy system rather than as disconnected devices.  

The renewable-ready grid is therefore not necessarily a grid with more infrastructure. It is a grid with more flexibility in how existing and new resources are managed. Where appropriate, that flexibility can help utilities make better use of existing network capacity while determining where new physical investment is truly required.  

3. Modernize infrastructure without starting from scratch  

There is a tendency to assume that integrating renewable energy requires utilities to replace the entire grid. In reality, much of today’s infrastructure will remain part of the electricity system for decades. The challenge is determining where physical modernization is essential and where digital intelligence can extend the capabilities of existing assets.  

A practical approach can begin with modernizing critical substations and distribution infrastructure, adding sensors and connected equipment, introducing ADMS and DERMS capabilities, and automating network operations where appropriate. Utilities can then use operational data to prioritize future physical investments and integrate storage and other distributed resources where they provide the greatest value.  

This phased approach allows utilities to make progress without waiting for a wholesale rebuild. The grid cannot simply be switched off and redesigned while the world continues to depend on it.  

The grid of the future will be renewable, digital and flexible  

Renewable energy integration is only one part of the broader transformation underway across the electricity system. Future grids will need to accommodate increasing amounts of solar and wind alongside hydroelectric and other renewable resources, while also managing distributed generation, battery storage, EV charging, electrified buildings and industry, microgrids and increasingly dynamic electricity demand.  

The more resources we add, the more important coordination becomes. Without digital intelligence, every new source of generation, storage system or electrified load can add another layer of complexity. With a connected digital foundation, those same resources can become part of a more coordinated and responsive energy architecture.  

This is where the physical and digital sides of grid modernization come together. Utilities need the right electrical infrastructure, but they also need the ability to understand what is happening across that infrastructure and act on it. AI-enabled analytics, forecasting, automation and increasingly sophisticated grid-management systems can help operators make better decisions as the number and diversity of energy resources grow.  

Building the renewable-ready grid today  

Scaling renewable energy is not simply a generation challenge. It is a grid management challenge.  

The electricity system of the future will be more distributed, dynamic and interconnected than the system many utilities were originally designed to operate. Successfully managing that transition will require physical modernization and digital intelligence to work together.  

The benefits extend beyond integrating more renewable generation. A more visible and flexible network can improve operational control, support reliability and resilience as generation and demand patterns change, and create a stronger foundation for storage, electrification and new distributed energy resources.  

Most importantly, utilities do not need to wait for a complete grid rebuild before moving toward a renewable future. By modernizing strategically, digitizing existing infrastructure and creating greater flexibility at the grid’s edge, they can begin building a renewable-ready grid today.  

The renewable energy transition will ultimately depend on more than how much clean energy we can generate. It will depend on how intelligently we can move, manage, and integrate that energy. 

See how ElektroDistribucija Srbije (EDS) is modernizing its grid to support renewable energy integration and improve network performance.

Watch the video to discover how end-to-end renewable solutions can help utilities build a smarter, more resilient energy future: 

Add a comment

All fields are required.