Powering growth: The EOEM opportunity for electrical contractors

Data center growth, electrification, and rising customer expectations are turning equipment manufacturing into an EOEM opportunity for electrical contractors. Here’s what’s driving the shift, what separates those who succeed, and what to ask before taking the leap.

Mary Derrick, VP of EOEM and Power Applications at Schneider Electric, beside her quote on why contractors are uniquely positioned

Electrical contractors have always been close to the customer, the application, and the realities of installation. Today, those strengths are opening a new path for growth: expanding into electrical original equipment manufacturing, or EOEM.

The timing isn’t accidental. Demand from data centers, critical infrastructure, and electrification projects is increasing the need for custom, higher-reliability electrical equipment. At the same time, customers expect more speed, flexibility and coordination across engineering, manufacturing and installation than ever before. In my work with contractors, EOEMs, integrators and partners across North America, I see a growing number of firms responding by adding manufacturing to their installation business.

It’s a real opportunity, but it isn’t the right move for every contractor. The firms that succeed treat manufacturing as a distinct business with its own engineering, quality, and supply chain demands, and they start from a clear sense of where they can win.

What we mean by EOEM

An EOEM is a company with the capability to manufacture electrical distribution equipment. That can include switchboards, panelboards, low-voltage and medium-voltage switchgear, controls, and prefabricated power assemblies. You’ll also hear terms like OEM, panel builder, power equipment manufacturer, and custom equipment manufacturer used for the same general idea.

The defining feature is the engineering, not the product category. An EOEM takes customer and application requirements, translates them into a compliant, optimized design, and then builds and delivers that solution under its own name. Simply assembling or reselling equipment doesn’t meet that bar, a point I’ll return to later.

What makes this especially relevant for contractors now is convergence. Manufacturing, engineering, configuration, and installation were once handled by separate players in sequence. Increasingly, customers expect them to work as a single, coordinated effort.

The market forces behind the shift

Several trends are converging at once:

Data center and critical infrastructure demand. The data center boom, driven heavily by hyperscalers, has sharply increased the need for custom, high-reliability electrical equipment. Grid, industrial, and other critical infrastructure work is adding to that demand.

A premium on speed and responsiveness. These customers aren’t only looking for more capacity. They value local responsiveness, flexibility and speed to market, and they want partners who can engineer, manufacture and deliver around their specific requirements.

Faster innovation cycles. Energy demand from data centers is pushing manufacturers to bring new solutions to market at a pace the industry hasn’t historically seen. Equipment is increasingly custom-designed around operating requirements rather than pulled from a catalog. Even established EOEMs that built their businesses in sectors like oil and gas are adapting as they move into data center work.

Integration of individual products. Customers no longer want components from separate silos. They want integrated systems spanning low-voltage switchboards, medium-voltage switchgear, controls, and prefab. In prefabricated solutions especially, manufacturing and installation effectively have to become one process. When manufactured equipment isn’t well coordinated with the installer’s work, the results can be costly for everyone.

Taken together, these shifts reward companies that can see a project from design to commissioning, which is exactly where contractors already operate.

Build on the advantages contractors already have

Contractors who move into equipment manufacturing don’t start from zero. They have a unique advantage because they already understand the customer, the application, and the realities of installation. They work closely with engineers, understand how equipment is applied, installed, and commissioned, and see firsthand how customer requirements are changing.

That perspective translates directly into better equipment. A contractor who has lived with the consequences of design decisions in the field can engineer equipment that is easier to install, better aligned with the application, and more responsive to the customer’s schedule.

Adding engineering, manufacturing, prefab, and certification capability lets a contractor deliver a finished system under its own brand. That changes the business in several ways:

  • Broader relationships with existing customers, who can source more of the solution from a single, trusted partner.
  • New project opportunities that a pure installation business wouldn’t reach.
  • Recurring, lifecycle revenue from retrofits, upgrades, modernization, and service.

This hybrid solution-provider model lets contractors capture more of the value they already help create, rather than participating in a single phase of the project.

What successful EOEMs have in common

The EOEM space is crowded, and not every contractor that enters it gains traction. The companies that succeed tend to share four characteristics.

They know where they’re differentiated. Winners can clearly state who their target customer is and why that customer should choose them. Those that struggle often decide to “get into manufacturing” without a defined value proposition or assume that assembling or reselling equipment is enough. It isn’t. Customers need meaningful engineering and integration behind the finished solution, and the right offer builds on a contractor’s specific strengths rather than trying to cover every capability at once.

They run it as a separate business. Manufacturing is fundamentally different from contracting. Successful firms build distinct engineering teams, service teams, systems, and processes, and they hire specifically for the manufacturing side rather than borrowing capacity from field operations.

They invest in engineering and certification. Whether a company starts with UL 891 switchboards or another segment of the market, it needs in-house engineers who can interpret UL requirements and produce compliant designs, along with a solid working relationship with UL. This is a new skill set for most contractors, and it’s non-negotiable. The strongest teams take a customer-first approach, starting with requirements and designing around them.

They treat quality as a core discipline. In my conversations with large end users, the quality of some prefab solutions they receive today is a consistent frustration. Customer relationships may open the door, but they won’t survive a late or flawed delivery. Firms that pair consistent quality with dependable supply and execution stand out quickly.

Building supply chain resilience

Supply chain is one of the hardest parts of the business right now. Demand is high across the market, and upstream constraints affect nearly every component category, from circuit breakers to surge protective devices, metering, and relays.

For an EOEM, resilience is part of the value proposition. A customer choosing a manufacturing partner is also choosing that partner’s ability to deliver on schedule.

That makes planning a core competency. Contractors entering the space need disciplined internal planning and transparent relationships with upstream suppliers. That means understanding realistic lead times, forecasting quantities accurately, and being clear about what they need from each relationship.

Many contractors find it helpful to work with an established manufacturer that already operates in this space. An experienced partner can support design decisions, UL strategy, and component supply at the same time, which shortens the learning curve considerably.

Collaboration is the competitive advantage

Roles that used to be distinct are converging. Distributors are moving into panel building, manufacturers are developing broader solutions, and contractors are adding manufacturing. The result is a hybrid model in which traditional boundaries matter less than capabilities.

End users are driving this change. They need responsive partners who understand the full spectrum, from the application to the right solution to execution and installation.

In this environment, every player needs to be clear about the value it brings and how it works with others. Relationships among manufacturers, distributors, contractors and EOEMs are becoming more collaborative, with shared access to opportunities, joint work on technical solutions and transparency around supply.

Commercial models are evolving too. Partners are increasingly sorting out which part of a job each does best, and in some cases sharing risk to win an opportunity together. No single capability is enough on its own. The companies best positioned for growth will be clear about where they lead and where collaboration can reduce risk or improve the customer outcome.

Start focused, then scale

Data centers are an important market for custom power distribution and prefabricated solutions, but they’re far from the only one. Infrastructure, industrial applications and buildings all offer room for growth.

The right path depends on where a contractor already has customer relationships, application knowledge, and the ability to differentiate. That argues for starting with focus rather than scale. Enter the markets and applications you already understand, build the engineering, certification, quality and supply capabilities to deliver consistently, and then expand from a position of demonstrated strength.

Is it right for your business? Questions to ask first

Any contractor considering this move should start with an honest assessment of its right to win. Useful questions include:

  • Which customers or industries do we understand better than our competitors?
  • What problems can we solve that the market isn’t solving well today?
  • Can we invest in dedicated engineering, manufacturing, and service teams that operate separately from our contracting business?
  • Which certifications and UL competencies will our chosen equipment lines require?
  • Can we secure a reliable stream of components, and do we have manufacturer relationships to support design and supply?
  • Are we prepared to operate with the quality discipline these end users demand?

You don’t have to go it alone. Established manufacturers and other experienced partners can help contractors evaluate certification needs, set engineering and design approaches, plan component supply, and build the relationships needed to enter the market responsibly. For contractors with a clear point of differentiation and the commitment to build it properly, the EOEM path can turn installation expertise into a much larger role in the market.

Listen to the full EC&M On Air episode, “Powering Growth: The EOEM Opportunity for Electrical Contractors,” to hear the complete conversation.

Ready to explore your EOEM opportunity? Discover tools, resources, and partnership support to help you design, build, and grow at se.com/us/eoems.

Add a comment

All fields are required.