Speed to power: Why Energy Parks need a new delivery model

AI is changing the timeline for data center development. Projects that once had plenty of time to plan for future power demand are now racing to bring capacity online. But in many markets, getting a new grid connection can take years.

Energy Parks offer a way around that constraint by bringing generation and power infrastructure closer to the load. But solving the grid-connection problem doesn’t automatically solve the power delivery problem.

Generating power independently may bypass the wait for utility capacity. But it doesn’t eliminate the engineering, manufacturing, supply-chain, and construction constraints involved in delivering what is effectively a city-scale electrical system.

Energy Parks are changing how developers think about getting power to data centers.
Energy Parks are changing how developers think about getting power to data centers.

An Energy Park isn’t simply a power plant added to a data center. It is a tightly integrated infrastructure system in which generation, distribution, controls, mechanical systems, digital technologies, and other components must work together from day one as one system. Delivering that system quickly requires a different way of working across the project.

The challenge isn’t simply generating power faster. It’s delivering the entire power system faster—and that requires a fundamentally different project delivery model.

Energy Parks require a new delivery model

Traditional construction tends to move linearly: design to procurement, procurement to construction, and construction to commissioning. That model works poorly when generation, distribution, controls, automation, mechanical systems, and commissioning are tightly interconnected.

Each participant can move quickly within their own scope and still slow the overall project. A decision in one discipline can create costs, delays, or lost functionality elsewhere. By the time those conflicts appear in the field, they’re typically far more expensive and disruptive to resolve.

A project of this scale requires the principal participants at the table much earlier, before individual teams advance too far with their own specifications. That means confirming use cases, technical requirements, interfaces, and future operating to shape the design.

The objective isn’t to centralize every decision; it’s to make sure the right people can see the decisions that affect them. That means shared project information, clearly defined outcomes, and a common understanding of how decisions affect the overall system.

How digital twins can reduce delays

One of the clearest ways to accelerate delivery is to find problems early in the process, when they are easier and less expensive to fix.

Ideally, a design conflict is identified in the digital model before construction begins. If it escapes the model, it should be caught during engineering review or factory integration and testing. Discovering it during site construction is considerably more disruptive. Discovering it after the facility becomes operational is even worse.

Digital twins and shared design environments can give project participants a common view of physical and electrical systems. Revisions, interface decisions, design changes, and exceptions become visible to everyone they affect. Instead of relying on disconnected drawings and assumptions, teams can evaluate decisions against the complete system and its intended operating outcomes.

How prefabrication and modular construction accelerate Energy Park delivery

Industrialized delivery provides the physical counterpart to that digital collaboration.

Prefabricated assemblies, switchgear skids, e-houses, and other modular systems allow more engineering, integration, and testing to occur in controlled environments before equipment reaches the site. The site then becomes a place for assembly and commissioning rather than custom construction and problem-solving.

This also requires the industry to reconsider its long-standing preference for highly bespoke designs. Standardized architectures can help manufacturers forecast demand, secure capacity, simplify supply chains, and improve delivery with each deployment—while still accommodating customer-specific requirements.

The goal isn’t to make every Energy Park identical. It’s to standardize what can be standardized while preserving flexibility where it matters. Customer-specific requirements can increasingly be met through validated, interoperable systems adapted to each project.

Why Energy Park projects need new commercial and contracting models

Technology and better project processes can help teams work faster. But they can only go so far if the commercial structure still rewards each participant for optimizing their own scope rather than the project as a whole.

Construction contracts often focus on individual scopes, deadlines, and penalties. That can encourage participants to protect their own interests, even when doing so creates delay or rework elsewhere.

A useful place to start is with a simple question: What does the whole project need next?

  • Agree on milestones that matter to everyone. Finishing one scope early isn’t progress if the next team can’t use it.
  • Create shared incentives. If mechanical, electrical, and systems integration must come together, part of the incentive should depend on achieving that milestone together.
  • Work from the same information. Everyone should have a clear view of design status, changes, dependencies, and unresolved risks.

No single commercial formula fits every project. But the principle is simple: an early milestone only creates value if it unlocks progress for everyone downstream. The goal is to reward teams for moving the system forward, not for winning their individual scope.

How a more integrated delivery model can improve speed to power

Energy Parks can solve one of the biggest barriers to AI infrastructure: access to power. But getting power to the campus faster is only half the challenge. That advantage can disappear if we deliver the infrastructure the same way we’ve delivered conventional projects for decades.

Speed to power isn’t just about finding or generating more electricity. It’s about finding a better way to turn power into an operating data center. How we deliver that infrastructure will matter just as much as what we build.

How is your organization navigating grid delays and speed-to-power constraints? Contact our team to learn how integrated project delivery can help compress timelines, reduce risk, and accelerate your path to power.

Add a comment

All fields are required.