How to successfully electrify a fleet with Schneider Electric DC Fast Charging Solutions

The electrification of bus and commercial vehicle fleets has become a strategic priority for local authorities and transport operators. Balancing regulatory requirements, operational demands and cost efficiency requires more than simply replacing diesel vehicles with electric alternatives.

A successful transition depends on an integrated approach that combines electrical infrastructure, charging technology, energy management and long-term support services.

This is where Schneider Electric DC Fast Charging Solutions provide a clear advantage. By delivering an end-to-end ecosystem covering power distribution, fast charging, depot energy management and lifecycle services, Schneider Electric helps operators accelerate fleet electrification while maintaining reliability, efficiency and scalability.

Future-ready electrical infrastructure for Schneider Electric DC Fast Charging Solutions

Every successful electrification project begins with a reliable and properly dimensioned electrical infrastructure. Schneider Electric designs and deploys power distribution systems that:

  • Support the high-power requirements of Schneider Electric DC Fast Charging Solutions.
  • Ensure continuous operation across the depot.
  • Anticipate future fleet expansion and increasing energy demand.
  • Comply with local regulations and utility requirements worldwide.
  • Deliver sustainability benefits through compact, SF6-free technologies.

This scalable, future-ready architecture protects long-term investments while enabling operators to grow their charging capacity without significant infrastructure redesigns.

Schneider Electric DC Fast Charging Solutions designed for real depot operations

With a complete charging portfolio ranging from 60 kW to 720 kW, Schneider Electric DC Fast Charging Solutions can support a wide variety of depot configurations, including all-in-one chargers, decentralised architectures and overhead charging systems.

For demanding fleet operations, the Schneider Electric DC 720 charger delivers up to 600 A in Boost Mode, enabling ultra-fast charging during critical operational windows. With charging efficiency of up to 97%, operators can also reduce energy losses and lower operating costs.

With a charging portfolio ranging from 60 kW to 720 kW, Schneider Electric Charging Solutions can support a wide variety of depot configurations
With a charging portfolio ranging from 60 kW to 720 kW, Schneider Electric Charging Solutions can support a wide variety of depot configurations

Designed specifically for electric bus and commercial vehicle depots, Schneider Electric DC Fast Charging Solutions offer:

  • Cable lengths of up to 10 metres.
  • VDV 261 compliance.
  • B2B Toggle Wake-Up functionality.
  • Dynamic simultaneous charging.
  • Multiple authentication methods, including Autocharge and ISO 15118.

Built for reliability, these charging solutions operate in temperatures ranging from -30°C to +55°C (with derating above 50°C) and feature an IP55 protection rating.

Advanced embedded sensors continuously monitor system health, while CSMS notifications provide immediate alerts in the event of power interruptions. A dedicated remote maintenance platform enables rapid diagnostics and issue resolution, helping operators maximise uptime and maintain dependable charging operations.

Although eBus and eTruck fleets share many charging requirements, their operational patterns differ significantly. Dedicated Schneider Electric application notes help operators design depot infrastructure and charging strategies that address the specific needs of each use case.

Discover Schneider Electric eBus and eTruck depot application note here.

DELMS: Maximising the value of Schneider Electric DC Fast Charging Solutions

At the heart of every high-performing electric depot is intelligent energy management. Schneider Electric’s Depot Energy & Load Management System (DELMS) serves as the central intelligence layer behind Schneider Electric DC Fast Charging Solutions, ensuring reliable charging operations while optimising energy costs and sustainability performance.

DELMS guarantees fleet readiness by managing charging schedules, vehicle state-of-charge targets and site electrical constraints in real time. By integrating seamlessly with fleet management platforms such as VDV 463, the system aligns vehicle charging with operational schedules while respecting grid limitations.

Through advanced monitoring and control capabilities, DELMS helps maintain charger and electrical infrastructure availability above 98%.

Software solutions like EV Charging Expert and the Dynamic Load Management System (DELMS) help operators to optimise the charging processes
Software solutions like EV Charging Expert (shown in the picture) and the Dynamic Load Management System (DELMS) help operators to optimise the charging processes

With a charging portfolio ranging from 60 kW to 720 kW, Schneider Electric Charging Solutions can support a wide variety of depot configurations

Optimising energy costs

Beyond operational reliability, DELMS enables operators to maximise the value of their Schneider Electric DC Fast Charging Solutions through:

  • Smart charging optimisation.
  • Time-of-use tariff management.
  • Integration with battery energy storage systems.
  • Coordination with local renewable generation.
  • Peak demand reduction.

This intelligent approach reduces exposure to electricity price volatility while ensuring charging performance remains aligned with operational priorities.

Supporting sustainable fleet operations

DELMS also supports broader sustainability objectives. Combined with Schneider Electric’s advisory services, operators can integrate renewable electricity procurement strategies, including Power Purchase Agreements (PPAs), into everyday depot operations.

By aligning Schneider Electric DC Fast Charging Solutions with renewable energy availability and distributed energy resources, operators can lower carbon emissions, improve energy resilience and support long-term decarbonisation goals.

Reducing operational and maintenance costs

Remote diagnostics, monitoring and control capabilities enable operators to manage charging infrastructure more efficiently. Many issues can be identified and resolved remotely, reducing unnecessary site visits, lowering maintenance costs and improving overall depot resilience.

Lifecycle services supporting Schneider Electric DC Fast Charging Solutions

Electrification does not end at commissioning. To ensure reliable, efficient and durable operation throughout the project lifecycle, Schneider Electric provides a comprehensive portfolio of support services.

Engineering and planning

From the earliest project stages, Schneider Electric conducts detailed engineering studies and infrastructure assessments to ensure charging systems are correctly sized and integrated with existing electrical assets.

Commissioning and deployment

During implementation, Schneider Electric manages testing and commissioning to ensure all components, including power distribution, chargers and supervisory systems, perform according to operational requirements.

Ongoing maintenance and support

Following deployment, operators benefit from expert maintenance services, remote monitoring capabilities and technical support designed to maximise infrastructure availability and minimise operational disruption.

Future expansion

As fleets grow, Schneider Electric provides guidance and support for capacity expansion, infrastructure upgrades and evolving energy strategies. This allows operators to scale their Schneider Electric DC Fast Charging Solutions with confidence.

Reliable and safe solutions for operators with the end-to-end approach from Schneider Electric
Reliable and safe solutions for operators with the end-to-end approach from Schneider Electric

Why choose Schneider Electric DC Fast Charging Solutions?

Choosing an end-to-end Schneider Electric approach delivers significant advantages:

  • A single point of contact throughout the project lifecycle.
  • A fully integrated charging and energy management ecosystem.
  • Improved control of energy consumption and operating costs.
  • Safer, more reliable and more efficient depot operations.
  • Scalable infrastructure designed for future fleet growth.
  • Coordinated site-wide services and support.

Rather than assembling multiple disconnected technologies, operators benefit from a unified ecosystem built around Schneider Electric DC Fast Charging Solutions, helping them achieve reliable fleet operations, optimise energy performance and prepare for the transport networks of the future.

Learn more about Schneider Electric DC Fast Charging Solutions in our Schneider StarCharge Fast page.

Add a comment

All fields are required.