Utilities have long relied on both CAD-based graphic design tools and GIS-based systems to plan, design, and operate their electric networks. Historically, these two worlds have operated in parallel—CAD excelling at detailed drafting and visualization, and GIS serving as the system of record for spatially accurate asset data. However, modern workflows demand tighter integration. When CAD-based graphic work design is paired with GIS-based graphic work design like EcoStruxure ArcFM Design, utilities can unlock a powerful, unified approach that combines speed, precision, and operational awareness.
The strengths of CAD-based graphic work design

CAD tools are widely recognized for their strengths in detailed engineering design. They enable designers to quickly draft complex layouts, create visually rich representations, and iterate on designs with flexibility. CAD-based solutions are highlighted for their ability to drive efficient design workflows when users are already proficient with these tools, particularly in scenarios requiring rapid adjustments or highly customized layouts.
Designers benefit from:
- High-performance drafting tools
- Familiar workflows for engineering teams
- Precision in geometry and visual detail
- Rapid iteration during early design phases
These capabilities make CAD an ideal environment for conceptual design and fine-grained graphic work. However, CAD environments often lack deep integration with enterprise GIS systems, financial and inventory systems like Maximo and SAP, which can lead to data silos and additional effort when transferring designs into operational systems as well as a lag in process between designs and as-builts, introducing unnecessary errors and potential safety risks. Additionally, many CAD platforms are burdened with an overwhelming number of features and buttons, many of which are rarely used in typical workflows. This complexity creates a steep learning curve for new users and can reduce overall productivity, as engineers must spend significant time navigating the interface and mastering tools that may not be essential to their day-to-day tasks.
The power of EcoStruxure ArcFM design

ArcFM builds on Esri’s ArcGIS platform to provide a GIS-native design environment tailored for utilities. It goes beyond traditional drafting by embedding design directly into the system of record, ensuring that every design is inherently tied to real-world spatial and asset data.
Key capabilities include:
- Direct integration with GIS data models
- Direct integration with work management systems
- Connectivity-aware design and validation
- Seamless alignment with enterprise systems, including ADMS
- Advanced design lifecycle management
- This GIS-centric approach ensures that designs are not just visually accurate but also operationally valid and ready for downstream applications.
Where CAD and EcoStruxure ArcFM work best together
Rather than replacing CAD, EcoStruxure ArcFM Design complements it. The combination of both tools creates a best-of-breed workflow that leverages the strengths of each.
1. Conceptual design in CAD, operational design in GIS
CAD tools can be used to create initial layouts and explore design options quickly. Once a concept is validated, it can be brought into EcoStruxure ArcFM for integration into the GIS model, where connectivity, phasing, and standards are enforced.
2. Complex urban projects
In dense urban environments, designers often require detailed drafting capabilities to work around constraints. CAD enables this level of detail, while EcoStruxure ArcFM ensures the final design aligns with the network model and operational requirements.
3. Stakeholder visualization and communication
CAD-generated visuals are often more intuitive for sharing with external stakeholders, such as contractors or city planners. EcoStruxure ArcFM then ensures that these designs translate accurately into the system of record without rework or data loss.
Design standardization and compliance
EcoStruxure ArcFM enforces utility standards and rules. CAD designs can be refined and validated within ArcFM to ensure compliance before construction begins.
How EcoStruxure ArcFM design outperforms CAD-based design tools

While CAD-based provide strong drafting capabilities, EcoStruxure ArcFM offers significant advantages that make it the superior platform for utility design.
1. Managing phased and proposed designs
EcoStruxure ArcFM supports phased design workflows, allowing large projects to be broken into manageable segments. These systems can be designed, tracked, and completed independently. This is especially valuable for large neighborhoods, where infrastructure can be planned and energized in phases. This enables incremental service activation while remaining work continues.
Coming in 2027, ArcFM will support proposed designs within the GIS environment. This “pre-push” capability allows teams to evaluate and refine designs before committing them to the operational system. It supports scenario planning and reduces risk by ensuring only validated designs are implemented.
2. Rebase functionality
One of the standout features of ArcFM is rebase. ArcFM allows designs to stay synchronized with the latest GIS data. If the underlying network changes during the design process, designers can rebase their work rather than starting over. This dramatically reduces rework and ensures designs remain accurate in dynamic environments.
3. Native GIS integration
Unlike CAD-based tools that require data translation, ArcFM operates natively within the GIS. This eliminates duplication, reduces errors, and ensures a single source of truth. Every design element is immediately connected to the broader network model.
4. Native operational insights and network intelligence
EcoStruxure ArcFM connects seamlessly with Advanced Distribution Management Systems (ADMS). This enables operational feedback to inform design decisions. Designers can understand how changes will impact load, reliability, and switching operations—something CAD tools alone cannot provide. Network validation of connectivity, etc.
5. End-to-end design lifecycle management
EcoStruxure ArcFM supports the full lifecycle from planning to construction to as-built updates. This continuity ensures that designs are not lost in translation and that all stakeholders work from consistent, up-to-date information.
6. Innovative tools to increase productivity
EcoStruxure ArcFM enhances productivity with powerful core design tools and a simplified, intuitive interface that minimizes distractions. Context-aware features, snap guides, and configurable search accelerate workflows, while automated compatibility checks and unit assignments reduce errors and manual effort. Auto-recovery safeguards progress, and full offline field design support ensures uninterrupted work—enabling teams to design efficiently from concept through execution.
7. Less training, faster adoption
Design further simplifies the user experience by offering a more intuitive and streamlined interface compared to traditional CAD platforms like CAD. With fewer unnecessary buttons and a focus on commonly used workflows, users can quickly become productive without needing extensive training. Its streamlined workflows and intuitive user interface reduce the learning curve, allowing both new and experienced designers to navigate the system with ease. As a result, teams can spend less time learning complex tools and more time focusing on delivering accurate, high-quality designs.
8. Fully enabled offline field design capabilities
EcoStruxure ArcFM enables full offline field design, allowing users to capture, edit, and validate designs without requiring connectivity. Teams can perform staking in the field—such as placing and recording pole locations or assets—to initiate designs directly on site and ensure accurate, real-world alignment. Once reconnected, all collected data and updates seamlessly sync back to the system for continued design and collaboration
Leverages existing engineering analysis tooling
EcoStruxure ArcFM includes embedded engineering analysis tools focused on secondary circuit analysis and real-time design feedback, such as load flow (kVA demand and power flow), voltage drop, voltage flicker, and fault current calculations to support “what‑if” scenario evaluation. Additionally, the application continuously recalculates network conditions (e.g., voltage, load balance, and transfer loading) as designers edit the system, giving immediate analytical insight during the design process.
Beyond those tools, instead of reinventing the wheel and creating embedded tools that might compete with tools that have already been habituated in the design process, EcoStruxure ArcFM leverages those existing tools through integration.
Conclusion
The future of utility design lies in integration—not replacement. CAD-based graphic work design and GIS-based EcoStruxure ArcFM Design each bring unique strengths to the table. When used together, they create a workflow that is both flexible and robust.
CAD empowers designers with speed and precision in drafting, while EcoStruxure ArcFM Design ensures those designs are spatially accurate, operationally valid, and fully integrated into the enterprise GIS. With advanced capabilities such as pre-push design management, rebase, native GIS integration, and ADMS connectivity, EcoStruxure ArcFM stands out as a superior platform compared to traditional tools like AUD.
By embracing a hybrid approach, utilities can improve efficiency, reduce errors, and deliver better outcomes—ultimately building smarter, more resilient networks.
See CAD and EcoStruxure ArcFM Design in action together with a complete end-to-end workflow for energizing a new utility network.
Learn more at Esri User Conference 2026 in San Diego! Visit us July 13-17, alongside thousands of GIS, utility, and infrastructure leaders.
We’re excited to connect with customers and partners to discuss how location intelligence, automation, and data integration are helping utilities modernize operations, improve resiliency, and make smarter decisions.
If you’ll be attending Esri UC, stop by our booth 619! Learn more on how EcoStruxure ArcFM orchestrates and connects the grid from planned to operational.
Add a comment