5 ways Schneider Electric is delivering microgrids faster (and more affordably)

As energy reliability and flexibility become top priorities, more organizations are turning to decentralized energy solutions. 

Microgrids offer a powerful path forward – but delivering them hasn’t always been straightforward. Projects can quickly become highly customized, slowing deployment and introducing unnecessary complexity.

That’s starting to change. 

Schneider Electric is rethinking how microgrids are designed and deployed – making them more standardized, faster to implement, and easier to scale. 

Here are five ways Schneider Electric is accelerating microgrid deployment today: 

1.Testing and validation in a lab environment

Microgrid performance can be established before a system ever reaches the field. 

At Schneider Electric’s Microgrid Testing & Validation Lab in Andover, MA, systems are tested in a high-power environment as a fully integrated solution – not as individual components. Real-world scenarios are replicated in advance, from controls behavior to communications across assets. 

By the time the equipment reaches the site, the system has already been validated as a complete solution. Commissioning becomes faster and more predictable, with systems operational in as little as two weeks. 

2. Standardized, repeatable designs 

Every microgrid is unique – but the outcomes they’re designed to deliver are not.  

Focusing on common objectives like resiliency, cost optimization, and capacity expansion allows designs to be standardized around what matters most. Instead of reinventing the system each time, teams can build on proven architectures that have already been engineered and tested.  

That consistency streamlines design, reduces variability, and makes it easier to scale projects across sites. 

3. Integrated electrical and control systems 

Microgrid success depends on how well electrical infrastructure and controls work together.  

Schneider Electric designs these as a single, integrated system – from switchgear to edge control to cloud-based platforms. This unified architecture ensures interoperability is built in from the start, rather than addressed later through complex integration efforts. 

The result is a system that operates seamlessly, reducing commissioning effort and accelerating time to value. 

4. Front-loading design to accelerate delivery 

Microgrid performance is defined early – by how well system behavior, controls, and infrastructure are aligned from the start. Schneider Electric brings this alignment forward in the process, using feasibility studies and early design definition to establish clear functional intent before implementation begins. 

With a fully aligned system architecture and pre-validated designs, projects move from installation to energization more smoothly – reducing rework, accelerating commissioning, and delivering faster time to value. 

5. Industry-led collaboration: The accelerating resilient infrastructure initiative 

Deploying microgrids at scale requires more than technology – it requires a coordinated ecosystem. 

Many customers face the same barriers: high upfront costs, complex procurement, and a lack of technical expertise on staff. To address this, Schneider Electric launched an industry-wide consortium, Accelerating Resilient Infrastructure (ARI) Initiative. ARI’s ambition is to pair over $7.5 billion in private clean energy capital with a national network of 40+ developers and technology partners to accelerate resilient energy projects.  

Through ARI, microgrids can be deployed at critical facilities using an Energy-as-a-Service (EaaS) model, transferring ownership and operational risk to the developer. The result is reduced risk, faster deployment, and more resilient infrastructure where it is needed most.  

Microgrids have moved beyond early adoption – they are now a practical and scalable solution for delivering resilience, flexibility, and energy cost optimization.  

What’s changing is not just the technology, but how these systems are designed and deployed. By standardizing architectures, validating systems upfront, and leveraging alternative delivery models, projects become faster, more predictable, and easier to replicate.  

The result is a shift from one-off, complex installations to a more streamlined and scalable model for delivering resilient energy infrastructure – exactly where and when it’s needed.  

About the author

Annamarie Martin, Microgrid Channel Partner Enablement

Annamarie Martin is responsible for Microgrid Channel Partner Enablement at Schneider Electric, where she leads partner training initiatives and drives channel marketing to support the deployment of scalable microgrid solutions across North America. In this role, she works closely with partners to build technical capabilities, align delivery approaches, and bring standardized microgrid architectures to market more efficiently.
 
She brings a strong technical foundation to her work, having previously served as a Microgrid Systems Test Engineer in Schneider Electric’s Microgrid Testing & Validation Lab. There, she was responsible for system-level validation of integrated microgrid architectures, with a focus on controls, communications, and overall system performance.
 
Prior to joining Schneider Electric, Annamarie supported distributed energy resource (DER) integration efforts at the Electric Power Research Institute (EPRI) as a student employee, where she worked on advanced simulation and hardware-in-the-loop testing for grid-edge technologies.
 
Annamarie holds both Bachelor’s and Master’s degrees in Mechanical Engineering from the Georgia Institute of Technology, with a concentration in energy systems.

Add a comment

All fields are required.