Public leaders know the stakes: Energy costs are surging, demand is at an all-time high, and deferred maintenance is straining public budgets. They also know the solution is to modernize energy infrastructure.
The how of this transition is critical. Traditional, slow-moving project delivery approaches can take years and have become a liability. Public-Private Partnerships (P3s) offer the streamlined mechanism agencies need to bypass bureaucratic friction. By leveraging a P3 collaborative framework, leaders can execute a sprint strategy that accelerates delivery without sacrificing long-term accountability.
To help navigate P3 options, Schneider Electric developed a P3 Playbook centered on three models: ESPC, PPA, and EaaS. This is the fifth in a series of articles to help public leaders learn about the benefits of P3s. Other articles in the series are:
- Strategic Financing is Accelerating Critical Energy Infrastructure Projects
- Why P3s Are the Financial Answer to Limited Public Capital
- Selecting the Right Energy P3 Model
- Bridging the Expertise Gap to Successfully Deploy P3 Models

Taking years off delivery time for significant projects
Public agencies have an opportunity to significantly reduce the time between project inception and financial close. This isn’t about cutting corners; it’s about eliminating the dead time inherent in traditional design-bid-build cycles while retaining a fair, competitive, and transparent procurement process. By integrating financing, design, and operations into a single procurement, agencies may be able to bypass years of sequential approvals. In fact, studies show P3 projects can reduce schedule overruns to less than 1%, compared to 30–38% for traditional design-bid-build—saving years in delivery.
Leverage master agreements to scale faster
One of the most effective tools for rapid deployment is the Master Energy Services Agreement (MESA). Think of a MESA as a framework for the future.
Instead of negotiating a separate, complex contract for every individual building or microgrid, a public entity establishes a single Master Agreement that sets the core legal, financial, and performance terms. Individual projects are then added over time as schedules or work orders under that master umbrella.
The MESA advantage:
Reduced legal friction: Terms and conditions are settled upfront, meaning subsequent projects don’t require starting from scratch with legal counsel.
Portfolio scalability: It allows an agency to start with a pilot project and then rapidly scale across an entire portfolio of assets.
Streamlined approvals: Governing boards only need to approve the master framework once, with subsequent projects following a pre-defined pathway.
3 ways to bypass red tape to fast-track your project
For agencies that need to move even faster, there are three express lanes to consider:
Piggybacking: This allows one public entity to utilize a contract that was already competitively awarded by another public agency for similar services. If a neighboring city or a state agency has already vetted a partner and negotiated terms, you may be able to piggyback on that existing contract, saving months of solicitation time.
Cooperative purchasing: By joining a public purchasing cooperative, agencies can leverage pre-vetted contracts and the collective buying power of multiple entities. This ensures competitive pricing and regulatory compliance without the administrative burden of running a solo RFP.
Progressive P3: In a Progressive P3, a partner is selected early based on qualifications rather than a final fixed price. The public agency and the partner then collaborate to define the project scope, design, and cost in a transparent process. This model is ideal for complex, innovative projects such as multi-asset microgrids where the full scope is difficult to define at the outset.
3 steps to ensure long-term oversight and accountability
Speed must never come at the expense of stewardship. Because P3 and EaaS agreements often span 15 to 25 years, long-term governance is essential. Accountability must be the foundation of any partnership. To ensure success over the decades, public leaders should:
Define clear KPIs: Establish Key Performance Indicators (KPIs) such as microgrid uptime or specific carbon reduction targets before selecting a partner.
Incentivize performance: Ensure that the partner’s payment is directly tied to meeting these KPIs. If the infrastructure doesn’t perform, the public entity doesn’t pay full price.
Built-in re-openers: The world will change over the next 20 years. Include contract provisions that allow for adjustments if market conditions, technology, or laws shift significantly.
Download our P3 Playbook for a roadmap to smarter infrastructure delivery
Public sector leaders can transform their infrastructure from a liability into a strategic asset. Achieving energy efficiency, deferred maintenance goals, and resilience starts with strategic financing and expedited procurement. The technology exists, and the financing is ready. The final step is action. Download our P3 Playbook to learn more about P3s.
Add a comment