Powering what’s next: How a future-ready grid will accelerate Europe’s energy transition

Future-Ready Grid

Europe’s energy transition is in full swing—and it’s not just the ambitious climate targets setting the pace. Renewable capacity is growing at a record pace, digital technologies are reshaping every industry, and electrification is expanding rapidly across all sectors.

Yes, despite this exciting momentum, there’s a significant constraint on decarbonization—the electricity grid.

While high electricity prices are indeed hindering the growth of renewable energy for both consumers and industry, grid capacity, flexibility, and the infrastructure itself are not keeping pace with advancing technologies and industry needs.  

The solution? Grid modernization and expansion.

Europe’s current state of grid constraints

Grid constraints are the primary barrier to scaling renewables.

Since 2021, European electricity markets have experienced sharp price volatility. A major driver is the rapid introduction of renewable energy capacity into systems that lack sufficient flexibility, capacity, and grid reinforcement.

Research reinforces this reality. Countries with a high share of renewable energy but limited grid adaptability experience more frequent and extreme price swings. At the same time, system operators are forced to curtail renewables when the grid cannot absorb or transport generation, triggering compensation payments that ultimately feed into electricity prices. Germany alone paid €20.9 billion in renewable energy compensation in 2024.

The challenge posed by grid limitations is clear in the energy transition project pipeline. For instance, over 1,700 GW of renewable and hybrid deployments are currently awaiting grid connection across Europe, with many delayed by limited access and inefficient allocation of network capacity. 

Planning gaps also worsen the challenge. A lack of grid capacity hampers clean energy deployment, especially for solar, with an expected 205 GW shortfall by 2030. 

Here’s the reality of what happens when aging infrastructure cannot keep up with demand or generation patterns.

For example, the 2025 Iberian power blackout, described as “the most significant power system event…in over two decades,” cut electricity to mainland Spain and Portugal for approximately 10 hours, and in some areas, even longer.

Waiting for the grid to fail is not an option. Now more than ever, there is an urgent need to accelerate investments in grid modernization and expansion.

Smart energy tech is turbocharging Europe’s transition

While grid structure and capacity are pieces of the puzzle, there are four additional converging trends adding to Europe’s decarbonization challenge:

  1. Industrial and process electrification
    Energy-intensive sectors such as chemicals and steel, along with advanced manufacturing and semiconductors, continue to reshape their electricity needs. While chemicals and steel are electrifying more of their processes, semiconductor manufacturing and other advanced production facilities are driving sharply higher electricity intensity and continuous baseload demand. In advanced manufacturing, such as battery production and semiconductor fabrication, a reliable, high-quality power supply is essential, as even minor disturbances can result in significant production losses. These industries rely on grid reliability and increasingly on modernization to remain competitive.
  2. Building electrification
    Electrifying residential and commercial heating, especially with heat pumps, is a key part of EU climate policy. These devices transfer large amounts of heat to the distribution grids, especially in winter when demand is at its highest. This calls for upgraded local networks, demand-response systems, and distributed storage solutions, none of which can be implemented overnight.
  3. Electric vehicles (EVs)
    EV adoption increases electricity consumption and creates new, often localized, peak-demand patterns. Expanding smart meter deployment and integrating EVs into demand response systems can mitigate load spikes, but only if grid infrastructure is upgraded to support bidirectional charging and flexible tariff mechanisms. Smart meters, for example, can reduce peak loads and household energy consumption by 2–10%. Additionally, our Canalis for EV solution provides the foundation for flexible, scalable parking infrastructure, whether for a smaller lot or a fleet depot.  It’s a robust, prefabricated, enclosed busway system that not only speeds outdoor installation but also reduces the risk of cable theft and environmental damage.
  4. Data centers
    This may be the fastest-growing source of new electricity demand in Europe. Data centers consumed roughly 1.5% of the world’s electricity and are projected to more than double by 2030. High-density AI workloads are driving power-density requirements, making grid availability and reliability decisive factors in siting these facilities.  For data centers, our Canalis KN busbar trunking solution is engineered for low-maintenance performance and reliable, high-power operational availability (up to 160A).

While these trends are essential to decarbonization, without grid readiness, they amplify system stress.

The urgency for modern grid investments

Over 40% of Europe’s distribution grids are more than 40 years old and approaching the end of their useful life.   However, addressing this requires an unprecedented level of investment and coordination:

  • €2.3 trillion in grid infrastructure by 2050
  • €90–100 billion annually, potentially higher with accelerated climate target timelines
  • 56% directed to distribution networks, which bear the brunt of EV charging, heat pumps, and decentralized renewables
  • €694 billion for transmission expansion, reaching capacity by 28% before 2030

Globally, grid length must increase by 20% by 2030, which would require a doubling of annual investment. Such investments will pay off, with a modernized grid expected to lower final electricity prices by 11% by 2035 and 30% in 2040.

Four priorities for change

Avoiding grid‑induced stagnation requires a substantial regulatory and market reset across four priorities to help close the gap between ambition and progress.

  1. Faster, dynamic grid planning.
    Grid planning must incorporate real-time data on electrification and renewable deployments; otherwise, future needs may be underestimated. The EU’s Grids Action Plan proposes a centralized scenario development and stronger top-down planning.
  2. Streamlined permitting.
    More than half of the transmission projects needed by 2030 are still awaiting permits. Permitting timelines stretching to a decade are incompatible with a transition that needs to move in years. The EU’s Grids Action Plan also proposes reducing timelines and exempting certain grid projects from environmental impact assessments to address the most severe delays.
  3. Market design that rewards flexibility.
    Energy storage, demand response, sector coupling, and smart-grid technologies can all reduce infrastructure pressures. But market design must also evolve to properly compensate for these services. This includes EVs equipped with bi-directional charging, which can further enhance grid stability, reduce congestion, and cut EU emissions by 7%, but only if markets are structured to reward that flexibility.
  4. Regulatory certainty for investment
    Scaling grid modernization requires predictable frameworks that support cost recovery and incentivize innovation, including digitalization, automation, and smart grid management. This is where the convergence of electrification, automation, and digital intelligence becomes essential to define the grid of the future.

Building the grid of the future

Modernizing and expanding electricity infrastructure are central to Europe’s energy transition and efforts to reduce carbon emissions.

As electrification accelerates across sectors, the grid is no longer a background enabler; it is the critical path. Every delayed connection, curtailed megawatt, or constrained industrial project represents a tangible setback.

Only with modern, future‑ready grids can Europe fully unlock the benefits of renewables, stabilize electricity prices, strengthen industrial competitiveness, and deliver on climate ambitions.

As an energy technology partner, Schneider Electric is advancing energy tech across buildings, data centers, industrial applications, and power grids to keep energy moving.

Let’s get there together.

Add a comment

All fields are required.