Five years ago, if a utility ordered a new transformer—the heart of every substation—the lead time was four to six weeks. Today, that same order may take three years to arrive.
And while utilities wait, much of the electrical infrastructure already in service is now over 40 years old and nearing the end of its design life. The grid isn’t just aging. It’s operating on borrowed time. Lead times have turned failures into strategic events.
Utilities can’t solve these problems overnight. But solving them does not require replacing installed assets. In fact, the most impactful modernization strategies are often about adding intelligence to existing infrastructure, not tearing it down.

From snapshots to continuous visibility
Historically, utilities monitored substation equipment through scheduled inspections. Those inspections are still important, but they provide only a snapshot in time.
Between inspections, critical events can go unnoticed. Equipment may cycle during transient faults. Thermal stress can begin to develop. Load conditions may gradually shift. These signals often appear long before a failure occurs, but they are easy to miss when measurements are taken only periodically.
Digitized substations change this model. Sensors and intelligent electronic devices continuously collect operational data, including voltage levels, breaker activity, temperature conditions, and power quality indicators. That data is automatically centralized and stored, providing both real-time visibility and a long-term operational record.
This shift provides immediate benefits:
- Fewer manual inspection requirements
- Improved worker safety by reducing time spent near energized equipment
- Better visibility across critical assets
More importantly, it allows utilities to analyze equipment behavior over time.
Turning operational data into asset intelligence
Most equipment failures develop gradually as small changes accumulate. Continuous monitoring allows utilities to identify these changes early. Over time, operational data can reveal patterns such as:
- Waveform distortions indicating electrical stress
- Early signs of insulation degradation
- Abnormal switching activity
- Environmental conditions affecting equipment performance
This allows utilities to move from time-based maintenance schedules toward condition-based asset management.
Instead of replacing equipment purely based on age or reacting to unexpected failures, operators can prioritize maintenance and capital investments based on actual equipment condition. The result is better allocation of maintenance budgets and more informed asset management decisions.
A transformer failure that didn’t become a substation crisis
The operational value of digitization becomes particularly clear when dealing with large grid assets. For example, a utility customer installed an asset-monitoring system on a major transformer. Large power transformers are expensive, operationally critical, and increasingly difficult to replace quickly.
Monitoring data from the system began to reveal subtle changes in current waveforms. Small anomalies suggested partial-discharge activity and early insulation degradation, indicating that the transformer could fail within months.
Based on those insights, the utility ordered a replacement transformer. Six months later, the existing transformer failed. The failure occurred one week before the replacement unit arrived.
Instead of managing a year-long equipment shortage, the utility needed only to manage a temporary operational gap for seven days. When a replacement transformer can take three years to arrive, that difference matters.
The role of analytics and AI
AI without structured data is noise. As substations generate more operational data, advanced analytics become increasingly important.
The volume of electrical and environmental data produced by modern monitoring systems is far too large for manual analysis. Machine learning and analytics tools are particularly effective at identifying patterns in repetitive operational data.
Artificial intelligence is expected to further expand these capabilities. Over time, AI systems may help utilities:
- Detect equipment degradation earlier
- Optimize maintenance scheduling
- Automate certain operational responses
- Improve overall system reliability
No one knows exactly what grid requirements will look like in 2035. But every utility that has operational data structured and accessible today will be better positioned to meet them, whatever they are. Digitization is, above all, a hedge against the unknown.
Modernizing without introducing new substation risk
Despite the benefits, many utilities approach modernization cautiously. Reliability remains the highest priority, and new technologies must not introduce unnecessary operational risk. For this reason, modernization often occurs in stages.
One important step is developing internal expertise in digital substation standards such as IEC 61850. Engineers who understand these communication architectures are better equipped to evaluate modernization strategies and manage implementation risks. Utilities can also create parallel testing environments (where digital substation architectures can be validated before deployment) when building or upgrading substations. These environments allow engineering teams to experiment with digital architectures and train operators before deploying new systems into production.
This incremental approach allows utilities to modernize while maintaining operational stability.
Where to begin with substation modernization
Modernization doesn’t have to start with a large-scale overhaul. Many successful projects begin with a focused pilot:
- Start with a single substation: Choose a site scheduled for maintenance or modernization. A single substation provides a manageable environment to test digital architectures without introducing risk across the broader network.
- Focus on visibility first: Digitization begins with operational data. Implement continuous monitoring to provide insight into equipment behavior: breaker operations, load conditions, temperature, and power quality. The goal is to build the data foundation.
- Build internal expertise: Develop internal proficiency in standards such as IEC 61850 to evaluate technology choices and manage implementation risks. Many utilities designate a lead engineer to develop this capability.
- Test before scaling: Parallel testing environments allow utilities to validate configurations, train operators, and experiment with digital architectures before deploying them in live substations.
Learn more about digital substation architectures and how they help utilities modernize existing infrastructure while improving reliability.
Add a comment