Embracing the low-voltage grid 

As the energy transition accelerates, utilities are facing a new frontier: low voltage (LV) grid. Once considered the quiet end of the distribution spectrum, LV networks are emerging as a critical point of transformation, driven by the rise of electric vehicles, heat pumps, rooftop solar, and battery storage. These technologies are reshaping consumption and generation patterns, introducing unprecedented complexity into grid operations. 

For utility executives, this shift presents both a challenge and an opportunity. The challenge lies in managing increasingly volatile grid conditions. The opportunity is in leveraging digital technologies to turn complexity into control and control into value. 

The new reality: Two extremes, one grid 

LV grids are now operating under two intra-day extreme conditions: 

  • Low load, high generation injection: Driven by distributed photovoltaics (PVs), this scenario causes overvoltage and reverse power flows. 
  • High load, low generation injection: Fueled by EVs and heat pumps, this leads to transformer and cable overloads, pushing voltage profiles out of range. 

These conditions are not theoretical; they are happening now. The result? Delays in connecting new assets, disconnection of prosumers, and increased outages. And with outages now affecting heating, mobility, and remote work, customer dissatisfaction is more acute than ever. These phenomena are extensively documented in Schneider Electric’s Low Voltage Grid use case, which highlights how DER growth is reshaping voltage profiles globally.

Rethinking strategy: From reinforcement to intelligence

The LV grid is no longer a passive endpoint, it’s a dynamic, data-rich environment that demands strategic oversight. For C-level leaders, the imperative is clear: invest in digital intelligence to unlock operational efficiency, meet sustainability targets, increase flexibility and customer satisfaction, and grid resilience. 

Traditional grid reinforcement strategies, high CapEx, slow deployment are no longer sufficient, particularly noting the LV grid’s orders of magnitude larger than MV and HV and lacking historical digitization investment. Instead, utilities must adopt a smarter, faster, and more flexible approach. This means combining IoT devices with advanced software platforms to enable real-time visibility with predictive analytics, grid management and optimization. 

Key strategic use cases include: 

1. Grid awareness (monitoring) 

Real-time visibility in LV grid conditions is foundational. Utilities can monitor feeder and transformer headroom, detect theft, disaggregate loads, and assess hosting capacity. Dynamic topology and state estimation further enhance situational awareness. 

2. Outage management 

Smart meters and integrated systems enable precise fault detection and localization. Utilities can automate switching plans, crew dispatch, and customer notifications. This not only reduces outage duration but also improves transparency and customer trust. 

3. Capacity management 

Utilities can mitigate overloads and voltage issues by optimizing grid assets (e.g., OLTCs, LV switches) and leveraging flexibility services. Smart charging, remote control of DERs (e.g. via IEEE2030.5), and integration with demand response platforms are key enablers. 

4. Low voltage modeling 

Auto-discovery of service delivery points connectivity and impedance matrix enables utilities to correct topology errors and uncover non-telemetered switch statuses critical for accurate planning and operations. The integration into a geographic information system (GIS) further enhances the understanding of low voltage grids.  

5. Asset management 

Monitoring transformer temperature and gas conditions helps utilities evaluate asset health and anticipate maintenance needs. Combined with estimating cable and transformer life expectancy, this proactive approach extends asset life and reduces unplanned outages. 

6. Power quality 

With more granular data available, utilities can monitor waveform distortions and harmonics introduced by inverter-based resources such as solar PV systems and electric vehicle chargers. Addressing these issues is critical to maintaining voltage stability and reducing technical losses. 

For a clear and visual explanation of today’s LV grid challenges, watch our expert video featuring Jacqui Mills, Marketing Manager ESX Power & Grid and Cyril Domenech, Application Architect Lead. 

Quantifying the impact 

Utilities implementing these strategies are already seeing measurable benefits: 

  • Improved grid observability: Real-time monitoring from MV to LV networks. 
  • Reduced outage duration: Faster fault detection and customer communication. 
  • Enhanced DER integration: Dynamic export/import limits and market participation. 
  • Optimized voltage profiles: Real-time reconfiguration using OLTCs and LV switches. 
  • Energy savings and customer satisfaction: Lower bills and improved service reliability. 

For example, a utility in Italy expanded its dynamic grid topology from MV to LV, improving planning and operational efficiency. In Sweden, automated outage notifications enhanced customer experience. In Australia, real-time constraint management enabled flexible DER integration. And in the UK, voltage optimization using OLTCs led to energy savings and better power quality. 

Strategic deployment: Standalone vs. integrated platforms 

Schneider Electric supports utilities’ two main deployment pathways: 

  • Standalone LV management: Tailored software solutions focused exclusively on LV grids. 
  • Integrated ADMS platforms: Comprehensive systems managing MV and LV together. 

The latter is gaining traction for its holistic capabilities. Real-time monitoring of MV/LV substations using IoT sensors, connected via RTUs or directly to cloud platforms is already being implemented across Europe and Australia. 

A phased, future-proof approach 

Schneider Electric’s solutions suite support utilities at every stage of their LV grid modernization journey. Starting with basic use cases like visibility and outage management, utilities can scale up as data availability and organizational readiness improve. 

Key value propositions include: 

  • Modular, future-proof platform: Agility to adapt to evolving grid conditions and regulatory requirements. 
  • Centralized data governance: Streamlined access, analytics, and reporting. 
  • Situational awareness: Real-time and forecasted insights into DER impacts and outages. 
  • DER planning: Simplified customer connections, hosting capacity analysis, and scenario simulations. 
  • Grid asset control: replacement of aging assets with smart kiosks enables edge applications, analytics and control 

By embracing a phased, data-driven approach to LV grid management, utilities can not only meet today’s challenges but also shape the future of energy distribution. 

Low‑Voltage Grid Management Report provides a comprehensive strategic framework for LV grid modernization. 

Add a comment

All fields are required.