Reimagining circuit protection: Why EasyPact™ NW changes the conversation

As leaders in the energy management and automation space, we constantly ask ourselves a simple question. Are we solving yesterday’s problems, or preparing our customers for tomorrow’s realities? 

Today, electrical systems are no longer just about switching and protection. Industrial plants, hospitals, hotels, data centers, and commercial spaces are running more complex electrical networks than ever before. One fault, one delay, one blind spot can cost far more than downtime. 

This is why we created the EasyPact™ NW Series, not as just another circuit breaker, but as a new way of thinking about circuit protection. 

At Schneider Electric, we believe protection should be proactive, visible, and intelligent. EasyPact™ NW was built to make that belief real. 

Breaker health at a glance. Empower operators to take proactive actions with real-time breaker health and alarms.

A single platform. A smarter future. 

One of the most powerful advantages of EasyPact™ NW is its unified design philosophy across frame sizes. Whether it’s NW1 or NW2, the operational experience stays consistent. The system grows with your needs, rather than forcing you to change platforms as demands evolve. 

A shift from reaction to intelligence 

Traditional protection systems were designed to react after something went wrong. But modern power systems can’t afford to wait for failure. 

EasyPact™ NW introduces a new layer of intelligence into low-voltage protection. With scalable Trip Systems (TSS 2.0 to TSS 6.0), users can choose protection levels that fit their environment from basic overload protection to advanced earth-fault detection and energy metering. This means protection is no longer uniform; it becomes purpose-built. 

This modular intelligence means the same platform can serve everything from small commercial buildings to the most demanding critical infrastructure. It doesn’t force complexity, it adapts to it. 

Add to that programmable M2C contacts, and the system doesn’t just protect, it communicates, alerts, and automates. 

Visibility that changes everything 

One of the biggest risks in electrical systems is not failure. It’s not knowing a failure is coming

EasyPact™ NW changes this through native digital readiness and NFC connectivity. With a simple smartphone tap, teams can instantly view: 

  • Instantly access breaker health 
  • View trip history and fault diagnostics 
  • Eliminate the need for HMIs or external tools 
Breaker status at your fingertips. Detailed trip cause insights, delivered via reliable NFC connectivity in EPD, improves predictive maintenance and enhances safety.

Through the EcoStruxure Power Device App, users can visualise data, and restore operations faster, without opening panels or shutting down systems, reducing downtime dramatically. 

For facility managers, this removes guesswork. 

For maintenance teams, it removes wasted hours. 

For businesses, it removes risk and reduces service costs. 

This is not convenience. This is a fundamental shift in how protection is managed. 

Digital-first commissioning: Faster, smarter, error-free 

  • EcoStruxure Power Commission software simplifies setup, testing, and reporting, helping consultants and panel builders reduce onsite effort and eliminate configuration risks. It can generate very detailed, standardized factory and site acceptance reports, ensuring consistency and peace of mind. It also provides easy firmware upgrade capability. 

With the Product Selector and MySchneider platform, system design and ordering are seamlessly connected. From design to doorstep, Product Selector + MySchneider makes every configuration land the first time right —no fixes, no fuss The result? Faster project execution and cleaner handovers in every deployment. 

Safety without compromise 

When it comes to protection, safety can never be optional and EasyPact™ NW treats it as a core design principle, not an add-on. 

Built-in safety shuttersrobust door interlocks, and fully rated neutral protection create a secure operating environment, ensuring compliance while protecting personnel and equipment at every stage. 

This is safety engineered into the system, not added around it. 

Fault diagnosis made simple 

Downtime is expensive. Guesswork makes it worse. 

EasyPact™ NW transforms fault investigation into a fast, data-driven process through: 

  • Integrated trip history and detailed event logs that enable accurate root cause analysis 
  • NFC-enabled access to instantly retrieve fault data through a smartphone 
  • EcoStruxure Power Commission for advanced diagnostics and automated reporting 

What once took hours is now accessible in minutes helping teams move from reactive troubleshooting to confident decision-making. 

One feature I consider crucial is the internal battery–powered fault indication system

Even when the breaker is open or de-energized, the fault LEDs remain active. This simple innovation allows: 

  • Faster root-cause identification 
  • Reduced restoration time 
  • Safer troubleshooting 

And yes, the battery is easily testable and replaceable without removing the breaker, ensuring the system stays reliable over its lifetime. 

Designed for scale, built for real-world pressure 

When you work closely with customers across industries, you realise one simple truth. The pressure points are different, but the expectation is the same. Power cannot fail. 

EasyPact™ NW naturally adapts across these realities. You don’t have to rethink your design philosophy or rebuild your architecture every time you move from one application to another. Whether it’s a hospital, a hotel, a factory, or a transport hub, the performance remains consistent, predictable, and scalable. 

That’s what makes the difference. It doesn’t force you to design around the product. It allows your infrastructure to grow without friction. 

Sustainability with transparency 

Every EasyPact™ NW breaker is supported by Schneider Electric’s Environmental Data Program, delivering: 

  • Lifecycle footprint analysis 
  • Repairability and recyclability metrics 
  • Verified data for ESG reporting 

This gives consultants, specifiers, and end users the ability to make responsible, traceable choices without compromising performance. 

“EasyPact™ NW isn’t just an upgrade, it’s a rethink. We’ve taken the complexity out of protection and put intelligence, safety, and simplicity into the hands of every customer. Whether you’re building a commercial mall or powering a hospital, EasyPact NW is your new standard.” 

Explore the EasyPact™ NW range and discover how it can transform your next project, whether you’re designing, building, or operating. 

Visit Schneider Electric

About the author

Amit Chaturvedi, Director Offer Marketing PP & FD

With a career that’s spanned R&D labs, customer frontlines, and marketing strategy rooms, Amit Chaturvedi now leads Offer Marketing for Schneider Electric’s LV & MV Power Products. He’s passionate about translating technology into meaningful value for customers and writes about how innovation and digitalization are reshaping the future of power distribution.

Add a comment

All fields are required.