From data centers to AI factories: Three steps for scaling infrastructure for the future

AI is accelerating a seismic shift in how colocation data centers design infrastructure, consume power, and deploy and scale compute for tenants. With demand skyrocketing and chip innovation speeding ahead, traditional data centers can no longer keep up. Industry analysts forecast the global data center sector will expand at a 14% CAGR through 2030, with AI workloads accounting for half of all workloads by 2030. Fortunately, the architectural transformation colocation providers need to rapidly yet efficiently right-size and scale infrastructure is already underway.

Schneider Electric recently hosted a discussion on what it means to prepare data center infrastructure for an AI-centric future. Perspectives from operators such as Colovore contributed real-world insights to the conversation. We both had the privilege of sharing insights, lessons learned, and best practices of what it means to prepare data center infrastructure for an AI-centric future, today. You can hear our complete conversation in the recent Schneider Electric Innovation Talk: “From data center to AI factory: scaling infrastructure for the future of artificial intelligence.”

Let’s take a look at some essential considerations for colocation data center providers to turn traditional data centers into AI factories that empower large-scale enterprise tenants to charge ahead along their AI innovation roadmaps.

1. Modularity is the key to speed.

This first point of advice is non-negotiable. Data centers looking to accommodate ever-increasing AI loads must build infrastructure with modularity as the design driver. Why? Because modularity equals speed without stranding Capex investments in empty data center halls that were overbuilt from the get-go. It is imperative to design for flexibility and scalability to enable rapid fit-outs only when they are needed.

When it comes to provisioning for large-scale enterprises, we would argue that the challenge is building with enough flexibility to serve the here and now while making sure the infrastructure is future-ready. Another challenging factor is that the mixture of the floor in terms of what tenants will be adding often is undetermined upfront. After all, there is nothing more deflating than building out an entire 12,000 square-foot quadrant for 21 KW racks only to have a customer say they really need only six one MW racks. 

The solution is to ensure that modularity is possible. This approach takes a back-of-the-rack framework, where modular physical infrastructure (that is, racks, cooling distribution units (CDUs), and power) can run up to each rack, thereby solving for the variation that’s always going to be present as tenant needs change over time.

In short, modularity allows colocation providers to scale infrastructure, maintain security measures tenant-by-tenant, and upgrade as needed (e.g., when tenants decide to migrate from air infrastructure to a variety of different liquid cooled chipsets that are better suited for AI workloads). The Schneider Electric EcoStruxure™ pod data center, for example, is a rack-ready, vendor-agnostic, future-ready, and scalable infrastructure solution that can be deployed in increments of eight to twelve racks. 

While this modular approach to data center design and buildouts is innovative and advanced, we can harken back to the old-school analogy of Tinker Toys to explain why it is so valuable. Just like building with Tinker Toys, you can direct the right amount of infrastructure to the right place at the right time.

2. Liquid cooling should complement, not replace, air cooling.

Since the rise of AI workloads, liquid cooling has taken center stage. Without question, it is essential for high-density AI racks. In reality, though, most enterprises won’t leap from air to full liquid overnight. Deployments still require hybrid environments, where air and liquid must work together along the same loop. Not to mention that different chips require different water temperatures, making adaptable cooling loops essential.

Cooling strategies therefore must balance liquid and air for efficiency. The approach we suggest is “working from the silicon out.” In other words, build out flexible cooling infrastructure in advance of each new GPU.

But first, it’s important to clarify some of the confusion about cooling AI workloads. We know that deploying liquid cooling is pivotal for high-density AI, but flexibility is the key for colocation fit-outs or upgrades. Many large-scale enterprise colocation tenants started long ago with air-cooled racks, for instance, and are only now scaling up their next generation of infrastructure to be liquid-cooled. It is up to the colo to help them scale based on their innovation needs and schedules. That may mean scaling gradually, rack by rack, so as not to disrupt existing operations. Again, modular infrastructure applies to cooling and includes back‑of‑rack cooling, primary loops, and CDU-based designs, which reduce wasted capital and shorten deployment time.

Other considerations include the fact that different chips need different water temperatures to cool them. Eventually colocation providers can start removing compressors and chillers on the floor and shifting toward more dry-pan units and other infrastructure with a much lower PUE. In fact, achieving lower PUE is an integral aspect of the end goals of running AI factories: higher efficiency and fewer compressors.

3. Partnerships turn complexity into repeatability.

The name of the AI factory game is collaboration. We don’t mean just buy the product; work together on design, deployment, and commissioning; and then say good-bye to the vendor. Instead, we advocate for establishing and engaging in a long-term partnership — one that even opens pathways for co-engineering or fine-tuning solutions.

It is within this type of dynamic, collaborative ecosystem — including operators such as Colovore, manufacturing and software teams such as Schneider Electric, and cooling innovators such as Motivair by Schneider Electric — that stakeholders can work closely to deliver reliable AI infrastructure at scale and over time.

Schneider Electric and Colovore have collaborated for more than 10 years, combining infrastructure innovation with real-world deployment experience based on end-customer use cases. By working together, we address issues such as how to better manage CDU technical loops in relation to water requirements, power management, and even considerations related to smart grid integrations to improve efficiency. This approach enables continuous feedback from operators to inform design, deployment, and operation, helping drive innovation and more efficient and predictive manufacturing solutions.

An important aspect of this ecosystem is Schneider Electric’s commitment to supporting grid reliability and resilience in communities near data center sites (e.g., during cold snaps or heat waves), particularly as AI infrastructure demand continues to grow.

Accelerating the future of AI factories

As we discussed in the Schneider Electric Innovation Talk: “From data center to AI factory: scaling infrastructure for the future of artificial intelligence,” the AI era demands a new generation of data centers, which must be modular, capable of transitioning to liquid cooling, software‑driven, and community-conscious. While the shift from traditional data centers to AI factories is really only just beginning, we know that change is happening at lightning speed.

By embracing modularity and flexibility, designing hybrid cooling strategies, and forging strong ecosystem partnerships, colocation data center operators can lead the way. To us, the opportunity to shape the future of AI infrastructure is exciting, actionable, and transformative.

By Vandana Singh, Senior Vice President, Secure Power NAM, Schneider Electric, with perspectives from Jeff Springborn, CEO of Colovore

Add a comment

All fields are required.