AI colocation cooling: How US neoclouds specify liquid-cooled multi-tenant capacity

Summary
  • AI colocation cooling must be specified around the actual GPU platform, not rack density alone. Temperature, flow, pressure, coolant compatibility, residual air load, and heat-rejection capacity determine whether a facility can support the intended hardware.
  • Shared infrastructure requires clear service and isolation boundaries. Colocation providers and neoclouds should define ownership, fault containment, maintenance responsibilities, and measurable delivery conditions across cooling interfaces.
  • The cooling architecture must be evaluated across the full thermal path. Direct-to-chip systems, CDUs, HDUs, rear-door heat exchangers (RDHx), chillers, and heat rejection create different requirements for retrofit, hybrid, and new-build environments.
  • Repeatable capacity depends on testing and documented operating limits. Acceptance testing, phased commissioning, and expansion planning help ensure new GPU capacity can be added without compromising neighboring racks or existing service.

Author: Mike Donahue, Solution Architect, North America Operations

A neocloud can secure colocation space and electrical capacity yet still lack the cooling conditions its GPU racks require. A facility’s advertised rack density leaves important questions unanswered: what happens during maintenance, how the system responds to a leak, and whether the next hardware generation will fit the same thermal architecture.

US deployments are making those questions concrete. Switch has announced a liquid-cooled NVIDIA GB300 NVL72 deployment for CoreWeave, while TeraWulf’s Lake Mariner campus in New York is integrating Motivair by Schneider Electric cooling equipment in three of the buildings to support cloud-provider tenants.

AI colocation cooling should be specified around the operating requirements of shared infrastructure. A strong specification connects hardware requirements, fault containment, facility interfaces, and acceptance testing so operators can confirm which capacity is ready for customer workloads.

AI colocation cooling starts with the service boundary

Multi-tenant AI capacity involves two distinct relationships. A colocation provider hosts a neocloud’s infrastructure; that neocloud may then serve multiple customers through its platform. A customer’s logical cloud environment does not automatically require a dedicated physical cooling loop.

The practical requirement is to define how cooling events affect the infrastructure supporting those customers. A rack, branch, row, or pod may form an isolation boundary. Each choice changes the amount of capacity exposed to a maintenance activity or fault.

Before selecting equipment, the colocation provider, neocloud, specifier, and contractor should agree on who owns the CDU, manifolds, hoses, coolant monitoring, and emergency response. Those responsibilities belong in the design and service agreement, with measurable delivery conditions at the handoff between facility and IT cooling.

The service agreement should also describe a cooling-service breach in measurable terms. Temperature, flow, pressure, duration outside tolerance, and affected capacity provide measurable criteria. Agreed measurement locations and escalation procedures give both parties a shared basis for responding when delivered conditions move outside the equipment’s approved limits.

Specify an operating envelope for the actual GPU platform

A rack-density figure is useful only alongside the conditions under which cooling can deliver itA rack-density figure is useful only alongside the conditions under which cooling can deliver it. The AI colocation cooling specification should identify:

  • Facility-side and technology-side supply and return temperatures.
  • Required coolant flow, pressure limits, and system pressure drop.
  • Approved coolant chemistry and wetted materials.
  • Heat captured by liquid and any remaining air-cooled load.
  • Performance during normal operation, maintenance, and defined equipment failures.

These inputs establish whether the complete cooling path can support the proposed installation. A CDU’s nominal capacity cannot compensate for inadequate facility flow or insufficient outdoor heat rejection.

Match the architecture to the hardware generation

At the kind of densities NVIDIA’s Vera Rubin delivers, the rack, coolant distribution, facility plant, and electrical supply need coordinated engineering.

The liquid-to-air heat split also varies by platform and configuration. Operators should obtain the requirements for their actual equipment rather than carry a fixed percentage from an earlier installation into a new specification.

For example, before reserving adjacent racks for a second GPU platform, a neocloud should check its temperature, flow, and coolant requirements against the existing cooling envelope. Floor space alone cannot establish compatibility.

Make rack isolation and maintainability explicit

Rack-level monitoring and isolation controls are especially important in shared infrastructure. Designs should allow operators to monitor flow, temperature, pressure, and leaks and isolate an affected rack or branch without unnecessarily disrupting neighboring capacity.

A procurement specification should state what happens after an alarm, including valve closure, workload shutdown requirements, and the capacity that remains operational while the affected section is drained, repaired, and recommissioned.

Maintenance access deserves the same attention as fault response. Shared infrastructure needs accessible isolation points, documented fluid-handling procedures, and an agreed method for returning serviced equipment to operation. The Open Compute Project’s modular technology-cooling guidance provides a useful framework for branch isolation, cleanliness, and future adaptation.

Follow the heat through the colocation facility

Liquid cooling moves heat through several interfaces before it leaves the site. Each interface needs a defined duty, operating condition, and owner.

Connect direct-to-chip cooling to facility heat rejection

In a liquid-to-liquid architecture, Coolant Distribution Units (CDUs) transfer heat between the technology coolant circuit and facility water while separating those circuits. Direct-to-chip accessories, including in-rack manifolds and hose kits, complete connections near the IT equipment and need compatible materials, pressure ratings, and service access.

Chillers and heat rejection equipment handle the downstream thermal duty. Selection depends on the rack requirements, facility-water temperatures, local design weather conditions, and resilience strategy. A system specified for a Texas site needs assessment against that site’s conditions even if its rack layout matches a New York deployment.

Warmer coolant can create opportunities for economization, but direct-to-chip (DTC) cooling does not automatically eliminate chillers. Energy and water performance depend on the complete heat-rejection design.

Evaluate AI colocation cooling retrofit options against remaining facility capacity

Heat Dissipation Units (HDUs) provide a liquid-to-air path where an appropriate facility-water connection is unavailable. Motivair by Schneider Electric’s HDU transfers heat from the liquid-cooled equipment to room air. The existing air-cooling system must then carry that additional load.

Rear-door heat exchangers (RDHx) serve a different role: they capture heat from rack exhaust air and transfer it to a liquid circuit. They can support hybrid environments, including configurations with residual air-cooled loads, subject to equipment and facility compatibility.

Consider a neocloud leasing space in an existing air-cooled hall. An HDU may provide a connection path for liquid-cooled servers, but the assessment still needs to establish room-level cooling headroom. A rear-door approach requires a suitable liquid heat-removal path. Both decisions should follow a site assessment before capacity is committed to customers.

Build repeatable expansion around defined interfaces

The useful unit of expansion may be a row or pod with defined electrical, thermal, control, and service interfaces. Prefabricated modular IT pods can organize that infrastructure into a repeatable deployment framework, provided the selected configuration supports the intended equipment and cooling design.

As capacity grows, additional racks change flow demand and pressure conditions, while a new GPU platform may change temperatures, fluid requirements, or the air-cooling load.

Design teams should identify what can remain standard and what requires reassessment for each phase. Reserve connection points, document expansion limits, and align cooling increments with electrical capacity. A repeatable layout gives procurement and construction teams a common basis for delivery while leaving specific hardware requirements visible.

Test the cooling system under representative operating conditions

Acceptance testing should demonstrate how the installation behaves when compute, power, controls, and cooling operate together. The project team should agree on tests for sustained load, changing load, partial occupancy, and selected failure or maintenance scenarios. Relevant measurements include rack-inlet coolant temperature, flow, pressure, alarms, and recovery behavior, with acceptance limits tied to the hardware requirements.

For a shared loop, test an isolation event and confirm conditions at neighboring racks. For phased construction, establish how a new section will be flushed, checked, connected, and commissioned alongside operating capacity.

Handover should document control sequences, alarm ownership, maintenance procedures, and escalation paths so the operations team has a clear basis for protecting service after construction ends.

Apply an end-to-end cooling approach to shared AI capacity

TeraWulf’s Lake Mariner campus project scope illustrates the connection between rack-level cooling and facility delivery. For projects serving multiple cloud providers, the engineering task is to coordinate those systems while defining each tenant’s cooling interfaces, service responsibilities, and expansion requirements.

With Motivair by Schneider Electric, Schneider Electric’s comprehensive liquid cooling portfolio spans direct-to-chip connections, coolant distribution, and facility cooling and heat rejection. Its greatest value to neocloud operators lies in coordinating those interfaces with power, monitoring, and lifecycle support for extreme thermal loads.

Review the proposed GPU platform and colocation site against one agreed operating envelope, responsibility map, and acceptance plan. That gives AI colocation cooling a clear basis for deployment and expansion. Explore Schneider Electric’s end-to-end liquid hub and reference designs to inform that discussion. View our guide to Liquid Cooling Architectures to learn how to plan a cooling architecture that can support higher-density workloads, existing-facility constraints, and evolving resource requirements.

Frequently Asked Questions About AI Colocation Cooling

What should neocloud operators look for in AI colocation cooling?

Neocloud operators should evaluate whether a facility can deliver the temperatures, coolant flow, pressure, and heat rejection their GPU hardware requires. The specification should also define maintenance access, fault isolation, monitoring, and responsibility boundaries between the colocation provider and neocloud. An advertised rack-density rating alone does not establish compatibility or operational readiness.

Does each tenant need a dedicated liquid cooling loop?

A dedicated liquid cooling loop is not automatically required for every tenant or compute customer. Shared loops can serve multiple racks when the design provides appropriate flow control, monitoring, and isolation. The specification should define which racks remain operational during a leak, equipment failure, or maintenance activity. Physical cooling boundaries and logical cloud-customer boundaries are separate design considerations.

Can an existing air-cooled colocation facility support liquid-cooled GPU racks?

An existing air-cooled facility may support liquid-cooled GPU racks after an assessment of its electrical capacity, cooling infrastructure, space, and hardware requirements. A liquid-to-liquid (L2L) CDU requires a suitable facility-water connection. A liquid-to-air Heat Dissipation Unit (HDU) transfers heat to room air, so the existing air-cooling system must have sufficient capacity to remove that load.

Does direct-to-chip liquid cooling eliminate the need for air cooling or chillers?

Direct-to-chip liquid cooling does not automatically eliminate either air cooling or chillers. Some hardware configurations retain air-cooled components, while others capture more heat through liquid. Chiller requirements depend on coolant temperatures, local climate, heat-rejection equipment, and resilience needs. Operators should specify both heat-removal paths for the actual hardware configuration.

How should liquid cooling be tested before GPU capacity enters service?

Acceptance testing should verify cooling performance under representative sustained loads, load changes, and agreed maintenance or failure scenarios. Measurements should include coolant temperature, flow, pressure, alarms, and recovery behavior. For shared infrastructure, testing should also confirm how isolating one rack or branch affects neighboring capacity, with acceptance limits tied to the IT equipment’s requirements.

Add a comment

All fields are required.