AI data centres in Australia: How liquid cooling can stretch a capped grid connection

Summary
  • Grid capacity is becoming a defining constraint for AI data centres in Australia. With large connection pipelines in NSW and Victoria, operators need to treat secured grid capacity as a finite resource and design facilities to use it efficiently.
  • Cooling efficiency directly affects how much power is available for compute. Lower facility overhead can increase the share of a fixed connection available to IT, making PUE and reliable compute per secured megawatt important capacity measures.
  • The right liquid-cooling architecture depends on the facility and deployment model. Rear-door heat exchangers (RDHx), Heat Dissipation Units (HDUs), and liquid-to-liquid CDUs each bring different trade-offs across retrofit and greenfield deployments, with distinct considerations for colocation and neocloud operators.
  • Cooling and electrical design need to be planned together. Reducing mechanical load only creates usable IT headroom when the electrical architecture can deliver that released capacity to the compute load.

Author: Mark Deguara, Technology Innovation Leader

Building an AI data centre in Australia increasingly requires close attention to grid capacity. At the end of Q2 2026, AEMO was tracking 9.0 GW of maximum data-centre connection capacity in the formal transmission connection process, with 52% in New South Wales and 31% in Victoria. In Western Sydney, Transgrid has said existing network capacity has already been allocated to signed agreements representing about 1.5 GW, leaving limited capacity for additional large connections without augmentation.

Cooling directly influences how much of a fixed connection can support IT. Power consumed by cooling and other facility infrastructure reduces the capacity available to compute. Liquid cooling can lower that overhead by removing heat efficiently at the source and reducing reliance on fans and mechanical cooling. The potential gain depends on the architecture across the full thermal system.

Grid capacity is setting the ceiling for AI data centres in Australia

AEMO’s Q2 2026 data shows 17 data-centre projects representing 9.0 GW of maximum connection capacity in the formal transmission connection process. NSW accounted for approximately 4.7 GW and Victoria for about 2.8 GW. Most remained at the application stage, so the figures describe the formal development pipeline rather than committed operating load.

Western Sydney is already experiencing tighter constraints. Transgrid has reported more than 20 GW of data-centre connection enquiries and about 1.5 GW covered by signed agreements. Further large connections will require additional transmission capacity.

AEMO Victorian Planning has also received more than 18 GW of large-load enquiries, largely associated with metropolitan Melbourne data centres. A secured connection now represents a finite resource within the facility design. Lower infrastructure overhead can leave a larger share of that capacity available to IT.

Capped connections place compute and cooling within the same power budget

Power Usage Effectiveness (PUE) compares a data centre’s total facility power consumption with the amount used by its IT equipment. With a fixed grid connection, dividing connection capacity by PUE gives the maximum theoretical power available to IT. Consider a simplified 100 MW connection. At a PUE of 1.55, theoretical IT capacity is about 64.5 MW. At 1.20, it rises to 83.3 MW, an 18.8 MW difference within the same electrical envelope.

Actual facilities also account for redundancy, utilisation, maintenance states, power quality and other operating constraints. Cooling influences both facility and server power; air movement and mechanical systems consume facility energy, while onboard server fans consume IT energy.

Liquid cooling can reduce both, with results shaped by coolant temperature, heat-rejection design, utilisation and the share of equipment being liquid cooled. Reliable compute per secured megawatt provides a useful capacity measure alongside PUE.

Cooling architecture determines how much overhead can be reduced

Liquid cooling includes several architectures with different facility-level outcomes for AI data centres in Australia. Rack-level heat capture is one part of a larger system that includes coolant distribution, residual air cooling, pumps, chillers and final heat rejection.

Rear-door heat exchangers (RDHx)

A rear-door heat exchanger captures hot exhaust air at the rack and transfers the heat to liquid. The approach can reduce room-cooling demand and support higher-density racks, particularly in existing colocation halls and mixed-density environments. Internal server fans remain in use, while water temperature and the downstream cooling plant influence overall efficiency.

Direct-to-chip cooling with HDUs

Direct-to-chip (DTC) cooling uses cold plates on high-power components such as CPUs and GPUs. A Heat Dissipation Unit (HDU) can transfer heat from the liquid loop into data-hall air where facility water is unavailable. Retrofit facilities, colocation environments and neocloud deployments can use this architecture to introduce direct-to-chip cooling without extending a facility-water loop to each deployment. Because the heat returns to the room, the existing air-cooling system continues to carry part of the facility load.

Direct-to-chip cooling with liquid-to-liquid CDUs

A Coolant Distribution Unit (CDU) transfers heat from the technology cooling loop into the facility-water system while keeping the two loops hydraulically separated. More heat can bypass room-air infrastructure, reducing demand on fans and air handlers. Supply and return temperatures, pump energy, heat exchangers and chilled-water conditions all influence performance.

Dedicated warm-water systems can further reduce chiller use in greenfield campuses and major expansions where climate and design conditions permit. Chillers and heat rejection remain integral to the thermal architecture because the captured heat ultimately has to leave the facility.

New rack-scale AI systems are increasing the thermal loads these architectures must accommodate, making coordination between chip cooling, coolant distribution and facility heat rejection increasingly important.

Cooling priorities vary across the Australian data centre market

Hyperscalers and internet giants

Campus-scale deployments benefit from evaluating efficiency across the complete electrical and thermal system. Useful measures include IT MW per secured grid MW, cooling-system power, usable GPU capacity and performance per watt. Liquid-to-liquid architectures and warmer coolant temperatures can reduce mechanical cooling demand. Electrical distribution also needs enough flexibility to make released capacity available to IT.

Colocation operators

Mixed tenant hardware and staggered adoption create different requirements for colocation facilities. Liquid-to-air HDUs can introduce direct-to-chip equipment before facility-water distribution reaches an entire hall, while liquid-to-liquid CDUs can serve larger deployments with lower room-cooling demand. Service delivery also depends on clear specifications for supply temperature, flow, pressure, water quality, redundancy and ownership of the secondary loop.

Neocloud providers

Rapid GPU deployment and high utilisation can favour modular direct-to-chip systems and HDUs where facility water is unavailable. Prefabricated modular IT pods can also support repeatable capacity expansion for AI data centers in Australia. As deployments increase in scale, cooling overhead has a larger effect on lifetime power consumption. Liquid-to-liquid (L2L) systems can reduce facility demand compared with architectures that return the captured heat to the data hall.

Specifiers, contractors and developers

Early-stage design modelling should cover normal, redundant and maintenance states, residual air load, CDU power paths, supply and return temperatures, pump power, heat rejection and the expected mix of air- and liquid-cooled IT. Transformer allocation deserves the same attention. Reducing mechanical load produces additional IT headroom only when the electrical architecture can deliver that capacity to the compute load.

Common questions about AI data centres in Australia

Are there any AI data centres being built in Australia?

Yes. Australia has several AI-focused and AI-ready data-centre projects in development. NEXTDC’s S7 campus in Eastern Creek, Sydney, is currently in planning and is designed for high-density AI and cloud infrastructure, while Macquarie Data Centres has been developing its 47 MW IC3 Super West facility for AI and cloud workloads. These projects add to a wider pipeline of hyperscale and high-density development across NSW, Victoria and other Australian markets.

How many AI data centres does Australia have?

There is no single authoritative count of AI-specific data centres in Australia because facilities are not consistently classified by workload. However, Data Center Map lists 296 data centres across 33 markets in Australia, including major hubs such as Sydney and Melbourne. Only a portion of those facilities are purpose-built for, or equipped to support, high-density AI workloads. As AI infrastructure expands, measures such as available power, rack density and cooling capacity can provide a more useful view of market readiness than the number of facilities alone.

Why are so many data centres being built in Australia?

Demand for AI, cloud services and other digital infrastructure is driving additional capacity, while Australia offers several characteristics that support large-scale investment. The Australian Government points to its stable operating environment, legal protections, renewable-energy potential, available land, international connectivity and proximity to growing Indo-Pacific economies.

That growth is increasing pressure on electricity networks, particularly around established data-centre clusters in NSW and Victoria. Grid access, cooling efficiency and site infrastructure are therefore becoming closely connected development decisions.

Use secured grid capacity more efficiently

Cooling choices influence how much of a constrained grid allocation can reach IT in an AI data centre in Australia. Liquid cooling can reduce power used for fans, air movement and mechanical cooling, with the final result determined by the path from direct-to-chip heat capture through CDUs or HDUs to chillers and heat rejection. Rack density remains an important design input, while reliable compute per secured grid megawatt gives operators a broader view of capacity efficiency.

With Motivair now part of Schneider Electric, our comprehensive liquid-cooling portfolio spans CDUs, HDUs, rear-door heat exchangers (RDHx), chillers and heat rejection and the wider cooling infrastructure around them to support architecture choices based on the facility’s power, thermal, and deployment constraints.

Explore Schneider Electric’s Liquid Cooling Hub to learn about comprehensive thermal architectures. For a closer look at how to select and design the right system for your facility, download the Liquid Cooling System Architecture Guide.

Add a comment

All fields are required.