Summary
- Prefabricated modular AI factories can reduce implementation time by up to 60% compared with traditional construction.
- Integrated power, cooling, and compute infrastructure helps maximize AI performance and tokens per watt.
- Pre-engineered modular solutions reduce infrastructure complexity and streamline deployment.
- Modular infrastructure enables phased expansion as AI computing requirements grow.
- Factory-tested modules and 3rd party certifications simplify commissioning and shorten time to first token.
The future of the AI factory is modular. As GPU capacity grows at dizzying speed, traditional construction methods struggle to keep up. The fastest way to build AI factories is to leverage prefabricated data center modules.
NVIDIA plans to introduce higher-capacity GPUs soon. NVIDIA’s next-generation Vera Rubin is already in production, with systems beginning to ship in late 2026 and the more powerful Vera Rubin Ultra expected to follow in 2027. Organizations investing in AI want to leverage this capacity as quickly as possible to accelerate time to revenue. For them, a prefabricated modular AI factory may be the best option for fast implementation, even up to 60% faster than traditional construction. The modular approach enables data center construction piece-by-piece so customers can realize value from AI investments as soon as the first components are in place.

How NVIDIA DSX Architecture optimizes AI factory performance
AI factories are evolving into gigawatt-scale compute environments with thousands of racks and unprecedented power and cooling requirements. Supporting that density requires extensive networking, electrical, and thermal infrastructure. NVIDIA DSX is designed to optimize these interconnected systems as a whole, from compute and networking to power and cooling.
The guiding principle behind the architecture is to keep resource consumption as low as possible while maximizing tokens per watt (TPW). This level of optimization requires a deep understanding of various factors, including the availability of behind-the-meter power, network capacity, and water and energy consumption. The more efficient the operation, the better the TPW.
This marks a shift from traditional compute implementations, where servers were typically overprovisioned and underutilized. Now, with AI investments reaching billions of dollars, designing the architecture to maximize throughput has never been more important.
Reference design for modular AI factory
Organizations building AI factories may need guidance because these industrial-scale facilities require integrating networking, power, and cooling infrastructure to optimize efficiency. To that end, Schneider Electric works with NVIDIA to support customers building AI factories. We have made two significant DSX architecture-related moves:
- Released Reference Design 115, modularizing the DSX architecture to accelerate AI factory deployment
- Reintroduced our Power Modules, Power Skids, Data Halls, All-in-One Modules, and IT Pods as RapidScale, which is Schneider Electric’s industrialized solution for designing, delivering, and supporting modular AI infrastructure at scale.
The reference design provides a pre-engineered blueprint for a fully modular AI factory built on DSX principles of output maximization, balanced with optimized resource consumption. The design calls for a completely modularized scalable unit and deployment unit. The scalable unit, which includes the white space, is built around Schneider’s RapidScale IT Pods, which are optimized for high-density AI workloads and deploy 80% faster than traditional stick-built pods or hot-aisle containment systems (HACS).
These IT Pods or as described in the DSX architecture as compute and support pods are supported by skidded prefabricated cooling plants, power distribution units (PDUs), remote power panels (RPPs), and fan walls, supplying liquid & air cooling and power to the pods. Four scalable units are within a deployment unit, supported by outdoor power and cooling modules. The deployment unit is designed to scale repeatedly based on AI Factory capacity needs. This supports a parallel construction approach, with units added as compute needs increase.

The design is built around RapidScale units pre-engineered, assembled, and validated at our factories. We ship them to the facility site with all the power and cooling infrastructure needed to support white space. The RapidScale approach industrializes the DSX architecture, enabling customers to accelerate time to first token (TTFT).
RapidScale delivers deployment speed with a pre-engineered solution optimized for DSX. Units are delivered on site ready to be plugged in. This supports a parallel construction approach, with units added as IT expands. Because we test all module components at our factory, on-site commissioning is minimal.
How industry collaboration advances modular AI factory innovation
Schneider Electric drew on our vast experience with modular designs and our collaboration with other industry leaders to develop AI-ready RapidScale solutions and the DSX reference design. We have delivered prefabricated data center modules for more than two decades, and now we have optimized them for AI deployments. Recently, our RapidScale Power Skids earned an industry first UL 2140 certification, and our RapidScale Power Modules meet UL2755, adhering to strict safety, performance, and integration standards.
Our work with partners like NVIDIA allows us to keep up with fast technology developments so we can support partners and customers alike as they move forward with AI implementation. The DSX reference design represents the first phase of modularized AI factory implementations. As new GPUs are introduced, the design will evolve to accommodate changes and continue helping customers accelerate time to token and maximize tokens per watt. To learn more view the Reference Design 115.
Add a comment