Summary
- Securing power is only the first step toward AI readiness; electrical, cooling, and IT infrastructure must convert those megawatts into deployable critical IT capacity.
- TeraWulf is transforming the site of a former coal-fired power plant into a 500 MW AI campus on an accelerated timeline.
- A proven Motivair by Schneider Electric thermal platform helped support high-density AI infrastructure and speed of deployment.
- The scalable thermal architecture supports future high-density AI workloads and potential expansion to approximately 750 MW.
Author: Andrew Whitmore, Vice President of Sales at Motivair by Schneider Electric
In the AI race, securing power is only the starting point. Available megawatts do not automatically translate into AI data center capacity. The competitive advantage lies in how quickly data center operators can operationalize that power, which means coordinating the electrical, cooling, and IT infrastructure required to convert megawatts into AI-ready infrastructure.
Achieving this transformation requires a carefully orchestrated effort across the entire facility. Data center developer and operator TeraWulf proved how making smart architectural decisions early in the building process can accelerate timelines without sacrificing long-term efficiency or scalability.
On the shores of Lake Ontario near Buffalo, TeraWulf has rapidly expanded Lake Mariner from a proof-of-concept into a large-scale, phased digital infrastructure campus. Such builds typically take around 36 months, but by partnering with Motivair by Schneider Electric and other strategic vendors, TeraWulf leveraged a scalable liquid-cooling infrastructure that kept pace with the accelerated deployment and enabled the aggressive timeline. The facility known as Lake Mariner Data will deliver 500 MW of gross capacity across six buildings, with plans to expand to 750 MW.

Building an AI-ready data center starts with power and planning
As demand for AI grows and rack densities increase, access to power has become one of the biggest constraints on new AI data center development.
“In today’s AI infrastructure market, the critical question is where you can secure reliable power. TeraWulf prioritizes sites with access to utility-scale power and transmission infrastructure, which can materially shorten development timelines relative to traditional greenfield projects.” the company says.
Power availability gave TeraWulf a strong head start, but rapid deployment also depended on getting the design right from the beginning. That included selecting the right data center cooling architecture and coordinating the mechanical, electrical, and IT systems early to support higher rack densities, future GPU generations, phased campus expansion, and long-term operational efficiency.
TeraWulf’s compressed timeline meant every infrastructure dependency was important, because any deviation could delay the project’s critical path toward timely completion.
Turning power into AI capacity with the right thermal architecture
TeraWulf’s cooling infrastructure needed to do more than meet immediate thermal requirements. It had to be engineered and deployed at the pace of the build, ensuring cooling did not become a constraint as available power was converted into operational AI capacity.
Selecting the right thermal architecture is an early, critical decision for AI deployments. Rack density, facility constraints, deployment timelines, and operational goals determine how cooling technologies are applied. At Lake Mariner, the priority was proven high-density cooling technology that could meet the deployment’s thermal requirements, keep pace with an accelerated build, and provide a scalable foundation for continued expansion.
Motivair by Schneider Electric brought decades of experience supporting high-density supercomputing environments to the Lake Mariner deployment. Combined with proven rear door heat exchanger (RDHx) technology, that experience gave TeraWulf greater confidence that its thermal infrastructure could keep pace with the accelerated build, perform reliably once operational, and scale as compute requirements evolved.
That adaptability matters because AI compute evolves much faster than the facilities supporting it. Each new generation drives higher rack densities and new thermal requirements, while the underlying data center infrastructure must support multiple generations of compute.
TeraWulf needed a cooling architecture that could adapt and support future upgrades and expansion.
That requirement was particularly important given TeraWulf’s plans for future expansion. The goal wasn’t simply to provide a cooling infrastructure for the initial deployment, but to establish an architecture that could be repeated and adapted as additional AI capacity came online.
Motivair ChilledDoor® technology formed a key part of that platform, delivering up to 75 kW of cooling directly at the rack. In three of the buildings at Lake Mariner, the ChilledDoor system uses fans to draw room air through the servers while circulating cool facility water through the rear-door heat exchanger (RDHx) to achieve 100% heat removal and maintain room-neutral cooling. The system also integrates in-rack manifolds and in-rack coolant distribution units (CDUs), as well as a custom water-cooled loop for direct liquid-cooled (DLC) servers.
Together, these technologies created a proven, scalable thermal platform capable of keeping pace with deployment while adapting to future compute requirements. Cooling became part of the pathway from available power to operational AI capacity rather than a constraint on it.
Lessons for building future AI factories
TeraWulf’s experience shows that building AI infrastructure is not just a race to secure power. Success depends on how quickly that power can be converted into deployable critical IT capacity, and the cooling architecture is central to that equation. Thermal infrastructure has become a strategic architectural decision that directly influences deployment speed, scalability, and operational flexibility. As such, it needs to be included in planning from Day One. Validated cooling infrastructure from Motivair by Schneider Electric helped TeraWulf keep pace with its compressed construction timeline while providing the reliability and scalability needed for continued expansion at Lake Mariner.
The broader lesson for AI data centers is clear: securing power is only the starting point. Turning available megawatts into AI-ready infrastructure requires coordinated planning across electrical, mechanical, cooling, and IT systems so they can scale together as compute requirements evolve. Watch the broadcast to learn more about how TeraWulf accelerated the path from available power to AI-ready capacity
Add a comment