The modernisation imperative for data centre resiliency: Riding the heatwaves

Our climate is changing, and quickly. In the last few weeks, Europe has faced some of the hottest temperatures on record, with the World Meteorological Organization citing the impact of heatwaves on human health, agriculture, infrastructure, and major weather events including storms, drought and wildfires taking place across the region.

At the same time, the UK Met office has reported the number of days where average temperatures exceeded 28C has doubled, while the number of days with temperatures reaching 30C or more has trebled.

Heatwaves are no longer isolated events—they are becoming a recurring operational challenge that organisations must proactively address. In the face of more frequent heatwaves, and increasingly sustained periods of high average temperatures, the strain on mission-critical systems is exacerbated. They increase the risk of data centre overheating.

During these times, data centre physical infrastructure components including power, cooling systems, GPUs and servers must all work harder to main reliability – primarily because higher temperatures mean greater stress and consequently, a greater chance of failure. Stress points must, therefore, be quickly identified to mitigate downtime, and energy technology, data intelligence, and real-time analytics are vital to enable preventative measures.

As unexpected weather events increase in frequency and severity, how can data centres begin to cope with the thermal management challenges associated with heatwaves, and mitigate them?

Modernising data centre cooling for greater resilience and reliability

Today, data centre modernisation is no longer driven solely by AI adoption. As heatwaves become more frequent, workloads continue to intensify, and with extreme temperatures placing greater pressure on critical infrastructure, organisations must ensure their cooling systems are capable of delivering reliable performance and optimal efficiency under increasingly challenging conditions.

Why is AI data centre cooling important?

As organisations deploy larger GPU clusters and support increasingly demanding AI workloads, traditional cooling approaches may become insufficient. Modern AI environments require advanced thermal management strategies designed for high-density computing, making AI data centre cooling a growing priority for operators seeking to protect critical infrastructure investments. As the largest consumer of power away from the IT and GPUs, cooling system capacities must be continuously reviewed to ensure the highest levels of energy efficiency, resiliency and sustained performance.

For facility operators experiencing continued hotspots, outages or airflow issues, using a Computational Fluid Dynamics (CFD) platform allows them to quickly model and identify issues, and validate any changes to cooling capacities before the work is undertaken.

Operators can add simple fixes like blanking panels, test their system against a range of dynamic load profiles, or implement a Hot or Cold-Aisle Containment system (HACS / CACS) like Schneider Electric’s EcoStruxure™ Row Data Centre, allowing them to quickly improve cooling at the touch of a button.

Additionally, adding or upgrading a CRAC (Computer Room Air Conditioning) system may improve thermal dynamics immediately – allowing operators to improve spend, minimize energy wastage and ensure that the data centre is performing at optimum performance during peak temperatures. 

However, modernisation should not stop at infrastructure upgrades alone. Regular servicing and planned preventative maintenance must form a core part of seasonal readiness strategies. Routine maintenance helps extend equipment life, optimise overall data centre performance and identify potential issues before they escalate into critical failures. Operators should also ensure cooling systems are tuned to perform efficiently during the summer months while remaining optimised for lower-demand winter conditions.

How software and services support reliable data centre operations

Modernisation is most effective when paired with intelligent software and expert services that provide continuous oversight. Whether deploying AI workloads in enterprise, cloud, or edge environments, maintaining optimal data centre temperatures is paramount to deliver the highest standards of uptime – and protecting your investment as heat can lead to failure and chips are an expensive investment for data centres.

High-density racks, for instance, are sensitive to increased power fluctuations and like traditional servers, changes in temperature.  During times of increased grid stress or higher external temperatures, there is a greater likelihood of outages, making server or GPU reliability harder to assure.

For enterprise, hyperscale, neocloud, and colocation operators seeking to mitigate these issues, using advanced software and services, can reduce power, cooling and electrical failures by up to 70% – combining real-time analytics with data-driven insights to identify hotspots, faulty power and cooling systems, and proactively deploy service personnel to remediate them.

Building heatwave-resilient data centres for the future

Heatwaves may be unavoidable, but downtime doesn’t have to be. Modernising cooling infrastructure, implementing preventative maintenance and leveraging real-time operational intelligence can help data centres remain efficient, resilient and always available.

Schneider Electric’s data centre infrastructure portfolio including hybrid cooling systems, DCIM software and lifecycle services provide the foundation operators and owners need to keep critical infrastructure running—regardless of the temperature outside.

To learn more about our end-to-end AI-ready infrastructure solutions, advanced data centre cooling technologies and strategies for AI data centre cooling, visit Schneider Electric’s AI Factory hub.

Add a comment

All fields are required.