Traditional AI infrastructure models are reaching operational limits at AI factory scale

AI infrastructure is reaching new operational limits

For decades, data center infrastructure and compute platforms evolved largely independently. Organizations selected servers, storage, and networking technologies, then designed facility infrastructure around them. 

AI is changing that model. 

The latest generation of AI platforms is driving unprecedented increases in power density, cooling requirements, and operational complexity. Deployments now routinely target rack densities exceeding 200 kW, rely on liquid cooling technologies, and require tightly coordinated interactions between compute, power, cooling, and networking systems. 

At these scales, infrastructure decisions directly influence performance, reliability, efficiency, and deployment timelines. 

As a result, many organizations are facing a new challenge: 

How do you deploy AI fast enough, at scale, without failure?  

The answer requires a fundamental shift.  AI infrastructure must be co-engineered and jointly validated alongside the compute platform, not retrofitted after.

AMD and Schneider Electric  EcoStruxure reference design 121.

The challenge: Infrastructure is the bottleneck to AI factories 

The rapid growth of AI workloads is placing new demands on data center environments. 

Modern AI clusters require: 

  • Rack densities reaching up to 246 kW per rack 
  • High-capacity liquid cooling architectures 
  • Multi-megawatt power and cooling systems 
  • High levels of resilience and operational availability 
  • Accelerated deployment schedules without compromising reliability  

Traditional deployment methodologies often treat infrastructure as a downstream activity. Compute platforms are selected first, followed by the design of power and cooling systems required to support them. 

However, at AI factory scale, this sequential approach introduces significant risk. 

Power distribution architectures, cooling technologies, floor layouts, thermal management strategies, and operational software all influence the ability of a facility to support high-density AI workloads. Design decisions made in one area can directly affect performance and reliability in another. 

As rack densities continue to increase, infrastructure is no longer a passive foundation. It has become a core component of system design. 

What is a reference design? 

A reference design is a validated architectural blueprint that responds to a workload’s current and future growth requirements. Infrastructure components and the compute platform are designed to comply with this blueprint during implementation. 

Rather than requiring operators to design every aspect of a deployment from scratch, reference designs provide engineering guidance for power distribution, cooling systems, rack layouts, facility planning, and operational management. They help establish a proven framework that can be adapted to individual deployment requirements. 

For AI environments, reference designs are becoming increasingly important because infrastructure requirements are closely tied to platform characteristics. Power consumption, thermal loads, liquid cooling requirements, networking density, and rack architecture must all be considered together to achieve predictable performance and reliability. 

As AI deployments continue to scale, reference designs provide a structured approach for translating platform specifications into deployable data center architectures. 

The shift: Co‑engineering and joint validation  

To overcome these challenges, leading organizations are shifting to a new model:  

Co-engineer infrastructure and compute from day one and validate the system before deployment. In this model, compute and infrastructure are treated as a single system, with design decisions made simultaneously rather than sequentially.  

This model ensures:  

  • Infrastructure aligns to platform requirements upfront  
  • Performance is optimized before installation  
  • Risks are identified and mitigated early  

From an AMD platform perspective, architectures like the AMD Helios™ rackscale solution are designed to deliver breakthrough compute performance through higher density, bandwidth, and system integration.  

This reflects a broader reality:  

Co‑engineering is no longer an optimization. It is a requirement. 

What a jointly validated AI infrastructure reference design looks like

A true reference design delivers more than guidance. It provides a deployment ready blueprint for AI infrastructure. A jointly validated reference design is a pre-engineered architecture where compute, power, cooling, and networking systems are designed and tested together before deployment.  

The data center reference design for the AMD Helios™ rackscale solution, developed by Schneider Electric and AMD Ecosystem alliance, integrates:  

  • Power systems for multi-megawatt AI clusters (up to 10.4 MW of IT capacity) 
  • Liquid-first cooling architectures with hybrid support (84% of heat removed via liquid, 16% via air) 
  • IT layouts optimized for GPU clusters (up to 246 kW per rack) 

Lifecycle and digital layers via EcoStruxure™ for Data Centers

Each design is:  

  • Co‑engineered with AMD Helios™ rackscale solution requirements  
  • Validated via electrical and thermal simulations  
  • Designed for greenfield and retrofit use cases  

The result is a jointly validated architecture that removes uncertainty and accelerates AI Factory deployment.  

This collaboration ensures that both compute performance and infrastructure readiness are validated together, eliminating the gaps that traditionally slow down AI factory deployment. 

Real world AI factory deployment scenarios  

Greenfield AI Factory  

  • Up to 10.4 MW IT load  
  • 2,880 GPU clusters  
  • Tier III availability  
  • Up to 246 kW per rack  

High‑Density Retrofit  

  • Single AI pod transformation model  
  • Replacement of multiple legacy racks  
  • Incremental evolution to AI Factories  

In both scenarios, infrastructure is not adapted after the fact. It is co‑engineered and validated as a unified system. 

Why co‑engineered designs reduce risk  

Joint validation delivers:  

  • Faster deployments with pre‑defined architectures  
  • Reduced deployment risk from upfront validation  
  • Enhanced efficiency with optimized PUE  
  • Operational visibility via digital twins and monitoring  

Instead of reacting to failures, organizations deploy systems that are ready from day one.  

The Future: Infrastructure Defines AI Scale  

AI Factories are growing faster than infrastructure can evolve.  

The industry is moving toward:  

  • Integrated infrastructure ecosystems  
  • Platform aligned reference designs  
  • Co‑engineered power, cooling, and IT systems  

For hyperscalers and cloud providers, this is not a design preference. It is the foundation for scaling AI.  

Take the next step  

The Data center reference design for AMD Helios™ rackscale solution provides a scalable, validated blueprint for modern AI infrastructure.  

As AI scales, infrastructure is no longer just an enabler. It is the primary constraint determining how quickly and reliably AI can be deployed. 

Explore how co‑engineered infrastructure can accelerate deployment, reduce risk, and enable AI at scale. Download the Data center reference design for AMD Helios™ rackscale solution and engineering package.   

Add a comment

All fields are required.