The next phase of the digital economy will not be limited by compute – it will be defined by power. For decades, data centers scaled predictably, with racks consuming 5 to 15 kW and infrastructure evolving incrementally. That model no longer applies. The rise of AI factories – built to train and run large-scale models – is driving an unprecedented surge in energy demand, pushing power requirements from megawatts to gigawatts. Enter the AI factory.
This shift introduces a fundamental constraint: the ability to access, manage, and optimize energy at scale. As a result, AI is no longer just a technology challenge – it is an infrastructure and energy orchestration challenge. Tech companies are now facing incredible, gigawatt-scale power needs while staring down grid connection delays that can last for years. To solve this, the industry is realizing it must look at the big picture. Operating an AI factory reliably and sustainably means designing a smooth, uninterrupted power journey from the massive utility connection right down to the tiny processing chip. We call this the “grid to chip” approach.

The waiting game and the rise of energy parks
Imagine building the world’s most advanced data center in just 18 months, only to be told you must wait five to seven years for the local power company to turn the lights on. That is the challenge facing today’s major tech builders. The old way of simply plugging a building into the local power grid is broken when it comes to AI.
The amount of energy needed is simply mind-boggling. Some new AI campuses require up to 10 gigawatts of power, roughly the same amount needed to power the entire city of New York. Our existing electrical grids were never built to handle these massive, sudden jumps in demand. Power availability has become the ultimate choke point for AI scalability. While early warnings in hubs like Virginia projected connection delays out to 2030, the reality is escalating quickly: industry leaders are now facing transmission grid connection wait times of up to 12 years for new large-scale data centers.
With the median wait time for US grid interconnection now stretching to five years, data center operators are shifting their strategies. To bypass these delays, operators are funding localized, dedicated energy parks developed and managed by Independent Power Producers (IPPs). These multi-source parks, often combining gas turbines, solar arrays, and large-scale battery storage, operate strictly ‘behind-the-meter.’ Because they are grid-independent, they do not initially draw from or add strain to public utilities. This localized approach allows operators to slash time-to-power down to just 24 to 36 months, while simultaneously securing greater control over energy costs, resilience, and sustainability outcomes.
Building faster with factory-built systems
Finding power is just step one. The next challenge is building complex physical sites fast enough to meet tight launch schedules. Speed has become a competitive differentiator in the AI race. However, traditional construction approaches cannot keep pace with the scale and complexity of AI infrastructure, including supply chain headaches and a shortage of skilled workers.
The strategic shift is to move the hardest work off the messy construction site and into a controlled factory. Builders are now using prefabricated power modules. These are ready-made blocks that include all the necessary power controls and battery backups in one neat package. This plug-and-play method saves months of waiting and reduces mistakes on the actual building site. It is also much safer, as it lowers the risk of dangerous electrical sparks when the system is turned on for the first time.
On top of that, engineers use pre-tested blueprints to plan these giant facilities with pinpoint accuracy. These designs are ready months before the newest AI chips even hit the market, ensuring the building is perfectly matched to the technology.
This shift delivers three critical advantages: accelerated deployment timelines, improved quality and reliability, and reduced on-site labor dependency. In a market where months can define competitive leadership, modularization is no longer optional – it is essential.
Inside the room: Handling the heat and power
Once the electricity reaches the building, the inside of an AI factory looks very different from an old-school data center. The actual space for computers is shrinking, while the room needed for heavy power equipment is growing fast. Inside the computer racks, the power density is going through the roof. Next-generation setups can draw an astonishing 200+ kilowatts of power per rack.
Trying to push that much energy through traditional electrical wiring creates a lot of heat and wastes a ton of energy. To fix this, the industry is switching to a much higher voltage system, known as 800 VDC, right inside the rack. By doubling the voltage, the electrical current drops in half. This means engineers can use smaller wires, reduce energy waste and heat, and make the entire facility run much more efficiently.
The Digital layer: Orchestrating the AI factory
Even with all this amazing physical hardware, the AI factory still needs a brain. To manage enough power for a small city, the facility has to be run by smart software.
This predictive modelling starts before a single brick is laid. Engineers use advanced software to build a “digital twin” of the entire power system. By testing for problems in a virtual world first, they can fix mistakes early and speed up the real-world building process. Once the facility is running, a central Energy Management System acts like an air traffic controller. It constantly monitors and balances the power coming from different sources, making split-second decisions to keep the facility stable.
Finally, artificial intelligence is used to monitor the health of the entire system, providing a few massive benefits:
- Stopping Outages: Smart software spots problems early and cuts the risk of unexpected power failures by up to 75%.
- Keeping Workers Safe: By predicting exactly when maintenance is needed, facilities reduce hands-on repair work by 40%.
- Making Equipment Last: Constant, smart monitoring helps crucial power parts live up to 25% longer.
The future is grid to chip
The AI revolution is pushing the boundaries of what is physically and digitally possible in the technology world. Building the infrastructure of tomorrow requires an entirely new approach that moves far away from bespoke, piecemeal solutions. Success in this demanding new era means seamlessly orchestrating the entire energy chain, all the way from the localized power park down to the high-density server rack. Companies can no longer rely on a fragmented power system for their most critical assets; they require a comprehensive, integrated, and smart power train.
Schneider Electric is uniquely positioned to enable this transformation. With deep expertise across power, software, and services, Schneider delivers a fully integrated, end-to-end solution – from grid connection and on-site generation to modular infrastructure and rack-level optimization. In the race to build AI factory at scale, power is the new frontier – and mastering it will define the leaders of the next decade.
To dive deeper into these insights and hear directly from the experts, you can learn more by watching the full broadcast of Powering the AI factory: The grid to chip journey, available on demand.
Add a comment