The uninterruptible power supply (UPS) used to play a passive role in data center infrastructure, but now it’s at the center of operations. AI workloads are driving profound changes in data center power dynamics, which new intelligent, compact UPSs are designed to address. As such, the UPS acts as a bridge between the facility and the power grid, buffering grid volatility and conditioning power to protect both the grid and the compute layer.

Changing data center power dynamics
Data center power loads were relatively stable until recently. But AI clusters introduce synchronized GPU (graphics processing unit) activity that triggers rapid load swings, high transient peaks, and sharp ramp rates – all within seconds, resulting in millions of load cycles every year.
Power loads can swing from 30% to as much as 150% in short bursts. In the past, a load above 100% was considered abnormal and a cause for alarm, but today it is considered normal behavior to accommodate AI load variations. These new power dynamics require a new generation of intelligent power systems.
Preventing load instability
Dramatic data center load swings can destabilize the electric grid. Operators are not equipped to balance the power supply when variations of hundreds of megawatts occur in just seconds.
This is where UPS’s new role comes in. Load-flattening and fault ride-through (FRT) in some models help maintain grid stability. FRT allows UPS to remain connected and continue operating through voltage dips or transient faults, rather than disconnecting immediately, thereby avoiding additional instability. Such features protect both sides of the grid connection while also helping data centers comply with federal and state requirements being introduced to maintain grid stability.
Advanced UPS capabilities also begin when data centers generate their own power with gas turbines or diesel generators. Because of power supply constraints, some AI data centers, such as the massive Stargate facility under construction in Abeline, Texas, operate off-grid, generating their own electricity.
Load variability can damage power-generating equipment. UPSs with load-smoothing features, including some new Schneider Electric Galaxy V series models, can switch to protect gas turbines and diesel generators. This occurs when load variations reach 1% per second with gas turbines, and 10% per second with diesel generators.

How to protect AI investments
AI data center operations are changing the financial consequences of power instability. In traditional data centers, brief power events were often viewed as operational disruptions. In AI environments, they can directly threaten the value of massive compute investments. Even minor disturbances can interrupt GPU training cycles, slow inference operations, reduce utilization of expensive AI clusters, and delay time to insight for business-critical applications.
The stakes are especially high because AI workloads depend on tightly synchronized, high-density systems operating at extreme performance levels. As AI deployments grow in scale and urgency, power resilience is no longer simply a facilities concern. It has become a business continuity, investment protection, and ROI requirement that directly affects the success and profitability of AI initiatives.
Why the UPS can’t be an afterthought
Planning for AI-ready data centers should include power architecture decisions made long before servers are installed. Traditional “UPS-last” design approaches, where backup power is treated as a downstream utility component, are increasingly out of step with the realities of AI deployments.
AI workloads introduce rapid load swings, high rack densities, and grid-sensitive power dynamics, requiring the UPS to play a more strategic role from the outset of the design process. By treating the UPS as a foundational element alongside computing, cooling, and facility planning, operators can build infrastructure that scales more efficiently, improves resilience, and better supports future grid-interactive capabilities.
AI-tolerant UPS technology
Deploying AI-tolerant UPSs, such as Schneider Electric’s Galaxy VXL, delivers benefits that extend far beyond backup power. Future features such as AI load smoothing and FRT will help operators stabilize dynamic AI workloads while reducing the need to overprovision infrastructure for peak demand. This enables a more efficient power architecture that lowers capital costs, improves utilization, and supports long-term scalability as AI environments continue to grow in density and complexity.
The Galaxy VXL UPS also addresses one of the biggest constraints in AI data centers: space. The latest models are up to two times denser than previous generations and occupy 52% less footprint in high-density environments, freeing valuable floor space for revenue-generating compute infrastructure. In addition, Schneider Electric closely aligns UPS innovation with NVIDIA GPU roadmaps to ensure power systems keep pace with rapidly increasing AI performance demands.
As AI deployments expand, UPS technology will play an increasingly strategic role. In addition to protecting critical infrastructure, AI-ready UPSs also help optimize AI investments, enhance operational resilience, and mitigate the impact of large-scale AI workloads on the electric grid. Learn how the Galaxy VXL helps stabilize AI workloads and optimize power performance.
Add a comment