Seven years ago, if someone needed new switchgear, they called their supplier, agreed on a lead time measured in weeks, and moved forward. Today, that same customer is asking for three times the volume, at higher amperage, packed into smaller footprints, and delivered within timelines that don’t reflect the realities of today’s supply chains.
And that is the gap where most projects start to drift. “How things worked before” still shapes expectations, but conditions behind those expectations have shifted.
Demand has accelerated, system requirements have become more complex, and the infrastructure needed to support that demand is under pressure to scale in ways it wasn’t designed for. Lead time for some crucial electrical assets is now measured in years. This marks a fundamental shift in supply chain constraints and how they now operate.

Demand has changed in scale and complexity
Electrification is expanding across sectors. Data centers continue to grow, and industrial capacity is increasing. Each installation now requires more power, delivered at higher amperage and voltage levels.
Global data center electricity consumption is projected to double to ~945 TWh by 2030.
Inside the equipment, that growth has direct implications: more power means more copper, more copper increases heat, and heat introduces tighter constraints on design, materials, and performance.
What was once a relatively stable engineering problem is now more challenging. Any increase in power density also increases complexity, requiring greater precision, coordination, and careful integration into the broader system.
Engineering has become a scaling constraint
A single large data center can require thousands of switchgear units, typically 7,000 to 12,000. Each unit must be designed to meet specific requirements for load distribution, protection, and physical layout. At that scale, engineering capacity becomes a defining factor in delivery.
There are different ways to approach this. One relies heavily on customization, treating each unit as unique—but this approach becomes difficult to sustain as volumes increase and timelines compress.
Another focuses on standardization and repeatability, using design-for-manufacturing principles to manage complexity. Organizations that perform well have invested heavily in engineering capabilities and tools to support this approach. Software-enabled design, standardized architectures, and repeatable configurations allow teams to process large volumes of work without introducing unnecessary variation.
Production must scale and become productive quickly
The more difficult challenge is turning that capacity into consistent output within a short timeframe. Across the industry, companies are investing heavily in new facilities, but the real differentiator is how quickly those facilities move from construction to production. A factory that exists on paper doesn’t reduce lead times—operational readiness does: the ability to produce at scale, maintain quality, and deliver reliably.
But upstream supply chain constraints remain. Lead times for large power transformers now often extend beyond 18–36 months, according to the U.S. Department of Energy, creating a structural tension: demand is accelerating, but key elements of the system can’t scale at the same speed.
Workforce capability is a key element
Scaling production also requires scaling people. Hiring at volume is one step, but building capability takes longer.
New employees must be onboarded, trained, and brought to a level of autonomy where they can contribute effectively—a process that can take months and creates another timing gap.
As demand accelerates and capacity is added, workforce capability develops on a different timeline. During that period, organizations must maintain quality, ensure safety, and manage the complexity of a rapidly evolving operation. Capacity can be added quickly, but capability develops over time.
What defines performance now
Consider what that looks like in practice. One manufacturer brought a 500,000-square-foot facility from empty space to $20 million in monthly shipments within four months, with a line of sight to $50 million.
That didn’t happen by accident. It required engineering software acquired years earlier and deployed as a core production tool, along with design-for-manufacturing principles applied before the first unit was built—and workforce training running in parallel to construction, not after.
The facility was producing while competitors were still announcing groundbreakings. That is the difference between capital deployed and capital productive.
This is the shift. Performance is about capacity, but also how quickly that capacity becomes usable.
What this shift requires
The organizations that will outperform over the next decade won’t necessarily build the most factories. They’ll build productive capacity faster than everyone else. This means they need to:
- Re-examine the engineering-to-production handoff.
If design and manufacturing aren’t aligned, complexity compounds quickly. - Measure how quickly capacity becomes productive.
Groundbreakings are easy. Reaching $20 million in monthly shipments within four months is not—that’s the metric that matters. - Train the workforce in parallel to construction.
A facility isn’t ready when the ribbon is cut; it’s ready when the people inside can execute.
Planning must catch up to reality
Planning based on past assumptions is now a risk: demand has increased, and system requirements are more complex. Timelines across engineering, production, and infrastructure are no longer as closely aligned.
Organizations moving forward are already adapting how they design, stage, and scale infrastructure in this environment. If you’re reassessing your approach—re-engineering your design process, accelerating production ramp-up, or aligning workforce development with construction timelines—it’s worth starting that conversation now.
Add a comment