Liquid cooling fluid management: How to protect AI infrastructure

Author: Corey Olson, Principal System Innovation Engineer at Motivair by Schneider Electric

Fluid is the lifeblood of data center closed-loop liquid cooling systems. Keeping it in optimal condition is vital to the cooling infrastructure and the high-priced AI systems it protects. Industry guidance from ASHRAE identifies coolant cleanliness as a key requirement for reliable direct-to-chip liquid cooling operation. This means performing regular maintenance and monitoring to prevent deterioration of the fluid and damage to servers and infrastructure.

As with the human body, it’s better to adopt healthy habits for liquid cooling fluid management than to remedy problems caused by poor fluid quality. Having a “fill it and forget it” mindset about liquid cooling can cause big problems. The coolant that flows through a closed-loop system’s pipes, manifolds, and pumps is subject to issues such as metal corrosion, organic buildup, fluid degradation, and loss of thermal conductivity.

liquid cooling management

Poor coolant quality can have serious consequences for closed-loop liquid cooling systems. As coolant degrades, corrosion, particulate contamination, and biological growth can accumulate within cold plates, heat exchangers, and piping, reducing heat-transfer performance and restricting flow. Research on heat exchanger fouling has shown heat-transfer degradation of up to 14% and pressure-drop increases of up to 45% as contaminants accumulate.

Increased fouling also forces pumps and cooling equipment to consume more energy to maintain thermal performance, raising operating costs and reducing overall cooling efficiency. In fact, fouling can reduce heat exchanger efficiency by up to 30%. Because modern AI servers rely on precise coolant flow and heat removal, ASHRAE liquid-cooling guidance notes that even minor fluid-quality issues can increase the risk of thermal throttling, equipment degradation, and unplanned downtime.

A well-defined liquid cooling fluid management regime prevents these scenarios.

Building a liquid cooling fluid management strategy

A successful liquid cooling fluid management strategy requires more than simply filling a system with coolant and expecting it to perform indefinitely. Maintaining coolant health demands a proactive approach that combines regular testing, filtration maintenance, contamination prevention, system redundancy, and continuous monitoring.

Explore liquid cooling solutions for AI data centers

How to test and monitor liquid cooling fluid?

Closed-loop systems dissipate the intense heat generated by high-density AI GPUs. Liquid cooling fluid in closed-loop data center systems typically consists of 75% deionized water and 25% glycol. This mix may differ slightly based on client or equipment specifications. Because it circulates in a closed loop, the fluid does not reveal obvious signs of distress, so you have to look for issues through testing.

How often should coolant be tested in a closed-loop liquid cooling system?

Coolant should be tested at three minimum intervals: at commissioning to establish a baseline, annually during normal operation, and semiannually for systems supporting high-density AI GPU workloads. Periodic coolant testing is much like routine bloodwork for humans—it helps identify developing issues before they impact performance or reliability. Regular analysis is the only way to detect coolant degradation, contamination, or chemistry imbalances that may require chemical rebalancing or a partial coolant replacement.

Coolant filtration: How to maintain filters in liquid cooling systems

Proper fluid management includes regular maintenance of coolant filtration systems. In closed-loop liquid cooling, filters are located in multiple places, including coolant distribution units (CDU) and Rear Door Heat Exchangers (RDHx). Filters prevent particulates from entering pumps or cold plates that absorb heat from GPUs and chips. Cold plate blockages reduce cooling efficiency and can cause chips to overheat.

By their very nature, filters tend to accumulate debris. They catch specks of metal and rubber gaskets, silicates, and microorganisms such as algae and bacteria that thrive in moisture and heat. Dirty filters cause pumps to work harder, reducing efficiency, so it’s important to keep them clean.

Sock filters vs. reusable metal filters: Which to use and when

Different systems use different types of filters. Motivair by Schneider Electric’s closed-loop systems use disposable filters, called “sock filters,” during installation and cleaning/rinsing cycles, but during normal operation, they are replaced with reusable metal filters that can be cleaned. Motivair CDUs employs sensing technology to determine when cleaning is needed. Without sensing equipment, you should do periodic checks at least every six months.

Liquid cooling pump redundancy

Effective maintenance practices start with proper system design. For instance, CDU redundancy design helps with reliability and serviceability. CDUs with two pumps (N+1 redundancy) ensure continuous operation if the primary pump fails or has to be taken offline for maintenance. As part of fluid management, pumps may have to be shut off; a redundant system ensures operational continuity.

How to prevent contamination in closed-loop liquid cooling systems

Proper fluid management prevents system contamination. Here are some recommendations:

  • Use good water. Tap water may contain chloride, magnesium, or calcium, so it’s important to use purified, deionized water to keep systems running at their best.
  • Clean all components. Cleanliness is critical, so be sure to perform a rinse cycle before activating the system. All new hardware should be cleaned and treated before it starts running.
  • Keep the fluid clean. Testing, chemical dosing, fluid replacement, and proper filtration prevent particulates and bio growth from clogging up the works.

Monitoring is also critical to proper fluid management in cooling systems. Advanced monitoring platforms use sensors to detect issues such as leaks and changes in temperature and pressure. Identifying and addressing these conditions early helps prevent damage to expensive AI hardware and protects overall facility operations.

Best practices for liquid cooling fluid management

Effective liquid cooling fluid management is about more than maintaining coolant. It is about protecting the entire cooling infrastructure that supports high-value AI workloads. As the lifeblood of closed-loop liquid cooling systems, coolant must be properly tested, filtered, and monitored to maintain peak performance. Without proactive fluid management, contamination and fouling can accumulate on heat-transfer surfaces, reducing cooling efficiency by as much as 30%, increasing pressure drops, driving higher energy consumption, and placing critical AI hardware at risk.

Regular testing, proper filtration, contamination prevention, redundant system design, and continuous monitoring help safeguard cooling performance, extend equipment life, and prevent costly disruptions. By treating coolant as a critical operational asset rather than a maintenance afterthought, data center operators can improve reliability, maximize efficiency, and protect their AI investments. To learn more about optimizing liquid cooling performance and developing a proactive fluid management strategy, visit our liquid cooling resource site.

Add a comment

All fields are required.