A single cooling failure in a high-density AI data center can trigger thermal runaway in seconds. As GPU clusters push power densities well beyond what traditional air cooling can handle, the question is no longer whether to rethink your maintenance strategy for liquid cooling infrastructure—it is how fast you can do it.
The AI data center liquid cooling market is projected to grow from $3.2 billion in 2025 to $15.3 billion by 2035, a CAGR of 16.9% [Precedence Research, 2024]. With 75% of new data center projects targeting AI workloads and 53% of operators expecting liquid cooling to dominate future high-density deployments [Uptime Institute, Annual Data Center Survey, 2024], the infrastructure landscape is changing fast. Maintenance strategies need to keep pace.
The new reality of AI data center cooling

Direct-to-chip liquid cooling is projected to command 47% of market share by 2025 [Global Market Insights, 2024], with hyperscale AI data centers accounting for 55% of liquid cooling deployments. GPU-based processing and high-performance computing applications generate thermal loads that air cooling simply cannot manage at scale.
But the operational complexity that comes with liquid cooling is less discussed. Coolant distribution units, heat exchangers, precision pumps, and manifold assemblies—whether in direct-to-chip, immersion, or hybrid configurations—introduce failure modes that differ fundamentally from conventional HVAC systems. These are not components that tolerate calendar-based maintenance rhythms designed for a simpler era.
To better understand how failures can arise in such systems, refer to the industry analysis of risks associated with liquid cooling in AI data centers, which highlights material compatibility issues, corrosion pathways, and the importance of engineered system integration.
Why preventive maintenance falls short
Traditional preventive maintenance was built for a more predictable world: lower power densities, simpler architectures, and less instrumented infrastructure. Today’s AI environments combine liquid-to-liquid and liquid-to-air systems that generate continuous streams of operational data from EPMS and BMS platforms. Treating that data as background noise—and relying instead on fixed inspection intervals—means leaving the most valuable maintenance signal on the table.
The cost of that choice is measurable:
- Up to 30% of preventive maintenance tasks may be unnecessary [U.S. Department of Energy, O&M Best Practices Guide, 2010], adding cost without adding reliability.
- Developing failures that emerge between scheduled inspections go undetected until they become critical.
- For liquid cooling supporting AI workloads, that gap translates directly into unplanned downtime and lost computational capacity.
Our recent white paper on AI driven Systemic Condition Based Maintenance (CBM)—Rethinking Data Center Service with an AIDriven Systemic Asset Management Strategy—shows why reactive and calendar‑based models fail in high‑density environments. This shift reinforces the core message of this blog: as liquid cooling becomes essential for AI workloads, predictive and condition‑based maintenance are critical for ensuring thermal stability, resilience, and uninterrupted performance.
The predictive maintenance advantage
Condition-based and predictive maintenance strategies use real-time monitoring, advanced analytics, and AI-driven algorithms to turn maintenance into a competitive differentiator rather than a cost of operations.
- Up to 18–25% overall maintenance cost reduction vs traditional approaches
- 30–50% reduction in unplanned downtime
- ROI of 10:1 to 30:1 within 12–18 months [Deloitte, 2017; Plant Engineering, 2023]
95% of organizations report positive returns, and 27% achieve full payback within the first year. For liquid cooling infrastructure, these benefits are amplified by the complexity and criticality of the systems being monitored.
As AI hardware pushes thermal boundaries to new extremes, it’s worth exploring why singlephase direct liquid cooling improves AI data center efficiency—a breakdown of thermal limits and why liquid cooling has become essential for reliable GPU performance.
Implementing predictive maintenance for liquid cooling: The Schneider Electric approach
This is where generic vendor claims tend to fall apart—so it is worth being specific about what effective implementation actually looks like in practice.
Key monitoring technologies include:
- Vibration monitoring on pumps and cooling distribution units detects mechanical degradation before it progresses to failure.
- Thermal imaging on heat exchangers and coolant distribution manifolds identifies temperature anomalies indicating fouling, flow restrictions, or thermal interface degradation—conditions invisible to scheduled visual inspections.
- Continuous analytics processing monitoring data against failure pattern libraries built from a global installed base, identifying trends and anomalies that human operators might miss.
The differentiator is not the sensors. It is what happens with the data.
Schneider Electric’s next generation of EcoCare for Cooling services will deliver exactly this capability: remote monitoring and data-driven insights that forecast when intervention is needed—with enough lead time to schedule maintenance without disrupting operations. For high-capital liquid cooling infrastructure, the projected ability to extend equipment lifespan by 20-40% through data-driven maintenance timing directly improves total cost of ownership.
The path forward
The data center cooling market is projected to reach $40.72 billion by 2030, growing at a CAGR of 16.46% [Mordor Intelligence, Data Center Cooling Market, 2024]. Organizations that align their maintenance strategy with this infrastructure evolution today will carry a structural advantage in reliability and operating cost over those that wait.
Adopting predictive maintenance for liquid cooling systems is not a technology decision—it is an operational strategy decision. The infrastructure is already generating the data. The question is whether your maintenance model is designed to use it.
Want to learn how Schneider Electric is redefining service for AI data center cooling? Stay tuned for the next generation of EcoCare for Cooling—and explore how our data-driven maintenance approach can help you protect your most critical infrastructure.
Add a comment