Powering the next wave of AI infrastructure with NetShelter Power Shelf

As AI workloads continue to scale at an unprecedented pace, data centers are being pushed to evolve just as quickly. High-density computing environments, especially those supporting next-generation accelerated systems, require not only more power but smarter, more integrated ways to deliver it.

To meet this demand, Schneider Electric is announcing the availability of the NetShelter Power Shelf, delivering up to 33kW at 48VDC for NVIDIA GB200 NVL72 systems. Designed as a high-efficiency power distribution platform, it integrates seamlessly with AI-ready NetShelter Open Architecture racks, bringing reliable, efficient, and scalable power closer to where it is needed most.

AI infrastructure

However, this launch is about more than a single component. It reflects a broader approach to how modern AI infrastructure should be built.

Moving beyond components to complete solutions

While the technical specifications of the NetShelter Power Shelf align with industry-standard designs, the real differentiator lies in how it fits into a larger, unified ecosystem. Rather than offering isolated products, Schneider Electric delivers a fully integrated approach with its EcoStruxureTM for Data Center infrastructure solutions, which spans power, racks, and modular systems.

This means organizations do not have to piece together solutions from multiple vendors. Instead, they can deploy a cohesive architecture designed to work together from day one.

An end-to-end partner for AI infrastructure

AI deployments at scale introduce complexity across every layer of the data center. From power distribution and thermal management to physical infrastructure and scalability, each element must be carefully coordinated.

Schneider Electric’s strength lies in its ability to simplify that complexity. With a global footprint and decades of experience in critical infrastructure, the company serves as a true end-to-end partner for AI-ready environments. The NetShelter Power Shelf plays a key role in this strategy, delivering localized high-density power as part of a broader pod and rack system designed specifically for AI workloads.

Designed for scale and speed

As organizations race to deploy AI capabilities, speed and scalability are critical. Integrated solutions reduce deployment friction, minimize compatibility risks, and enable faster time-to-value.

By combining standardized, high-performance components like the NetShelter Power Shelf with a fully engineered infrastructure stack, Schneider Electric helps customers move from planning to production more efficiently without sacrificing reliability or flexibility.

Enabling the future of AI

The demands of AI infrastructure will only continue to grow. Meeting those demands requires more than incremental improvements. It requires a holistic approach that brings together power, compute, and physical infrastructure into a unified system.

With the introduction of the NetShelter Power Shelf, Schneider Electric is reinforcing its commitment to enabling that future, helping organizations build the resilient, scalable foundations needed to support the next wave of AI innovation. For additional information, explore our end-to-end solutions for AI data centers.

Add a comment

All fields are required.