Building AI factories: Why integrated power and liquid cooling systems are critical for high‑density AI data centers

Executive summary

AI factories are pushing data center power and cooling requirements beyond traditional limits, making integrated AI data center infrastructure essential. As GPU densities rise, operators must adopt an end-to-end approach, from grid to chip and chip to chiller, combining power, liquid cooling, and digital systems into a unified architecture. This integrated model enables faster deployment, improved efficiency, and scalable performance, helping organizations meet growing AI demands.

Key Takeaways
  • AI factories require new infrastructure: High-density GPUs demand advanced liquid cooling and resilient power systems.
  • End-to-end integration is essential: Data centers must be designed holistically—from grid to chip and chip to chiller.
  • Liquid cooling is foundational for AI: Direct-to-chip cooling enables performance at extreme densities.
  • Integrated partners reduce complexity: Single-provider ecosystems improve efficiency and speed deployment.
  • Digital tools and global scale drive success: Modeling, monitoring, and manufacturing capacity enable faster, reliable AI infrastructure growth.

With AI factories pushing power densities beyond traditional infrastructure limits, it has never been more important for data centers to have reliable power and effective cooling. Without them, GPUs cannot deliver full performance. Processors are generating significantly more heat than traditional workloads, requiring advanced liquid cooling systems and methods for effective thermal management.

Why AI factories require a new class of partner with power and liquid cooling expertise

As operators rush to deploy AI factories, they need partners who understand energy transfer across the entire data center stack and recognize that liquid cooling is now a core part of the AI infrastructure delivered end-to-end, from the chip to the chiller. Unlike traditional air cooling, liquid cooling extends directly from the server and requires integrated plumbing systems to circulate coolant between IT equipment and chillers. This complexity impacts every layer of the data center—from the facility to the room, row, rack, and ultimately the chip.

high-density ai data center

Historically, operators sourced racks, power, and cooling from multiple vendors. But as facilities retrofit or build new infrastructure for AI workloads, coordinating multiple suppliers adds risk and complexity. Greater efficiency and reliability come from one integrated partner capable of engineering and delivering a fully synchronized power and cooling ecosystem.

Schneider Electric’s recent acquisition of Motivair augments its end-to-end approach, combining power, liquid cooling, and digital infrastructure, along with a global manufacturing footprint, to help operators deploy AI factories faster and scale with confidence.

Why AI data centers require integrated cooling and power infrastructure

AI requires an integrated cooling approach, unlike the past practice of adding isolated cooling products when needed. It is critical to build the bridge between facilities and infrastructure, enabling operators to treat data center cooling holistically when deploying high-density AI clusters while maintaining reliability and serviceability. For years, Motivair has pioneered advanced liquid cooling that removes heat directly from CPUs and GPUs in high-performance computing (HPC) and exascale environments. The cooling innovations and thermal engineering practices developed for these environments are becoming the foundation for AI data center design.

Motivair by Schneider Electric offers a complete liquid‑cooling ecosystem, including:

Schneider Electric also provides the resilient power infrastructure required to support high-density AI data centers. As GPU clusters push power demand to new levels, reliable uninterruptible power supplies (UPS) systems, power distribution units (PDUs), and electrical distribution become critical to maintaining uptime and performance. Integrated monitoring, global services, and lifecycle support help operators optimize efficiency and sustain operations as AI infrastructure scales.

At AI densities, even minor imbalances between electrical load and thermal rejection can lead to hotspots, throttling, or system instability. A holistic approach ensures synchronized design of power distribution, flow rates, pressure, and heat exchange capacity. This alignment is critical to maintain performance, reliability, and efficiency at scale. Treating one as secondary introduces failure risk in high-density environments.

Global manufacturing capacity: Mission critical to AI data center growth

AI demand is accelerating faster than the infrastructure required to support it. Building AI factories requires specialized cooling technologies, electrical infrastructure, manufacturing capacity, and coordinated global logistics.

AI infrastructure is not just about engineering innovation; it is about who can deliver equipment at scale. It is scaling faster than traditional supply chains can support. Schneider Electric’s global manufacturing network helps close that gap. Motivair by Schneider Electric liquid cooling solutions are produced in the United States, India, and Italy, giving data center operators the geographic scale and production capacity required to deploy high-density AI infrastructure quickly. This global footprint reduces supply chain risk, accelerates delivery timelines, and enables operators to bring AI capacity online faster—supported by the specialized cooling and electrical systems that modern AI factories demand.

The importance of digital design and lifecycle management for AI data centers

AI infrastructure should also be engineered as an integrated platform—and Schneider Electric brings together the power, cooling, and digital capabilities to make it possible. Those include the ETAP (Electrical Transient Analyzer Program) digital twins and software for the design, modeling, and simulation of electrical systems, as well as AVEVA’s industrial software.

By leveraging these platforms, construction teams can design integrated power, cooling, and digital infrastructure before construction starts. Simulation and modeling software make it possible to validate scenarios and provide solutions to issues that arise during construction. This, too, helps accelerate time-to-market to meet the high demand for AI factories.

Post‑implementation, Schneider Electric supports operators through:

  • Real‑time monitoring
  • Optimization software
  • Predictive maintenance
  • Lifecycle services

Scaling AI factories requires integrated power, cooling, and digital infrastructure

Scaling successfully in the AI era requires a new type of infrastructure partner. Building and operating AI factories demand deep expertise across power, cooling, and digital infrastructure, combined with the ability to deploy these systems reliably on a global scale. That’s why Schneider Electric is integrated into the broader AI ecosystem, working in close collaboration with chip designers like NVIDIA, server manufacturers, and other technology providers, rather than operating as a standalone vendor.

Schneider Electric, together with Motivair, understands the realities of building and operating AI factories offering:

  • Integrated power + liquid‑cooling architecture
  • End‑to‑end thermal and electrical design
  • Chip‑to‑chiller expertise
  • Global manufacturing capacity
  • Digital design, modeling, and lifecycle support

Ready to build AI‑ready infrastructure?

Discover how Schneider Electric and Motivair can help your organization deploy integrated power, cooling, and digital infrastructure designed for the next generation of AI factories.

Add a comment

All fields are required.