In recent years, AI has quietly rewritten assumptions about thermal management in data centers. High-density GPU workloads operate at sustained utilization levels that traditional workloads rarely demand, producing concentrated heat loads that challenge airflow-based architectures and require liquid cooling.
In this environment, cooling performance is no longer just about maintaining safe operating temperatures. It directly influences AI uptime, token generation rates, and the consistency of model training and inference. As organizations invest heavily in accelerated computing, many are discovering that effective data center thermal management is a prerequisite for predictable performance and a critical layer of infrastructure risk management.

Direct liquid cooling for AI data centers enables next-generation infrastructure
Operators are weighing multiple data center thermal management approaches, from stretching air cooling beyond practical limits to exploring single-phase immersion and direct-to-chip designs. In that landscape, direct liquid cooling (DLC) has moved beyond an efficiency upgrade to an enabler of technology for next-generation accelerators.
Among the available options, single-phase DLC has gained traction for its performance and practicality. Compared to alternative approaches, it offers:
- Efficient heat capture at the source — removing thermal load directly from CPUs and GPUs
- Operational familiarity — allowing integration with existing data center practices and workflows
- Serviceability advantages — enabling easier maintenance compared to full immersion approaches
- Scalable deployment models — supporting both greenfield AI factories and brownfield retrofits
GPU power is rising rapidly as AI accelerators scale. NVIDIA’s H100 operates at roughly 700 W, while the next-generation Blackwell B200 reaches nearly 1,000 W per GPU. Future architecture, including NVIDIA’s Rubin platform, is expected to push power envelopes even further. As accelerator power climbs toward the kilowatt range, the thermal demands placed on AI servers and data centers are increasing dramatically, forcing operators to rethink how heat is removed from high-density compute environments.
Thermal modeling illustrates why traditional cooling methods are reaching their limits. According to Dell’s comparative study of server cooling technologies, single-phase direct liquid cooling maintained chip-to-coolant temperature differences of roughly 17 to 20 °C at ~500 W processor loads, while comparable air-cooled systems exceeded 60 °C under similar conditions.
Among the cooling approaches evaluated, direct-to-chip liquid cooling delivered the most effective thermal transfer between silicon and coolant, reinforcing why it is increasingly viewed as the most practical and scalable architecture for high-density AI workloads.
Key technologies supporting liquid cooling for AI data centers
At the architectural level, this effectiveness is driven by a coordinated ecosystem of technologies that many operators are integrating into rack design. These components work together to create stable, repeatable cooling environments for high-density AI infrastructure:
- Cold plates — remove heat directly from CPUs and GPUs at the chip level
- Coolant Distribution Units (CDUs) — regulate flow, pressure, and temperature while decoupling facility and IT loops
- In-rack manifolds — distribute coolant efficiently across high-density racks and accelerator clusters
- Rear door heat exchangers (RDHx) — The ChilledDoor can capture residual heat and support hybrid cooling strategies alongside DLC
AI-ready cooling architecture transforms liquid cooling from a component-level enhancement into a scalable rack-level foundation for AI deployments, enabling consistent performance across legacy environments and next-generation infrastructure.
Liquid cooling as a revenue protection layer for AI operations
Cooling has taken on a new business dimension. Thermal instability can hinder performance, reduce accelerator utilization, and delay AI outcomes – risks that impact revenue realization and infrastructure ROI.
Well-designed liquid cooling environments support sustained GPU performance, predictable throughput, and greater confidence in scaling AI workloads. For many organizations, cooling is evolving from a background utility to a performance assurance layer that protects AI investments.
ESG benefits of single-phase direct liquid cooling in AI data centers
When considering liquid cooling vs. air cooling, another factor operators need to consider is sustainability. DLC is a more sustainable data center cooling method that provides infrastructure efficiency at scale.
By reducing energy consumption, lowering reliance on airflow-intensive systems, and enabling greater compute density per megawatt, liquid cooling helps operators maximize limited power resources as AI demand accelerates. This improves power usage effectiveness (PUE) and supports environmental, social, and governance (ESG), positioning liquid cooling as a foundational element of scalable, efficient AI data centers.
Sustainable data center cooling
For teams planning high-density AI workloads, figuring out how to integrate liquid cooling into existing and future infrastructure is now a priority. Evaluating single-phase direct liquid cooling as part of overall AI architecture planning can help support sustained accelerator performance, improve infrastructure efficiency, and enable repeatable AI-ready designs across both greenfield and retrofit environments.
To explore how liquid cooling architectures can support your AI strategy, review our liquid cooling solutions for AI data centers to identify deployment considerations and best practices.
Add a comment