The explosive growth of the data center industry—driven heavily by artificial intelligence (AI) and hyperscale computing—is reshaping the stability and resiliency expectations of the electric grid. As data centers account for a larger share of overall electricity demand, they are no longer passive consumers of power; they are emerging as critical actors influencing grid behavior.
Rising data center energy demand is creating deeper operational and reliability interdependencies between data centers and the grid. Below are the key drivers behind this growing impact on grid.

1. AI and hyperscale compute growth
The surge in AI workloads is dramatically accelerating data center power consumption.
The Lawrence Berkeley National Laboratory projects U.S. data center demand to increase from 176 TWh in 2023 (4.4% of U.S. electricity consumption) to 325–580 TWh by 2028 (6.7–12%). With this rapid rise, data centers are becoming one of the fastest‑growing and most influential load categories on the grid.
2. Regional concentration of facilities
Another critical factor shaping data center–grid interdependence is geographic concentration. Site selection for data centers is typically driven by access to reliable power, available land, favorable regulation, and skilled labor. As a result, development is highly concentrated.
According to CNBC, only four U.S. states currently host more than 200 data centers, creating pockets where data center loads represent a substantial portion of local grid demand. This growing concentration means local grids and data centers must adapt to work together for a reliable grid environment.
Why data center behavior matters during grid disturbances
When transient faults occur on the transmission system, most data centers—regardless of their distance—automatically reduce the amount of power they draw from the grid and switch to backup sources such as uninterruptible power supply (UPS) systems. This design protects sensitive IT equipment and ensures uninterrupted service for customers.
However, in regions with dense clusters of data centers, this collective response can cause sudden, large drops in demand within milliseconds. This leads to immediate supply‑demand imbalances and frequency deviations that affect the entire power system. Without rapid intervention, such deviations can trigger automatic generation tripping and potentially escalate into widespread outages.
Real‑world events highlight the outage risk
- Ireland, May 2025:
A remote transient fault caused 387 MW of data center load to drop instantly—52% of all data center demand at that moment—forcing EirGrid to activate emergency stability measures. - Northern Virginia, July 2024:
A voltage fluctuation caused 60 data centers to disconnect simultaneously, creating a 1,500 MW power surplus and requiring urgent adjustments to avoid cascading outages.
With similar incidents occurring globally, Transmission System Operators (TSOs) are introducing Fault Ride‑Through (FRT) requirements for large loads, including data centers, redefining how facilities can behave during transmission faults to support—rather than destabilize—the grid.

How UPS can help data centers become grid‑friendly
Traditional UPS systems instantly transfer data center load to the battery during any grid disturbance, and they do not transfer back until the grid is stable for a defined period. While this protects IT equipment, it also creates sudden, large demand drops that pose risks for grid operators—especially in regions with a high data center concentration.
Introducing a grid friendly UPS: Engineered for FRT compliance
- At Schneider Electric, we recognize the growing impact of data centers on grid stability and are actively addressing it. The Galaxy V Series UPS is engineered to meet these evolving requirements through: Robust hardware that maintains connection during specific grid events.
- Advanced firmware algorithms enabling controlled, standards‑aligned behavior to support FRT requirements from different TSOs worldwide.
As shown in the figure below, this architecture allows data centers to safeguard their mission‑critical loads while supporting broader grid stability.


The smart real-time monitoring and advanced algorithms of Schneider Electric UPSs enable both data center uptime and grid stability simultaneously. With the Galaxy V Series UPSs, data centers can avoid sudden, large power demand changes from the grid and become a friend to the grid’s reliability and resilience.
Shifting to grid responsive data centers
As data centers continue to scale to meet the demands of AI and digital infrastructure, their influence on grid stability will only intensify. The industry can no longer view power quality issues as isolated events; they are now interconnected challenges that affect entire regions and national grids. Proactive collaboration between data center operators, utilities, regulators, and technology providers is essential to ensure resilience at both the facility and grid levels.
Solutions like Schneider Electric’s Galaxy V Series UPSs demonstrate how advanced power technologies can help data centers meet emerging Fault‑Ride‑Through requirements and operate as responsible, grid‑supportive citizens. By adopting smarter, grid‑aware power architectures, the industry can continue its rapid growth while safeguarding the reliability and resiliency of the electric systems we all depend on.
Add a comment