As data center operators race to build and expand facilities, they are encountering shortages of the specialized skills needed to design, build, and operate AI-factory environments. From construction crews to cybersecurity experts to AI engineers to HVAC techs, to diesel mechanics and electricians, the workforce simply isn’t keeping pace with the speed of construction and innovation. The result is a growing concern that talent, rather than shortage of power or semiconductors, may become the primary barrier to scaling artificial intelligence.
With power density of AI factories roughly doubling every year, many companies do not have the extremely talented engineers to keep up. Advanced design and simulation software can help make digital twins of the power system, cooling systems and the entire data center. Also, prefabricated modules are available for the IT room, cooling, and power systems. Once the necessary site preparation is complete, they function as plug-and-play solutions. Built and tested in factories, they can reduce design time and costs while accelerating data center deployment.

Construction labor pains
Current skill shortages affect almost every aspect of data center operations, starting with power distribution, cooling, and building construction. As data center operators and hyperscalers rush to add capacity, they are finding that construction companies also face staffing challenges, in addition to slow permitting processes and access to power. Call it a perfect storm.
According to McKinsey, there aren’t enough trained professionals for the electrical and mechanical installation work required in data center construction projects.
The U.S. construction industry is currently short roughly 439,000 skilled workers, and more than half of data center construction sites report disruptions due to staffing shortages, contributing to extended project backlogs—a dynamic that especially affects rural builds and drives large contractors to partner with smaller regional companies to secure needed labor.
Operational staffing challenges
Once a data center is built or expanded, skill shortages don’t go away. All types of talent are needed to update, maintain, and operate equipment. But candidates for just about every role, from heating and cooling specialists to electrical engineers to project managers, are in short supply.
Many IT positions are difficult to fill. Cybersecurity talent shortages, for instance, are a chronic issue. And AI is so new that not enough skills have been developed to fill positions. According to Uptime Institute, 51% of data center operators struggled to find qualified candidates in 2024. The biggest gaps were in junior and mid-level operations roles, followed by shortages in operations management, mechanical, and electrical positions. In addition, retention will remain a challenge, with pending retirements and data center talent leaving for other opportunities. New research from DataX Connect forecasts that 40% of data center professionals plan to leave their roles despite rising salaries, potentially widening the talent gap. Why? Working in the data center industry is extremely demanding, with long hours and high-pressure projects, so professionals are looking for more than just a salary; they want benefits, flexibility with work-life balance, and visible investment in their career development.
Filling the data center talent gaps
It’s true that no single solution exists to address data center staffing gaps. But operators can take steps to alleviate the situation:
- Train existing staff – Organizations often overlook existing talent, focusing on outside recruitment to fill positions. Assess your departments to identify promising talent who can be trained in AI and other areas with shortages.
- Focus on retention- Offer continuous training, clear career paths, supportive leadership, and a strong workplace culture that reduces burnout and keeps employees engaged.
- Outsource tasks – In some cases, data center operators can outsource simpler, routine tasks, allowing in-house staff to focus on more critical functions.
- Automation – Leverage AI and robotics to automate tasks, which will help fill staffing gaps. Still, it raises a chicken-and-egg issue: You need AI talent to fill jobs created by AI before that talent is available.
- Work with academia – Forge relationships with universities, colleges, technical institutes, and high schools to groom the next batch of data center workers. Offer internships and apprenticeships to give promising young professionals a career start.
- Partner with a Vendor– Lastly, operators don’t have to tackle the AI talent gap and its related challenges alone. Schneider Electric offers a broad portfolio of data center solutions designed to support AI deployments from design through operations. These solutions help bridge skills gaps, streamline implementation, and optimize AI infrastructure.
Addressing the AI talent gap
As AI increases demand and strains data centers to the limit, the talent shortage is proving to be a significant challenge. We may eventually see highly autonomous facilities, but we’re not there yet—and human expertise is still critical to operations.
In the meantime, taking practical steps—such as upskilling and retaining existing staff, outsourcing routine tasks, leveraging automation, and building partnerships with schools and technology vendors—can make a measurable impact. By addressing the talent gap today, operators can stay ahead of accelerating AI-driven growth rather than constantly reacting to it.
Lastly, discover how Schneider Electric’s EcoStruxure™ Pod Data Center solutions can adapt to your facility’s specific requirements and simplify deployment, helping your team scale faster with less strain on internal resources.
Add a comment