Cyber Security

Stay Connected to Your Assets, Even When You’re Not There

Data is (or should be) at the core of nearly every business decision you make. It is necessary for the smooth, efficient and profitable operation of machinery, control systems and more.

However, problems may occur when your workforce can’t access the physical site where data is being created. This holds true for situations such as:

  • Operations are located far away from major land marks
  • Business is looking to restrict the number of personnel in one place at a time, or
  • Workforce are working remotely from home
Digitization can help ensure fast, safe and secure remote access of data.

Digitization is the Answer

Digitization can help ensure fast, safe and secure remote access of data. By digitizing your machine systems, your business can continue running (and even thrive) at times when others may be slowing down.

Schneider Electric’s EcoStruxure Secure Connect Advisor, a cyber secure solution, allows operators and experts to remotely access, program, diagnose and troubleshoot automation equipment as if they were onsite. This allows you to maintain full control over your assets by monitoring who can access your system and specifying what they can access and when. Your intellectual property is protected, and your business can run securely.

Contact Us Today

With data underpinning so many of the applications and predictive analytics necessary for your business, being able to access it, and also protect it from others, is of vital importance.

For more information on how an EcoStruxure solution and remote connection could help your business, please contact your local Schneider Electric representative.


No Responses

Leave a Reply

  • (will not be published)