4 ways to reframe building security from cost center to enterprise value driver

security

In 2024, the global surveillance camera market was valued at an estimated $43.6 billion and is projected to nearly double by 2030, driven by rising demand for advanced safety measures across global industries. But many organizations still treat security as a commoditized line item—“just cameras and card readers”—rather than a strategic operational asset.

That gap between investment reality and strategic opportunity is a missed lever for enterprise performance.

At Knight Watch, we help organizations elevate security into a core business function, using data and intelligence to drive financial discipline and operational efficiency. The shift starts with changing the conversation from tech specs to financial outcomes. Here’s how.

Instead of focusing on megapixels, corporate boards and CFOs are now asking about cash flow, productivity, and uptime. However, today’s AI-enabled, cloud-connected, and analytics-driven security platforms can reduce risk while also creating measurable business outcomes.

So what’s the barrier then? It’s not about the technology; it’s about how the investment is communicated. Labeling a security program as a “compliance cost” primes a finance team to treat it as discretionary overhead. But when you speak in terms of ROI, payback periods, internal rates of return, and net present value, you’re operating in a language CFOs understand.

Consider a major sports and entertainment venue we supported. AI-driven video analytics and threat detection, along with risk mitigation, significantly sped up entry lines. That meant fans were inside the building sooner, increasing time spent in concessions and retail.  Safer, faster throughput became a tangible revenue uplift.

That’s the kind of messaging—financial logic—that gets executive attention and budget approval.

Security spending has historically been capital-intensive: hardware up-front, long payback cycles. Now, the paradigm is shifting. Security-as-a-Service and consumption-based models allow organizations to convert lumpy CapEx into predictable OpEx.

Finance teams value predictability and scalability. Monthly, usage-based models align spending with outcomes rather than big, upfront hardware purchases. In a tight fiscal environment, this is often the only way modernization gets approved.

In fact, we’ve even structured payment deferrals and multi-year terms with partners so that organizations can modernize today rather than wait for an elusive next budget cycle.

When building a business case, it’s important to separate tangible savings from strategic value, because both influence executive risk appetite.

On the tangible side, analytics help reduce theft, fraud, and vandalism. In manufacturing settings, they can measurably improve safety and uptime. As I tell operations leaders, “Downtime costs more than cameras ever will.” If a $50 million production line improves efficiency by just 0.5 %, that’s roughly a quarter million dollars of value in one year. Add to this the compounded losses from idle production lines.

But it’s the intangible value that often flips approvals. For example, a security leader at a major cultural institution told me that their biggest fear isn’t theft; it’s reputational damage from a public incident. A single high-profile failure could cost more in brand erosion and lost trust than all the security systems they’ve ever installed combined. That’s enterprise value: protecting brand, patron trust, and long-term viability.

Security investments can stall when procurement, security leaders, and finance aren’t aligned. We once delivered exactly what a client asked for—25 specification revisions—only to have the project canceled because no one asked, “What internal ROI hurdles must this clear?” This exposed the language barrier: security focuses on risk, while finance demands ROI, cost, and coverage metrics.

Now, we bring procurement and finance into the conversation from the start. We equip security leaders with concise, executive-friendly business cases, not technical spec sheets. A CFO cares about cash flow and enterprise risk, and operations cares about usability and scalability. When a proposal bridges those worlds, decisions get made.

Security used to be a back-office function. Today, it intersects with customer experience, operational efficiency, and brand protection. Advancements like AI analytics and cloud connectivity have expanded what security technology can do, but the real payoff comes when leaders shift the way they think about it.

Whether you’re protecting a campus, stadium, hospital, or factory, we can help you turn “must-spend maintenance” into strategic modernization.

Ready to stop treating security like a tax and start leveraging it like the asset it can be? Contact us and begin crafting financially sound security strategies that reduce risk, enhance operations, and generate measurable enterprise value.

Add a comment

All fields are required.