The business case for smart charging as EV adoption accelerates

Commercial buildings are taking on a more active role in managing electricity demand. For decades, buildings drew power as needed and left the grid to absorb the peaks. That model is ending. Building owners now need to manage energy demand as a core operating responsibility.

The growth of electric vehicles is pushing commercial buildings to evolve from passive energy consumers into active participants in energy management. As EV adoption climbs through the 2020s and into the 2030s, every new charger adds demand that often arrives in concentrated waves, from hotel check-ins to morning office arrivals. The scale is already evident in the most EV-advanced markets: our analysis finds that a large office building may require dozens of simultaneous charging points. That figure rises above 100 by 2035, with other markets close behind.

smart charging

Our recent report, “Toward net zero buildings: The investment case for smart EV integration,” modeled 65 use cases across 13 regions and five building archetypes: hospitals, offices, schools, hotels, and retail sites. The central finding is that smart charging can keep EV growth manageable at the building level. By 2035, uncontrolled EV charging can push peak import power at small hotels and strip malls to 200%-300% of the site grid limit in the most EV-dense markets. The site grid limit is the maximum power a building connection is designed or contracted to draw from the grid.

With smart charging, every modeled site stayed within its grid limit. Smart charging means coordinating when and how quickly EVs charge based on expected departure times, available site capacity, and electricity price signals. The research findings show why EV readiness now depends on load management, tariff design, and grid planning.

EV readiness depends on active load management, not only on added electrical capacity.

1. Peak control is a business responsibility

Peak demand has traditionally been managed through grid-side capacity additions that include more capacity, more infrastructure, and faster connections. Smart charging changes this equation by giving buildings direct control over one of their fastest-growing electrical loads. By intelligently managing EV charging demand, buildings can limit peak consumption, stay within grid constraints, and defer costly electrical upgrades. When a building manages its EV load, it controls its own peak and stays within its grid limit, rather than pushing avoidable demand upstream.

Peak control without infrastructure upgrades

As EV adoption rises, many commercial sites will see charging demand concentrate around predictable arrival windows, creating short peaks that can exceed the power available at the building connection. The modeling shows that smart charging can smooth those peaks by coordinating charge timing and speed around driver needs and site capacity. Across every site tested, this kept buildings within grid limits without transformer upgrades, feeder reinforcement or driver queues.

100% of 65 modeled sites stay within grid limits with smart charging alone

≈100% EV driver satisfaction maintained — vehicles depart with the required charge

→  Shifts EV charging from peak arrival windows to lower-cost, lower-demand periods
→  Works across hospitals, offices, schools, hotels, and retail sites
→  Can be applied from the first charger, without on-site generation or storage

Source: Minier & Utrilla Bustamante, SERI, April 2026   ·   Smart charging only — no on-site generation or storage 

Peak behavior is highly site-specific. A hotel with a dozen EV chargers has a different demand pattern than an office building with 100 or a hospital with early-morning shift changes. Smart charging adapts to each environment, scheduling charging around departures and staying within the site’s power limits. The building manages charging demand instead of adding avoidable strain.

2. Tariff design determines the business case

In markets that reward peak-demand management, smart charging can pay for itself quickly. Demand charges bill customers for their monthly maximum load. Subscribed power arrangements set a contracted power level and penalize buildings that exceed it. Across all five building archetypes modeled for France, payback is achieved in under twelve months. When smart charging eliminates the need for a transformer upgrade, the avoided capital spending alone can exceed the controller cost before operating savings are counted.

Bill savings that pay back within the year

In markets with demand charges or subscribed power, such as France, Spain, Canada, and the United States, smart charging reduces electricity bills by avoiding peak-demand periods.

<1 yr
Payback on smart charging investment across all five archetypes in France

0 yr
Effective payback for LV-fed buildings — reinforcement savings alone offset controller cost

→  Optimizes time-of-use, demand charge, and subscribed power costs
→  Savings grow as EV adoption rises because there is more charging load to schedule.
→  Returns are strongest where tariffs make peak demand expensive

Source: Minier & Utrilla Bustamante, SERI, April 2026   ·   Smart charging only — no on-site generation or storage  

This investment case can even improve over time. As more employees, guests, and visitors arrive with EVs, there is more charging load to schedule and more savings to capture. A smart charging system installed today can become more useful as EV demand grows, especially where tariffs make peak demand expensive.

3. Smart building reduce grid strain

At one site, smart charging helps a building manage its own peak. At scale, the same building-level control can lower the amount of network capacity Distribution System Operators (DSOs) need to add to serve concentrated EV charging demand. DSOs are the organizations responsible for local electricity distribution networks.

Avoiding transformer upgrades and associated costs

The hidden cost of uncontrolled charging is the infrastructure it can require. Smart charging can avoid transformer and switchboard upgrades that direct charging may require.

>€100k Avoided capital spending for a large office at 2035 EV penetration

Zero No DSO investment in the smart charging system because grid relief comes from private building-side investment

→  At 2035 EV density, smart charging can help a large office avoid a second 2,000 kVA transformer
→  Based on NF C 15-100 installation standards and Enedis connection rules
→  Aggregated across many sites, lower building peaks can reduce network reinforcement needs

Brattle Group research estimates that demand-side management could save US utility customers $110 billion to $170 billion over the next decade. Our analysis points in the same direction: when many sites manage charging peaks locally, they can help avoid system costs that would otherwise fall to DSOs and ratepayers.

The policy implication is straightforward: tariffs with demand charges or subscribed power penalties make smart charging more financially attractive. Where that signal exists, buildings can provide grid relief through privately funded demand management. Without that signal, adoption can slow.

How smart charging helps buildings scale EV adoption

Smart charging gives building owners a practical way to prepare for EV growth without shifting avoidable peaks onto the grid. By coordinating charging around site capacity, driver needs, and tariff signals, commercial buildings can stay within grid limits, reduce operating costs, and help defer infrastructure investment as adoption rises. To explore the full modeling across building types, regions, and EV adoption scenarios, access the Schneider Electric Research Institute report, “Toward net zero buildings: The investment case for smart EV integration.”

Key Takeaways
  • Smart charging is a building investment that can also reduce grid strain.
  • For early adopters, the primary case is operational and financial: lower peak demand, lower operating costs, and readiness for rising EV charging load.
  • Grid benefits can follow at scale.

Add a comment

All fields are required.