The unsung hero of rooftop unit economizers: Why the damper actuator matters

Commercial HVAC Rooftop Units (RTUs) equipped with economizers are one of the most effective energy-saving strategies. By using outdoor air for cooling when conditions are favorable, economizers can reduce compressor runtime and overall energy consumption.

Because of these energy-saving benefits, energy codes and standards such as ASHRAE Standard 90.1 often require airside economizers for commercial RTU applications, depending on the building climate zone, cooling capacity, and system type.

While many discussions about economizers focus on sensors, control logic, or energy code compliance, one component ultimately determines whether the strategy works in practice: the damper actuator.

This actuator physically positions the outdoor-air and return-air dampers, making it the final control element in the economizer sequence.

The  damper actuator impacts RTU economizer efficiency, outdoor air control, energy savings, and HVAC code compliance.

Economizer strategies: The basics

Economizers operate by comparing outdoor air conditions with indoor return air conditions to determine whether outdoor air can provide free cooling.

  • Dry-bulb control compares outdoor air temperature with return air temperature. If outdoor air is cooler, the economizer increases outdoor airflow to provide cooling.
  • Enthalpy control evaluates the total heat content of the air, including temperature and humidity, preventing the introduction of cool but overly humid outdoor air.
  • Differential enthalpy control measures both the outdoor and return-air enthalpies and selects the air source with the lower energy requirement.

Regardless of the strategy, the sequence ultimately depends on one mechanical action: the dampers must move to the correct position, and that movement is controlled by the damper actuator.

The damper actuator: The real driver of economizer performance

In any HVAC control system, the controller sends a command signal—but the actuator performs the work.

For economizer applications, the actuator must:

  • Modulate the outdoor air damper
  • Coordinate with the return air damper
  • Maintain minimum ventilation positions
  • Respond accurately to control signals from the RTU controller or building automation system.

If the actuator performs poorly, the economizer strategy becomes ineffective, leading to increased compressor runtime, improper ventilation, excess outdoor air during humid conditions, and reduced occupant comfort.

Why actuator reliability is critical in economizer applications

Economizer dampers are among the most active moving components in an RTU. Unlike safety dampers or isolation dampers that move occasionally, economizer dampers may modulate continuously throughout the day.

Because of this high duty cycle, the actuator must provide accurate positioning, consistent torque delivery, long mechanical life, and stable response to control signals.

An actuator that suffers from drift, inaccurate positioning, or premature mechanical wear can compromise the entire economizer sequence.

The impact of proper installation

While actuator quality is critical, installation practices play an equally important role in system performance.

Proper actuator mounting, correct linkage alignment, minimal damper friction, accurate minimum-position calibration, and reliable wiring are all essential for proper operation.

Because the actuator physically translates control signals into changes in airflow, installation quality directly affects economizer performance.

Economizers, energy codes, and real-world performance

ASHRAE 90.1 recognizes the significant energy savings that economizers can provide. However, simply installing an economizer does not guarantee those savings.

To achieve the intended performance benefits, a successful system requires accurate sensors, proper control logic, well-designed dampers, reliable actuators, and correct installation and commissioning.

Among these elements, the actuator plays the most important role because it ultimately controls the airflow entering the building.

Economizers are only as good as their actuator

Economizers are among the most effective energy-saving strategies available for rooftop HVAC systems. Yet the success of an economizer sequence ultimately depends on the damper actuator’s performance.

Selecting reliable actuators, following proper installation practices, and ensuring accurate commissioning are essential steps to help ensure economizer systems deliver the energy savings and comfort improvements they are designed to achieve. Learn more about our damp actuator solutions.   

Add a comment

All fields are required.