Cable entries define how cables interact with the enclosure and play a key role in protection, installation efficiency, and future adaptability. Choosing the right cable entry depends on the conditions in which it will be used.
Considerations when selecting cable entries
Installation environment
The installation environment defines the required level of protection in the cable entry area. Exposure to dust, moisture, or outdoor conditions increases the need for effective sealing to preserve the enclosure’s IP rating, while controlled indoor installations typically prioritize basic mechanical guidance.
Beyond environmental exposure, cable entries must address two distinct risk factors. In accessible installations, cables may be subject to handling or access by unauthorized parties, requiring sufficient mechanical retention to prevent movement or damage. Separately, outdoor applications introduce additional biological risks such as rodents or insects, which can compromise cables and enclosure integrity if entries are not properly sealed.
In exposed context, solutions such as snap-in entries or hard-plastic entry plates combined with cable glands are typically selected whereas simpler membrane-based entries or cable entry plates may be sufficient in low-stress environments.

Project efficiency and installation flexibility
Cable entries also affect how efficiently a project can be installed and maintained. If the system is expected to evolve, cable entries that allow cables to be added or changed without removing existing wiring offer clear advantages. Flexible solutions support future upgrades while reducing modification work
This same flexibility also impacts installation time. Cable entries that are easy to assemble and tolerant of small variations in cable diameter simplify wiring work and reduce the need for precise pre‑planning. In repetitive or large‑scale projects, these characteristics can significantly shorten installation time and improve consistency across cabinets.
Multicable entry systems support future upgrades, reduce modification work, and avoid unnecessary disassembly.

Characteristics of the installation
The characteristics of the cabling system ultimately guide the selection of the cable entry solution. Simple cable entries are well suited to clearly defined layouts with a limited number of cables. In contrast, installations involving multiple cables typically benefit from solutions that allow several cables to pass through a single-entry point.
When cables are fitted with large or pre‑assembled connectors, the cable entry must enable installation without the need to remove those connectors. Furthermore, variations in cable diameter may call for adaptable entry solutions rather than fixed‑size openings.
Finally, ensuring compatibility between the enclosure material and the cable entry material is essential to guarantee long‑term mechanical stability and reliable performance.

Cable entry selection is a balance between protection, flexibility, installation effort, and cabling constraints. By focusing on a few essential criteria, it is possible to choose a cable entry solution that supports both current installation needs and future modifications, while avoiding unnecessary complexity or rework.
Treating cable entries as a functional part of the enclosure design leads to cleaner installations, improved reliability, and more adaptable systems.
Discover all the accessories for Universal Enclosures in our new catalogue.
Add a comment