Creating healthy classroom environments: A strategic priority for today’s school boards

School districts are being asked to do more than ever when it comes to classroom health, often in buildings that were never designed for today’s expectations.

According to the National Center for Education Statistics (NCES), the average U.S. school building is nearly 50 years old, and more than one‑third were built before 1970. That means many schools were constructed long before indoor air quality, energy efficiency, and modern ventilation standards became a focus. With limited upgrades over the years, districts are now managing aging HVAC systems, uneven comfort, and increasing pressure to meet new health guidelines.

So, the question becomes: How can schools create healthier classrooms when their buildings weren’t built for today’s needs?

As buildings age, maintaining comfortable and healthy classrooms becomes harder, especially when trying to deliver the same experience across every school. And this is not just about comfort.

The U.S. Environmental Protection Agency (EPA) has shown that temperature control, ventilation, and indoor air quality affect student focus, behavior, and learning outcomes. When classroom conditions are inconsistent, it can impact both students and teachers.

While modernization is clearly needed, large-scale HVAC replacements or construction projects often entail high costs, lengthy timelines, and classroom disruption. For many districts dealing with tight budgets and packed school calendars, full system overhauls simply are not realistic.

The good news is that meaningful improvements do not always require major construction.

When people hear “modernization,” they often assume it means replacing entire systems. In reality, meaningful improvements can start at the room level with solutions that are easier to install, scalable across a district, and budget-friendly.

One example is the SpaceLogic™ Touchscreen Room Controller, an all-in-one, room level solution with built-in sensors for temperature, humidity, CO2, and occupancy. By combining multiple functions into a single device, it installs quickly, simplifies upgrades, and helps schools improve comfort, indoor air quality, and energy performance, even in older buildings.

Unlike traditional thermostats, the Touchscreen Room Controller uses embedded AI directly in the classroom, rather than relying on cloud processing. This allows it to continuously fine-tune classroom conditions in real time, exactly where students and teachers experience them.

Because the intelligence is built into the device, schools benefit from faster, more precise adjustments without requiring internet connectivity. It also reduces system complexity, limits cybersecurity exposure, and eliminates ongoing subscription fees. The controller can operate as a standalone solution or integrate seamlessly into existing building systems.

It is also the first room controller to automatically maintain ASHRAE 55‑compliant comfort using fully embedded AI, helping classrooms stay comfortable throughout the day without constant manual adjustment.

For facility teams, the controller provides clear, real-time, room-level insight into temperature, occupancy, ventilation, indoor air quality, CO₂ levels, and equipment alerts. Instant CO₂ notifications and early issue detection make it easier to address problems before they become comfort complaints, while supporting compliance and proactive maintenance across all schools.

Teachers notice the difference immediately. A clean, intuitive touchscreen replaces confusing thermostats, reducing distractions and allowing teachers to focus on what matters most: teaching.

The controller integrates easily with EcoStruxure™ Building Operation, the Tridium Niagara platform, and other systems using open standards such as BACnet or Modbus.  This compatibility with both modern and legacy infrastructure helps districts deliver consistent comfort and performance district-wide.

Watch the video to see how the SpaceLogic Touchscreen Room Controller helps schools improve classroom health and efficiency without the cost and disruption of major renovations.

About the author

Melanie Parnass-Katz, Product Marketing Manager

Melanie is a Product Marketing Manager at Schneider Electric, where she is focused on smart building solutions. She works on shaping clear value propositions and go‑to‑market strategies that help customers understand new technologies and adopt them with confidence. Her experience spans building controls, hardware launches, and global marketing initiatives, with a focus on helping customers modernize building systems in a simple, reliable, and scalable way. 

Add a comment

All fields are required.