6 signs your building isn’t as smart as you think (and what to do about it)

smart building

Recently, I worked with a facilities director responsible for a large campus who had nearly a dozen separate logins just to do their job. One was on a Windows XP machine tucked in a closet because the system couldn’t be upgraded. Another handled HVAC in a single building, while yet another handled lighting in a different building. A stand-alone system managed cameras in the parking garage, with zero connection to the main entrance access control system.

This scenario is more common than many realize. Large facilities have an average of 17 different technologies running building operations, often requiring large teams just to keep them running. After two decades in this business, I’ve seen the same pattern play out. For years, integration was the goal. If systems could talk and data could move, that was success. But moving data isn’t the same as understanding it, and coordination isn’t the same as intelligence. A truly “smart” building connects and aligns systems, using data to support better decisions across operations.

At Knight Watch, we see this shift every day. We also know this process can feel overwhelming. Here are six signs your building isn’t as smart as you think, and where you can start moving towards true building intelligence.

Most facilities have already invested in integration. Systems can exchange data, trigger actions, and follow rules. However, they still depend on someone telling them what to look for. This is more choreography than intelligence.

The result is system sprawl. Multiple logins, dashboards, and versions of the truth, which really adds up. In fact, buildings account for nearly 30% of global energy consumption, driven significantly by operational inefficiencies between systems. So, what can be done?

Where to start: Pick one recurring manual report you run each week. Can it generate automatically using data from across your building, even if those systems weren’t designed to work together? If not, there’s your starting point.

If each of your systems work independently but not together, this is where you find yourself. This can look like:

  • Heat running when spaces are empty.
  • Lights staying on when rooms are unoccupied.
  • Access systems operating independently from occupancy.
  • Energy systems not reflecting real usage.

However, small changes can really add up. For example, recently, I was in an airport lounge, carrying a bag in one hand and a coffee in the other. The door to the next section had a hand-wave sensor—you waved, it opened. Compare that to a grocery store door that opens every time someone walks past it. In a busy airport, a hundred people may walk by that door, but only two need to go through. That wave sensor allows the door to open twice rather than 100 times. The outcome? Less wear on the motor, less maintenance, and less energy used. One $200 sensor can save thousands over the life of the door.

Where to start: Look for places where systems are working at cross-purposes. Where is one system undoing the work of another? That’s where coordination will pay off fastest.

Once systems can interpret data, they stop waiting for instructions and start identifying patterns, and thus, anomalies, such as:

  • Unexpected activity at 3 a.m.
  • Doors being used differently than expected
  • Equipment behaving outside normal ranges
  • Energy usage that doesn’t align with operations

These signals allow teams to act earlier, with more context and purpose.

Where to start: Check your systems for any recent anomalies. If they can’t tell you, they’re not thinking, they’re just recording.

We once had a customer who scaled back part of a security deployment to save roughly $10,000. While that felt like a large savings at the time, within months, they experienced losses approaching $750,000 due to the blind spot it created.

The same principle applies across operations. Facilities teams juggle many systems daily, many buildings are running full HVAC despite partial occupancy, and equipment is degrading faster due to unnoticed power-quality issues. Fortunately, these are common, solvable challenges.

Where to start: Look for the places where you’ve accepted a gap because filling it seemed too expensive. Run the math on what that gap has cost over the last year, and compare the two numbers honestly.

Imagine if in your building, schedules could adjust to actual usage, access could adapt to roles and behavior, and energy could align with demand. The building could respond rather than wait. But, this doesn’t happen by installing another system. It starts by asking:

  • Where are we operating blind?
  • Where are systems working in isolation?
  • Where are people compensating for technology gaps?

Where to start: Every time someone manually overrides a schedule, adjusts a thermostat, or unlocks a door by hand, write it down. At the end of the week, ask: which of these could a smarter system have handled automatically?

Smarter buildings come from changing how systems work together and what you expect of them, not from ripping out what’s already working. Once a building can interpret what’s happening within it, the organization’s role changes. You’re no longer reacting to problems; you’re deciding how far you’re willing to let the building think for you.

Where to start: This one isn’t for your facility teams, it’s for you.

Set a new expectation: from now on, every new system should be designed to share clean, structured, and accessible data with the rest of your environment. Custom integrations aren’t the problem; they’re often where the real value is unlocked. But they should build on a strong data foundation, not compensate for the lack of one.

That single shift changes everything. When your systems are built with interoperability and data quality in mind, AI can do its job; connecting insights, automating decisions, and creating outcomes your competitors can’t replicate.

Whether you’re running a college campus or a corporate headquarters, ask yourself:

“If you could stop telling your building what to do and start asking it what it sees, what would you change?”

Are you ready to see how well your facilities can think? Contact us, and we’ll help you ask better questions so your systems can start answering them.

Add a comment

All fields are required.