The convenience store scene across Asia-Pacific, especially in Southeast Asia, is undergoing incredible expansion. According to the report “Convenience Stores Market Report 2025” by Research and Markets, the sector’s global worth is expected to reach $1.26 trillion by 2025 and $1.75 trillion by 2029.
According to NielsenIQ, the Asia-Pacific region hosts over 26 million offline retail outlets, such as Alfamart and Indomaret, which are rapidly expanding and targeting smaller cities and rural communities. This growth opens up new opportunities for consulting engineers to create cost-effective, reliable electrical systems that keep pace with the demands of this thriving, fast-evolving market.
Designing for the tropics: Overcoming heat and humidity challenges
In Southeast Asia, mini markets are an essential part of daily life—compact, convenient, and often operating in challenging conditions. With humidity levels frequently exceeding 85% and temperatures above 30°C, these stores require electrical systems that can withstand heat, moisture, and continuous operation. For consulting engineers, designing efficient, durable, and cost-effective solutions for such environments is key to supporting business continuity and growth.
Reliable power solutions for mini markets: Simplifying electrical design against outages and voltage fluctuations
Reports from the International Energy Agency confirm that Southeast Asia faces growing risks of voltage fluctuations and unplanned outages, driven by extreme weather and rapid demand growth outplacing grid upgrades.
Picture this: the payment terminal, cash register, and Wi-Fi router are all humming along, then the refrigeration unit kicks in, demanding a huge spike in power. Suddenly, you’ve got a voltage surge wreaking havoc across the board. For store owners, this can mean losing sales, spoiled inventory, and frustrated customers walking out the door. That’s why having surge protection devices (SPD) and reliable power solutions baked into every design isn’t just a nice-to-have—it’s essential. Refrigeration systems add their own quirks to the mix. When they start up, they draw a lot more power than usual, causing lights to flicker, cash registers to reboot, and alarm systems to glitch. If the cooling fails, you’re looking at ruined stock, cloudy freezer glass, and inventory losses. Solving these problems means working smarter: include dedicated circuits, surge-resistant protective devices, and—if the budget allows—a basic soft-start mechanism or contactor to keep things running smoothly. Space is always at a premium in stores sized between 30 and 60 m², where every inch has to pull its weight. There’s hardly room for oversized electrical cabinets, large power backups, or elaborate monitoring setups. The real puzzle for electrical designers is making sure everything fits neatly, stays accessible for quick fixes, and doesn’t interrupt day-to-day operations. The smart play here? Compact and modular solutions. Pre-built distribution boards, well-planned kits, and clever placement of service points—like a unit near the checkout for easy access and another tucked away in the storage area—can simplify installations and maintenance while keeping things running smoothly.

Schneider Electric’s ready-made references – A competitive edge for design firms
At the heart of these decisions is a single overriding factor: cost. For mini market owners, flashy engineering isn’t the focus—they want solutions that are practical, reliable, and don’t burn through their budget. That’s why electrical systems need to be affordable, straightforward to maintain, and durable enough to handle everyday challenges. These essentials help speed up project delivery, ensure consistent outcomes, and create scalable designs—key advantages for clients managing or planning a chain of stores. Schneider Electric makes this process easier by offering ready-to-use electrical design templates and customized solutions tailored specifically for small retail spaces. Consulting engineers can skip the grind of building everything from scratch and instead tweak a pre-existing mini market electrical design to suit the customer needs.
That’s precisely what Schneider Electric’s Easy Reference Design for mini markets is designed to deliver. These ready-to-use electrical designs come as both CAD and PDF files, so you can start from a validated template rather than from scratch. This not only saves valuable time for consulting engineers, but also simplifies the entire electrical design process—making it easier for any engineer, regardless of experience level, to deliver accurate and efficient designs. This is particularly relevant as skill shortages continue to challenge the industry: according to the Upskilling and Reskilling in the Engineering Industry Statistics report by WiFTalents (Germany), 72% of engineering firms in 2025 reported losing projects or clients due to a lack of qualified talent.
Because the Easy Reference Designs are clear, straightforward, and ready to apply, they help bridge gaps in experience or expertise across teams—reducing risk, avoiding delays, and simplifying installation.
Each reference is:
- Tested, validated, and documented
- Aligned with current standards
- Built with cost-effective Schneider Electric offers that match small retail needs
By relying on Easy Reference Designs, you can accelerate your project timelines, maintain high quality across electrical designs, and stay competitive—even when resources are stretched thin.
What you get with the Easy Reference Design for mini markets
✅ An electrical reference design specifically for the needs of budget hotel projects
✅ End to end electrical and digital solution with SLD in CAD format
✅ Software native file for easy modification
👉 Access the Easy Reference Design for consulting engineers here

Optimize your projects with EcoStruxure power design – EcoDial
To support design professionals working on budget hotel projects, Schneider Electric offers EcoStruxure Power Design – EcoDial, a free software that simplifies electrical system design. With EcoDial, you can easily customize and adapt the budget hotels design references to suit your specific project needs, while benefiting from its robust calculation engine and intuitive interface. Whether you’re refining load schedules or validating protection settings, EcoDial helps you work faster and with greater confidence, making it accessible to any design team looking to boost efficiency and accuracy.
Add a comment