Social housing development is accelerating across Southeast Asia. In Vietnam alone, 132,616 social housing units are currently under construction, as part of the local Ministry of Construction’s broader plan to deliver one million affordable homes by 2030. Yet behind this rapid growth lies a practical challenge: how to design electrical systems that are safe, reliable, and easy to replicate—without driving up costs.
In dense tropical environments, where heat and humidity put constant stress on equipment, consulting engineers must focus on simple, robust, and scalable solutions. From affordable wiring layouts to modular components that streamline installation, the goal is clear: design electrical systems that perform consistently and can be deployed efficiently across hundreds of projects.
Overloaded circuits, heat, and humidity—everyday challenges in small apartments
Imagine a family living in a two-room apartment. A single electrical circuit powers a fan, a TV, a phone charger, and a small fridge. One kettle turned on—and the lights go out. Overloaded circuits are common. Thin wires, cheap extension cords, and poor protection make every socket a potential hazard.
In countries where indoor temperatures reach 35°C and humidity exceeds 80%, electrical cables suffer. In social housing buildings, often without air conditioning, wires run under thin plaster or inside metal conduits—which act like ovens. And the sun doesn’t just heat—it destroys. Installations on rooftops, corridors, and balconies often overheat. Add moisture to the mix: a bathroom without a window, steam after a shower, and a socket right next to it—with no cover. This scenario repeats thousands of times. And the pressure is only growing: Vietnam’s electricity-related emissions from residential and commercial buildings are expected to rise from 114.2 MtCO₂e in 2025 to over 400 MtCO₂e by 2050, according to the UNESCAP and Vietnam’s National Energy Master Plan.
Creative fixes and everyday solutions
In many social housing developments, maintenance and small repairs are handled with limited technical resources. This reality makes it crucial to design electrical systems that are safe, intuitive, and affordable—allowing quick fixes or component replacements without specialized tools or training.
Designing easy, not expensive—tailored electrical design for social housing
This isn’t about flashy technology—it’s about practical, reliable solutions that fit tight budgets. Electrical systems must be affordable to install, easy to maintain, and resilient to everyday challenges—from moisture to overloads. Faced with these recurring issues, consulting engineers are rethinking how electrical systems can be built to withstand the region’s realities—starting with simplicity and accessibility.
That’s exactly what Schneider Electric’s Easy Reference Design for social housing is built for. These ready-to-use electrical designs come as both CAD and PDF files, so you can start from a validated template rather than from scratch. This not only saves valuable time for consulting engineers, but also simplifies the entire electrical design process—making it easier for any engineer, regardless of experience level, to deliver accurate and efficient designs. This is particularly relevant as skill shortages continue to challenge the industry: according to the Upskilling and Reskilling in the Engineering Industry Statistics report by WiFTalents (Germany), 72% of engineering firms in 2025 reported losing projects or clients due to a lack of qualified talent.
Because the Easy Reference Designs are clear, straightforward, and ready to apply, they help bridge gaps in experience or expertise across teams—reducing risk, avoiding delays, and simplifying installation.
Each reference is:
- Tested, validated, and documented
- Aligned with current standards
- Built with cost-effective Schneider Electric offers that match social housing needs
By relying on Easy Reference Design, you can accelerate your project timelines, maintain high quality across electrical designs, and stay competitive—even when resources are stretched thin.

What you get with the Easy Reference Design for social housing
✅ An electrical reference design specifically for the needs of budget hotel projects
✅ End to end electrical and digital solution with SLD in CAD format
✅ Software native file for easy modification
👉 Access the Easy Reference Design for consulting engineers here

Optimize your projects with EcoStruxure Power Design – EcoDial
To support design professionals working on social housing projects, Schneider Electric offers EcoStruxure Power Design – EcoDial, a free software that simplifies electrical system design. With EcoDial, you can easily customize and adapt the budget hotels design references to suit your specific project needs, while benefiting from its robust calculation engine and intuitive interface. Whether you’re refining load schedules or validating protection settings, EcoDial helps you work faster and with greater confidence, making it accessible to any design team looking to boost efficiency and accuracy.
Add a comment