Zakaria Belhaja

Zakaria Belhaja

  • Connect with me
  • RSS
Zakaria Belhaja holds an engineering diploma from INSA Lyon (Institut National des Sciences Appliquées),and a Specialized Master in Innovation and Technology Management from GEM (Grenoble Ecole de Management), France. After 9 years in Research and Development in the arc fault detection domain, including architecture, algorithm development, testing and standardization, he is now AFDD offer manager, and is focused on developing IEC-compliant arc fault detection solutions.

The 5 critical faults that cause electrical fires

8.3K views 2 0 366

Countries pay huge costs in life and money for electrical fires

4.3K views 2 2 268

Preventing Arc Faults and Fires in Buildings Using New AFDD Technology

9.2K views 107 5 1.0K

Arc Faults: The Hidden Fire Risk Revealed

13.9K views 148 0 1.5K