Wendy Torell

Wendy Torell

Wendy Torell is a Senior Research Analyst at Schneider Electric’s Data Center Science Center. In this role, she researches best practices in data center design and operation, publishes white papers & articles, and develops TradeOff Tools to help clients optimize the availability, efficiency, and cost of their data center environments. She also consults with clients on availability science approaches and design practices to help them meet their data center performance objectives. She received her Bachelors of Mechanical Engineering degree from Union College in Schenectady, NY and her MBA from University of Rhode Island. Wendy is an ASQ Certified Reliability Engineer.
data center design

Back to the Basics: Data Center Capacity Planning Done Right

2.6K views 0 0 122
liquid cooling

It’s Not Just About Chip Density – Five Reasons to Consider Liquid Cooling for Your Data Center

5.4K views 2 0 285

OSDA – A More Flexible Data Center Availability Rating System

3.1K views 2 0 139
Smart city and communication network concept. IoT(Internet of Things). ICT(Information Communication Network).

48VDC and the Quest for Improved Compute Performance

3.7K views 1 0 165
two men discussion data center consolidation with their boss

How Your Data Center Consolidation Can Impress Your Boss: 5 Best Practices to Adopt

65.6K views 3 0 685
Li-ion calculator

Calculate and Compare the TCO of your Lithium-Ion vs. VRLA Batteries

8.0K views 3 0 596
data center cooling calculator

Air Economizers – Which Architecture is Best: Direct or Indirect?

7.1K views 0 0 330

12V vs. 48V: The Rack Power Architecture Efficiency Calculator Illustrates Energy Savings of OCP-style PSUs

9.1K views 4 7 390
woman and technology

How the Digital Economy is Shifting the Workforce Playing Field for Women

8.5K views 15 0 463
Data Center

How much power? What density? The IT Pod Sizing Calculator can help answer these data center questions.

8.3K views 21 0 955
data center

How data center pod frames can reduce IT room costs by 15%

5.5K views 0 0 675
Hyperpod data center

How data center pod frames can shorten IT room deployment time by over 20%

8.7K views 57 0 627