Vladislav Tverdochleb

Vladislav Tverdochleb

I am an enthusiastic leader for internal projects and initiatives in the company, hobbyist to learn new languages, culture and traditions add avid reader of technical publications. Since 2007 I have joined Schneider Electric Company in field of operational marketing and was in charge of low voltage strategic products launches. I have developed and implemented the Panel Builders policy in the region, principles and program of “Electricians Business School” for education centers. The key priority I keep in front of me is to engage colleagues, to be passionate story tellers about the company, products and solutions.

Best Electrician – Tell a story to grow your business

10.2K views 377 5 1.7K

Best Electrician – The extra something is a solution not a device

8.7K views 412 1 1.4K

Best Electrician – Learning more, earning more

15.2K views 265 46 3.0K

Best Electrician – Goes Beyond Customer Expectations

10.8K views 170 5 1.6K

IEC 60898-1 and IEC 60947-2: a tale of two standards

218K views 359 78 9.1K

Cascading and backup: Why coordination should be compulsory

14.0K views 60 0 2.8K

Selectivity: Positive discrimination for maximum safety

13.1K views 72 0 3.2K

Setting the standard for coordination

11.2K views 56 0 1.9K

IEC 60947-2 the “all-risk” insurance for circuit breakers – Part 3

22.1K views 119 0 2.1K

IEC 60947-2 the “all-risk” insurance for circuit breakers – Part 2

49.3K views 186 8 4.4K

IEC 60947-2 the “all-risk” insurance for circuit breakers – Part 1

67.9K views 266 7 5.9K