Thomas Patzner

Thomas Patzner

  • Connect with me
  • RSS
Thomas Patzner has over 20 years experience in the electrical industry including a start as an apprentice electrician in the late 1980’s. He is an electrical engineering graduate of Marquette University, class of 1992, and has been involved with the development and engineering of Square D branded Low Voltage Transformers since 1990. Department of Energy negotiation process committee for final rule, manufacture voting representative, 2011.

Get Ready for New Distribution Transformer Efficiency Rules

10.5K views 688 0 2.8K