Tom Fowler

Tom Fowler

  • Connect with me
  • RSS
Tom Fowler is a graduate of Rowan University in Glassboro, New Jersey. He is a 39 year employee of Schneider Electric working mostly in motor control product management. Tom is a member of the NEMA Industrial Automation section, is past chairman of the Business committee and member of the contactors and starters technical committee.

Clearing Up the Confusion Between NEMA and IEC Contactors

31.3K views 20 2 4.0K

A Brief History of UL 508A and Tips for How Control Panel Builders Can More Easily Comply

14.0K views 2 7 2.5K

Goodbye UL 508: A Transition More Than a Decade in the Making

24.6K views 300 6 3.1K