Thierry Cormenier

Thierry Cormenier

Having graduated from the Conservatoire National des Arts et M├ętiers in 1992 with a degree in engineering in Automation, Thierry Cormenier joined Schneider Electric in 2010. Previously he was designer for IBM and ANSALDO. Then he has held several management positions in the engineering department of the Medium Voltage Equipment. In 2001 he became an IEC member linked to its function of R&D manager for HV/LV prefabricated substations up to 2014. Actually is working as standardization and connected product manager.

Medium Voltage Digital Transformation: Smarter, Safer, and Longer Lasting Equipment

4.8K views 7 1 207
medium voltage

How Medium Voltage Switchgear Innovations Help Fight Extreme Weather

8.2K views 3 0 390
medium voltage

How Extreme Weather Causes Premature Aging in Medium Voltage Equipment

8.6K views 14 0 436

Medium Voltage Design: Evolving Standards

17.8K views 335 0 783

Medium Voltage Design Basics: Environmental & Operation Conditions

21.1K views 536 0 793

Medium Voltage Design Basics: Switchgear Introduction

29.2K views 905 3 1.5K

An e-House Substation that Ushers in New Technology and Rethinks Standards

17.9K views 31 0 2.3K