Sherry Rollins

Sherry Rollins

  • Connect with me
  • RSS
Sherry Rollins is a Product Manager with more than 10 years of expertise in design and manufacturing of MV Switchgear, PLCs, HMI, Panel-boards and other accessories for PSD equipment. Sherry holds a Master of Science in Electrical Engineering from the University of Tennessee at Knoxville.

IEC vs ANSI Switchgear – Understanding the Global Standards

16.3K views 17 0 992

Metal-clad Switchgear: The Industry’s Medium Voltage Workhorse

14.2K views 15 0 1.4K
Electrical worker in PPE

Fixed Vacuum Breakers: An Alternative to Withdrawable Breakers

9.6K views 12 2 1.8K