Steve Nibbelink

Steve Nibbelink

Steve Nibbelink is the Global Healthcare Security Program Director at Schneider Electric and is dedicated to helping healthcare facilities provide a welcoming, safe, and secure environment for patients, visitors, and staff. He is deeply involved in the security community and currently serves on the Board of Directors of the IHSSF and is a member of IAHSS, ASHE, ASIS, IACLEA and HBCU-LEEA. Steve is certified both as a Healthcare Protection Administrator and a trainer in the Management of Aggressive Behavior program. In addition, he has won 6 awards for his service and dedication to the security industry, including the 2011 IAHSS President’s Award. When he’s not helping to provide total hospital security, you can find Steve bicycling or refereeing soccer games in Pennsylvania.
2015 IHSSF Healthcare Crime Survey Schneider Electric

Perspective: When the Hospital is the Victim

4.8K views 116 1 973

Top 3 components of a solid healthcare security program

18.3K views 304 51 2.6K

IHSSF Weapons Survey – Summary

4.4K views 21 0 1.0K

Healthcare Events Focus on Improving Patient Care through Technology

5.0K views 9 0 856

Healthcare highlights from the 11th annual RFID Journal LIVE conference

4.8K views 3 0 796

Security lessons learned from Boston’s hospitals

5.1K views 5 2 971

Sharing healthcare security fundamentals in Sweden

5.5K views 4 1 847