Stephen Mooney

Steve Mooney

Based in West Kingston, RI, Steve Mooney is the Director of Global Marketing Strategy for Secure Power Systems. In his role, Steve is responsible for the development and analysis of marketing campaigns and communications supporting the Secure Power Systems strategic application area. Steve moved over to Marketing Strategy from Enterprise sales in 2005 and has been with Schneider Electric for over twelve years.
IT OT Collaboration

Ensuring Reliability of Internet of Things Applications Requires IT/OT Collaboration

5.0K views 6 0 168
facility manager

Personality Test: What Sort of Facility Manager Are You?

7.7K views 98 49 922
disaster recovery

For Healthcare Providers, Disaster Recovery is a Matter of Life or Death

5.5K views 72 21 821

Falling Prices Increases Importance of Secure and Continuous Oil and Gas Production

7.0K views 59 0 816

Protecting the Network Edge in an Internet of Things Environment

10.9K views 1.1K 0 1.1K

The Internet of Things Demands a Fresh Look at Power Protection

22.4K views 987 269 3.1K

Achieving Business Success with the Internet of Things Means Getting IT and OT to Work Together

9.3K views 547 29 1.3K

The Internet of Things: Simplifying the Reliability Equation

14.7K views 411 22 2.0K