Hans Luppens

Hans Luppens

  • Connect with me
  • RSS
Hans Luppens is the Global Business Development Manager for the healthcare, water and airports market segments for both IT and non IT Applications.
business continuity plan

No Room for Risk: A Sound Business Continuity Plan Is a Must for Healthcare Facilities

15.8K views 253 0 842
medical imaging

The Importance of a UPS in Medical Imaging and Diagnostics

6.9K views 85 0 687
business continuity

Why Hospitals Are Linking Business Continuity to Improved Patient Satisfaction

8.3K views 101 0 876

To Boil or Not to Boil? The Essential Role Critical Power Plays in Water Treatment to Ensure Community Safety

11.3K views 23 0 1.2K

How Can You Leverage Manufacturing Quality Improvement Techniques to Improve the Reliability of Your Healthcare Facility?

4.7K views 22 2 821

Critical Power Protection Helping Improve the Air Traveler’s Experience

8.4K views 73 48 799
Digital Medical Imaging

3 Core Challenges of Installing and Supporting Sophisticated Diagnostic Equipment in Hospitals

8.5K views 127 1 1.4K
Assessing the Health of Your Healthcare Facility’s Electrical Power Distribution System

Healthcare facility reliability and resiliency benefits from integrated design approach

7.2K views 43 0 997

Reliability Leads Secure Power Priorities in Water & Waste Water Sector

14.9K views 36 2 1.2K

Secure Power in Healthcare: Taking Care of the Pain Points

7.6K views 18 15 995