Rod West

Rod West is a Senior Staff Engineer for Schneider Electric. Mr. West holds a BS from Rose-Hulman Institute of Technology and is a registered Professional Engineer. He has worked in the electrical industry for over 27 years and holds a total of 11 Patents for various types of electrical equipment and components. Mr. West chairs the Board of Directors for Whitewater Valley REMC, is a NAFI Certified Fire and Explosion Investigator and is a member of the Electrical Section of NFPA. He serves as a principal member of both NEC Code Making Panel #8 and NFPA 70E, the Standard for Electrical Safety in the Workplace.

Normal Operating Condition of Electrical Equipment

3.6K views 0 0 201

NFPA 70E Changes: Now Everyone can Benefit from the Tables

11.5K views 128 20 1.8K
Electrical worker in PPE

The Risk Assessment: An Electrical Contractor’s Most Important Tool

12.9K views 0 5 1.4K