Peter Martin

Peter Martin

  • Connect with me
  • RSS
Dr. Martin is a recognized leader and innovator in the field of automation and control. He has been a practitioner in the field for over 37 years, has authored three books, coauthored two and has been a contributing author for three more, as well as publishing dozens of articles and papers in the field of automation and control. He holds or has pending multiple patents in the areas of real-time business measurement and control. He was recognized by Fortune as a Hero of U.S. Manufacturing, Intech as one of the Fifty Most Influential Innovators in Control, by Control as a member of the Automation Hall of Fame and received ISA’s Life Achievement Award. He has a BA and MS in Mathematics, an MA in Administration and Management, a PhD in Industrial Engineering, as well as a Masters and PhD in Biblical Studies.
automation control

If You Cannot “Control” it, Try to “Manage” it.

7.2K views 11 0 1.5K

What is Really Going on in Industrial Automation?

13.1K views 605 89 1.4K

Profitable Sustainability

6.3K views 14 0 929

Why All the Focus on Energy?

8.4K views 465 26 809

The Golden Age of Control

4.7K views 33 1 1.0K

Millennials – The right generation at the perfect time

7.3K views 486 3 1.1K

Where Have All the Control Engineers Gone?

6.8K views 768 3 1.1K

Do automation systems provide “improved business value”?

12.3K views 782 10 2.0K