Peter Martin

Peter Martin

  • Connect with me
  • RSS
Dr. Martin is a recognized leader and innovator in the field of automation and control. He has been a practitioner in the field for over 37 years, has authored three books, coauthored two and has been a contributing author for three more, as well as publishing dozens of articles and papers in the field of automation and control. He holds or has pending multiple patents in the areas of real-time business measurement and control. He was recognized by Fortune as a Hero of U.S. Manufacturing, Intech as one of the Fifty Most Influential Innovators in Control, by Control as a member of the Automation Hall of Fame and received ISA’s Life Achievement Award. He has a BA and MS in Mathematics, an MA in Administration and Management, a PhD in Industrial Engineering, as well as a Masters and PhD in Biblical Studies.

Out of Control Asset Performance!

4.4K views 2 0 211

A Year to Celebrate the Programmable Logic Controller!

8.1K views 16 1 489

Maintenance is not Enough!

4.7K views 0 0 282

The Need to Shift Control for Profitable Efficiency

7.5K views 293 0 427

Loss of a Legend – And a Friend

7.3K views 725 47 953

Power to the people: The human factor in the plant of the future

7.3K views 149 10 585

Define a Profitable Reliability strategy through Automation

12.2K views 45 3 853

IIoT-enabled Technology Ignites the Profit Engine of Industry

8.3K views 53 43 932
profit engine

A Profit Engine for your enterprise? It’s under control…

5.8K views 51 5 817
automation architecture

How Can We Make Automation Architectures fit Industry?

8.0K views 69 40 949
Autonomous IIoT Assets

IIoT and Autonomous Industrial Assets

6.6K views 21 3 937
IIoT control maintenance

IIoT Enables Real-Time Maintenance Control

6.5K views 50 2 1.1K